i.MX6 ASRC_ASRCTR setting.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6 ASRC_ASRCTR setting.

跳至解决方案
2,392 次查看
satoshishimoda
Senior Contributor I

Hi community,

I have a questions about i.MX6 ASRC_ASRCTR setting.

Please see chapter 15.7.1 in IMX6SDLRM Rev.1.

I understand pair A will automatic update when ATSA bit is 1, and update manually by USRA and IDRA bit when ATSA bit is 0.

Then, how about when the following setting?

Pair A will automatic update? or ASRC internal measured ratio will be used?

ATSA = 1

USRA = 1

IDRA = 0

Best Regards,

Satoshi Shimoda

标签 (2)
标记 (1)
0 项奖励
回复
1 解答
2,192 次查看
Yuri
NXP Employee
NXP Employee

Pair A will automatic update, based on ASRC internal measured ratio.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,193 次查看
Yuri
NXP Employee
NXP Employee

Pair A will automatic update, based on ASRC internal measured ratio.

0 项奖励
回复
2,191 次查看
satoshishimoda
Senior Contributor I

Hi Yuri,

According to your reply, ATSA setting and {USRA, IDRA} setting are applied at the same time.

Then, how about {ATSA, USRA, IDRA} = {1,0,0}.

I guess USRA & IDRA is ignored and "Pair A will automatic update its pre-processing and post-processing options based on the frequencies it detected".

Is this correct?

Best Regards,

Satoshi Shimoda

0 项奖励
回复
2,192 次查看
satoshishimoda
Senior Contributor I

Can somebody reply me?

0 项奖励
回复