i.MX6/7 HAB: does it need a stack ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6/7 HAB: does it need a stack ?

1,403 Views
vsiles
Senior Contributor I

Hi !

I have a couple question of the HAB of i.MX6/7:

- does it needs a valid stack to execute ?

- if the answer is yes, is there a minimal stack size that must be used ?

I didn't find anything in the "High Assurance Boot Version 4 Application Programming Interface Reference Manual"

Best,

V.

Tags (1)
0 Kudos
Reply
1 Reply

1,219 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello,

Hello Vincent,

You can find more details on how to use the HAB of the i.MX6 in the following thread.

Mx6 HAB (High Assurance Boot) 

If you need further information I apologize, but the information you are requesting is treated as confidential info at this time and requires a signed NDA (Non-Disclosure Agreement). Naturally, we cannot discuss this with you in public anyway, this requires to be handled as a Case. Be aware that to give you remote support through a Case, we will still need the confirmation of a NXP employee that the NDA is in place. If you want to go this route, the next steps will be: If you have already signed a NDA agreement for this product, please contact the person who assisted you or create a Case and name us a NXP person that can confirm this. If you have not signed an agreement, please contact your local NXP Distributor Salesperson or FAE for assistance. For a listing of our distributors, refer to: http://www.nxp.com/webapp/sps/site/overview.jsp?code=DISTRIBUTORS

Have a great day,
TIC

-------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-------------------------------------------------------------------------------

0 Kudos
Reply