Boot Animation taking too long on iMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot Animation taking too long on iMX6

2,162 Views
suhaskaundinya
Contributor I

Hello,

I am using i.MX 6Quad SABRE-AI with Andriod N.

The boot animation log is as follows, but it is taking 42 seconds to boot. Is there a way I can shorten the time? Is there a problem in the log? Also, how to change the permissions?

init: Starting service 'bootanim'...
type=1400 audit(12.610:14): avc: denied { getattr } for pid=299 comm="bootanimation1
type=1400 audit(14.520:15): avc: denied { write } for pid=377 comm="BootAnimation" 1
type=1400 audit(14.540:16): avc: denied { open } for pid=377 comm="BootAnimation" p1
capability: warning: `main' uses 32-bit capabilities (legacy support in use)
period 0 ,timeout is 0, wake up is : 0
period 0 ,timeout is 0, wake up is : 0
acc_open
acc_release
fec 2188000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr)
IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
period 66 ,timeout is 0, wake up is : 0
mma enable setting active
init: Service 'bootanim' (pid 299) exited with status 0

Regards,

Suhas

Labels (3)
0 Kudos
Reply
1 Reply

1,801 Views
diegoadrian
NXP Employee
NXP Employee

Hello Suhas,

Yes, you can optimize the booting process. You can make it by re-arranging the booting process and eliminating some unnecessary process for the booting. Unfortunately, we only have implemented this process for Android KitKat. However, you can go with NXP professional service support and they can help you make a patch for Android Nougat.

NXP Professional Services|NXP 

Furthermore, this is our patch for Android KitKat, if you are willing to check it out.

https://community.nxp.com/docs/DOC-173487 

Best Regards,

Diego.

0 Kudos
Reply