i.MX535 - LPDDR2 Kernel Config

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX535 - LPDDR2 Kernel Config

ソリューションへジャンプ
2,085件の閲覧回数
SrideviK
Contributor III

Hi,

We are using Android R10.4 BSP as our reference.

In our custom platform we are using LPDDR2 interfaced to i.MX535 and PMIC used in MC34708.

Basically without Power management we have the device running properly as the Uboot DCD customization is done to meet the LPDDR2 requirement.

But when the power management is enabled & device enters suspend mode, it gets stuck in suspend_in_iram. There are some configurations in suspend.s.

Pls advice on the Kernel changes required with respect to LPDDR2 configuration.

Regards,

Sridevi

ラベル(2)
0 件の賞賛
返信
1 解決策
1,915件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

Hi, Sridevi

     I think maybe you can try comment out the DDR IO related power setting(PM_SET_HIGHZ_PAD), as LPDDR2 has different IO settings.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,916件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

Hi, Sridevi

     I think maybe you can try comment out the DDR IO related power setting(PM_SET_HIGHZ_PAD), as LPDDR2 has different IO settings.

0 件の賞賛
返信
1,915件の閲覧回数
SrideviK
Contributor III

Hi Yongcai Huang,

Yes. Commented out the DDR IO related power setting (PM_SET_HIGHZ_PAD) in suspend.S.

Suspend & Wakeup is working fine.

Thanks for the support.

Regards,

Sridevi

0 件の賞賛
返信