i.MX53 custom board not booting - lost in boot ROM - please help

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX53 custom board not booting - lost in boot ROM - please help

1,212 次查看
pierreschirrer
Contributor II

Hello all,

We designed a custom board based on i.MX53 and LPDDR2. After figuring out the configuration of the SDRAM controller for the LPDDR2, and adjusted the DCD, we tried to boot the board from SD card. The board does not boot.

Debugging under JTAG we found out the following :

1. If the SDRAM controller is initialized through the JTAG, the board does boot.

2. Stepping through the boot ROM, we found out that the DCD is copied from the SD card to the iRAM, but the i.MX53 registers are never initialized according to this DCD table.

3. Debugging further the boot ROM, we found out that 2 compares in the boot ROM code are validated (code snippets below).

4. Strangely, when doing the same debug on another completely different board (still i.MX53 but DDR3) that is working for some time and does boot when used without debugger, presents the same problem at the 2 compares and does not boot when the debugger is used.

Debugger used : Segger JLink Ultra+

Boot ROM code snippets :

40831e:    2200          movs    r2, #0

  408320:    20dd          movs    r0, #221    ; 0xdd

  408322:    4611          mov    r1, r2

  408324:    f7ff     fe11         bl    0x407f4a    ;

  408328:    28f0          cmp    r0, #240    ; 0xf0    <=== Here we have 0x33 = 51 in r0

  40832a:    d10e          bne.n    0x40834a    ; TAKEN!!

and

  40d6ca:    f7fd ff5b     bl    0x40b584    ; @MF this also returns 33...

  40d6ce:    28f0          cmp    r0, #240    ; 0xf0  <=== Here also we have 0x33 = 51 in r0

  40d6d0:    d10e          bne.n    0x40d6f0    ; Taken when forced earlier...


if we put breakpoints at the 2 compares above and force r0 at 0xF0 = 240, the board boots from SD...


Does anybody know what these two compares achieve or why this setup brings these values of 51 instead of 240 ?

Is there a way to get the source code of the boot ROM to understand why the board does not boot ?


Any hints or help would be appreciated,


Best regards,

标签 (1)
0 项奖励
回复
2 回复数

1,087 次查看
pierreschirrer
Contributor II

Thanks Igor,

We figured out the problem, the reset timing of the i.MX53 was not correct.

Regards.

0 项奖励
回复

1,087 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Pierre

ROM sources are not avilable, but I would suggest to check ivt:

csf: Absolute address of Command Sequence File (CSF)

must be set to NULL when not performing a secure boot

and if DCD has valid address ranges: Table 7-35. Valid DCD

Address Ranges  IMX53RM

Best regards

igor

0 项奖励
回复