i.MX53 VPU decoder output timing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX53 VPU decoder output timing

ソリューションへジャンプ
1,731件の閲覧回数
torus1000
Contributor V

Hi Chip experts,

I have a quesion when i.MX53 VPU decoded data write to the frame buffer.

Which timing is correct?

a)  data wrote per each microblock decoded
b)  or data wrote only when whole frame decoded

Thanks.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,627件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

The VPU has an internal DSP called the BIT processor which controls the internal hardware blocks for

video decoder operations.

The BIT processor completes decoding operations on a frame-by-frame basis, which allows low level

independency of VPU operations to the host processor

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,628件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

The VPU has an internal DSP called the BIT processor which controls the internal hardware blocks for

video decoder operations.

The BIT processor completes decoding operations on a frame-by-frame basis, which allows low level

independency of VPU operations to the host processor

0 件の賞賛
返信