i.MX53 USB port access by User Application

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX53 USB port access by User Application

1,393件の閲覧回数
robertzdunski
Contributor I
I have an external device connected through USB interface to the i.MX53. That device might function as OTG, Host or slave, no problem, I have full control over it. Ideally I would like to have that device function as an HID class device connected to i.MX53 host, but it is not mandatory at all. Any suggestions of how the USB port of the i.MX53 could be accessed by my Android application (i.MX53 is running the most recent Android Gingerbred by Adeneo)?
タグ(1)
0 件の賞賛
返信
1 返信

1,308件の閲覧回数
rlorriaux
Contributor I
libusb can be ported fairly easily to android (search for "libusb android") and will let you access the USB port in a friendly way. Then, you can expose it to Java apps if you want to.
0 件の賞賛
返信