i.MX53 Serial communication

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX53 Serial communication

ソリューションへジャンプ
3,250件の閲覧回数
i_MX51EVKSDCard
Contributor II

I have imx53 on my board and had my sequence worked out. But I don't see any serial prompt something like ' >', am I suppose to see something at power up on the serial prompt? I wanted to run python script iMX_Serial_Download_Protocol.py

Please help

Thanks,

-Puneet


ラベル(1)
0 件の賞賛
返信
1 解決策
3 返答(返信)
2,631件の閲覧回数
Yuri
NXP Employee
NXP Employee

The internal serial (UART / USB) i.MX bootloader does not provide any special prompt.
Sometimes we can see some chars 'Vx' as standard (ACK) responses (0x56, 0x78), but those
are not prompt. Please look at section 7.8.3 (Serial Download Protocol) of the i.MX53 Reference
Manual. 

0 件の賞賛
返信
2,631件の閲覧回数
i_MX51EVKSDCard
Contributor II

Thanks Yuri.

Are there any examples I can load on-chip using JTAG to test some internal features like how fast is the core clock running, if serial port is initialized etc.?

Also we have DDR3 in our system, how to initialize it and adjust timing?

Please advice.

Thanks,

-Puneet

0 件の賞賛
返信
2,632件の閲覧回数
Yuri
NXP Employee
NXP Employee
0 件の賞賛
返信