i.MX53 Sabre Tablet Audio Path Setup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX53 Sabre Tablet Audio Path Setup

1,522件の閲覧回数
ChuckFarago
Contributor I

How do I set up the LINEIN to I2S to i.MX53 to Bluetooth audio path on the i.MX53 Sabre tablet?

ラベル(1)
0 件の賞賛
返信
1 返信

1,369件の閲覧回数
Yuri
NXP Employee
NXP Employee

If the Bluetooth configuration is alredy working ou only need the following:

1) Be sure in your Bluetooth firmware the audio output is set to PCM line or I2S.

2) Configure in your board file ( in case of Linux)  the proper I2S line to be used.

3) Maybe you need to add some pull up on the line.

0 件の賞賛
返信