Hi All,
We are using Audio DAC WM8523 from Wolfson in our i.mX53 based custom board.
The Audio DAC is interfaced to to the i.MX53 processor through I2S (Audio Mux) & I2C (Software Control Interface).
The WM8523 driver used is from (provided by Wolfson) : http://opensource.wolfsonmicro.com/cgi-bin/gitweb.cgi?p=linux-2.6-asoc.git;a=blob_plain;f=sound/soc/...
When we use this we are getting an error - "No MCLK configured, call set_sysclk() on init" and the System unable to detect the DAC as the sound device.
Has anyone used WM8523 with any of the i.MX series Processors and were able to get it work?
Regards,
Gopi
已解决! 转到解答。
GopiNagaBharath
We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the
issue, can we close the discussion? If you still need Freescale help, please feel free to contact us.
Thanks,
Yixing