i.MX53 SABRE Windows Embedded Compact 7 (WEC7) Command Prompt not working in iMX53_SMD_Mobility Project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX53 SABRE Windows Embedded Compact 7 (WEC7) Command Prompt not working in iMX53_SMD_Mobility Project

ソリューションへジャンプ
2,617件の閲覧回数
kriszawada
Contributor III

Hello,

I was able to successfully use Microsoft Visual Studio 2008 and Platform Builder to build Fresscale i_MX53 SMD ARMV7 Release version of the iMX53_SMD_Mobility project.  I can take the eboot.nb0 and NK.nb0, program SD/microSD and boot the the OS image.

Now, when I select START (Windows logo) | Programs | Command Prompt I can see that WEC7 attempts to open this application, but if fails to start and I can't see the graphical part of this.  When I use terminal program to look at the debug output I can see the following (after launching a few times):

PID:0775003E TID:0776003E  PID:0775003E TID:0776003E Pocket CMD v 7.00

PID:0775003E TID:0776003E \PID:0775003E TID:0776003E >PID:0775003E TID:0776003E  PID:0606004A TID:07E40046  PID:0606004A TID:07E40046 Pocket CMD v 7.00

PID:0606004A TID:07E40046 \PID:0606004A TID:07E40046 >PID:0606004A TID:07E40046  PID:00EA03DE TID:06D7007E  PID:00EA03DE TID:06D7007E Pocket CMD v 7.00

PID:00EA03DE TID:06D7007E \PID:00EA03DE TID:06D7007E >PID:00EA03DE TID:06D7007E  PID:00E903A6 TID:075D0086  PID:00E903A6 TID:075D0086 Pocket CMD v 7.00

PID:00E903A6 TID:075D0086 \PID:00E903A6 TID:075D0086 >PID:00E903A6 TID:075D0086  PID:00ED02BA TID:07F40096  PID:00ED02BA TID:07F40096 Pocket CMD v 7.00

PID:00ED02BA TID:07F40096 \PID:00ED02BA TID:07F40096 >PID:00ED02BA TID:07F40096

Why is it that with the example project iMX53_SMD_Mobility provided by Freescale does not allow the Command Prompt to work?  Is this a memory limitation of some sort?  Is there anyway I can get additional information?

ラベル(2)
0 件の賞賛
返信
1 解決策
2,217件の閲覧回数
kriszawada
Contributor III

The main reason for this not working is because the "Console Window" was not enabled in the Catalog items.

In Microsoft Visual Studio 2008 Open iMX53_SMD_Mobility Solution.  Then click on "Catalog Items View" and traverse "iMX53_SMD_Mobility" -> Core OS -> Windows Embedded Compact -> Shell and User Interface -> Shell -> Command Shell -> Place a check next to "Console Window".

MSVS2008_PlatformBuilder_ConsoleWindow.png

Once the "Console Window" is checked, rebuild the OS and reprogram the SD/microSD card with the bootloader and OS images.  Boot from the SD/microSD card and launch the command prompt again.  You will now see it.

Issue resolved.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,218件の閲覧回数
kriszawada
Contributor III

The main reason for this not working is because the "Console Window" was not enabled in the Catalog items.

In Microsoft Visual Studio 2008 Open iMX53_SMD_Mobility Solution.  Then click on "Catalog Items View" and traverse "iMX53_SMD_Mobility" -> Core OS -> Windows Embedded Compact -> Shell and User Interface -> Shell -> Command Shell -> Place a check next to "Console Window".

MSVS2008_PlatformBuilder_ConsoleWindow.png

Once the "Console Window" is checked, rebuild the OS and reprogram the SD/microSD card with the bootloader and OS images.  Boot from the SD/microSD card and launch the command prompt again.  You will now see it.

Issue resolved.

0 件の賞賛
返信