i.MX53 Quick Start-R and Battery Attach event

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX53 Quick Start-R and Battery Attach event

ソリューションへジャンプ
1,880件の閲覧回数
actarus999
Contributor I

Hi, I bought the i.MX53 Quick Start-R (I still waiting for the delivering).
I don't understood how I have to set event "Battery Attach" to perform the automatic startup when I plug the DC power supply.

Is there someone that can explain how I have to do ?

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
1,801件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Actarus ,

         

     You can go to Freescale's official website http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB to download the i.MX53QSB BSP. After you build the BSP succeed by LTIB , you can download the Image you have built to the board . If download finish ,you can boot the board in different ways after you giving the power supply. All details you can reference to the document "i.MX53_START_Linux_BSP_UserGuide.pdf". This document can be download here http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&fpsp=1&tab=Documentation_Tab, the name is IMX53_1109_LINUXDOCS_BUNDLE. There's also demo Image in http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB, you can have a try.

Hope this can help you~~

Best Regards

Dan

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,802件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Actarus ,

         

     You can go to Freescale's official website http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB to download the i.MX53QSB BSP. After you build the BSP succeed by LTIB , you can download the Image you have built to the board . If download finish ,you can boot the board in different ways after you giving the power supply. All details you can reference to the document "i.MX53_START_Linux_BSP_UserGuide.pdf". This document can be download here http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&fpsp=1&tab=Documentation_Tab, the name is IMX53_1109_LINUXDOCS_BUNDLE. There's also demo Image in http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB, you can have a try.

Hope this can help you~~

Best Regards

Dan

0 件の賞賛
返信
1,801件の閲覧回数
actarus999
Contributor I

OK, thank you.

I will try when the board arrive.

Bye

Actarus

0 件の賞賛
返信