i.MX53-QSB Linux. USB is not working.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX53-QSB Linux. USB is not working.

2,248件の閲覧回数
priyathamodela
Fresh Out Contributor

Hello,

I am using i.MX53 QSB with Linux. I am facing problem with on board USB.

It is unable to populate the device USB devices. I have connected a

Dell Optical mouse(Model: MS111), on the serial console i could see the following prints.

and for about 20 iterations board gets restarted. I am using prebuilt linux images downloaded from freescale.com

usb 2-1: new low speed USB device using fsl-ehci and address 2

input: PixArt USB Optical Mouse as /devices/platform/fsl-ehci.1/usb2/2-1/2-1:1.0/input/input4

generic-usb 0003:0461:4E22.0001: input: USB HID v1.11 Mouse [PixArt USB Optical Mouse] on usb-fsl-ehci.1-1/input0

usb 2-1: USB disconnect, address 2

usb 2-1: new low speed USB device using fsl-ehci and address 3

input: PixArt USB Optical Mouse as /devices/platform/fsl-ehci.1/usb2/2-1/2-1:1.0/input/input5

generic-usb 0003:0461:4E22.0002: input: USB HID v1.11 Mouse [PixArt USB Optical Mouse] on usb-fsl-ehci.1-1/input0

usb 2-1: USB disconnect, address 3

usb 2-1: new low speed USB device using fsl-ehci and address 4

input: PixArt USB Optical Mouse as /devices/platform/fsl-ehci.1/usb2/2-1/2-1:1.0/input/input6

generic-usb 0003:0461:4E22.0003: input: USB HID v1.11 Mouse [PixArt USB Optical Mouse] on usb-fsl-ehci.1-1/input0

usb 2-1: USB disconnect, address 4

usb 2-1: new low speed USB device using fsl-ehci and address 5

input: PixArt USB Optical Mouse as /devices/platform/fsl-ehci.1/usb2/2-1/2-1:1.0/input/input7

generic-usb 0003:0461:4E22.0004: input: USB HID v1.11 Mouse [PixArt USB Optical Mouse] on usb-fsl-ehci.1-1/input0

usb 2-1: USB disconnect, address 5


after connecting the device "lsusb" output is

(no device detected)


Bus 001 Device 001: ID 1d6b:0002

Bus 002 Device 001: ID 1d6b:0002

Thanks and Regards

Priyatham.

ラベル(3)
タグ(2)
0 件の賞賛
返信
1 返信

1,333件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

please download the BSP (L2.6.35_11_09_ER_SOURCE) and apply the patches (IMX53_LINUX_1109_BSP_PATCH).

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&fpsp=1&tab=Design_Tools_Tab

please try to build the image and then run it on the board.

0 件の賞賛
返信