i.MX53 QSB, Linux 3.7 and USB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53 QSB, Linux 3.7 and USB

Jump to solution
2,596 Views
nodan
Contributor II

Hi,

I'm running a Linux 3.7 kernel on an i.MX53 QSB. However, it looks like USB is not working properly. In /proc/devices I see:

# grep -i usb /proc/devices                                               
180 usb                                                                               

189 usb_device

but lsusb fails:

# lsusb                                                                   
unable to initialize libusb: -99

Actually I want to use a USB Wifi dongle. Has anybody done that with the QSB?


Regards,

Kai

Labels (2)
0 Kudos
Reply
1 Solution
1,975 Views
fabio_estevam
NXP Employee
NXP Employee

If you look at arch/arm/boot/dts/imx53-qsb.dts you will see that USB support is not in place yet.

You can look at arch/arm/boot/dts/imx6q-sabrelite.dts as this board has USB host support.

Then you can try to send your patch to linux-arm-kernel mailing list and we can discuss from there.

Regards,

Fabio Estevam

View solution in original post

0 Kudos
Reply
2 Replies
1,976 Views
fabio_estevam
NXP Employee
NXP Employee

If you look at arch/arm/boot/dts/imx53-qsb.dts you will see that USB support is not in place yet.

You can look at arch/arm/boot/dts/imx6q-sabrelite.dts as this board has USB host support.

Then you can try to send your patch to linux-arm-kernel mailing list and we can discuss from there.

Regards,

Fabio Estevam

0 Kudos
Reply
1,975 Views
nodan
Contributor II

Again, thanks.

I'll have a look but I'm not sure yet if I'll try to use USB or rather settle for an external wifi access point and use the LAN interface.

Regards,

Kai

0 Kudos
Reply