i.MX53 PMIC Options

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX53 PMIC Options

跳至解决方案
1,943 次查看
JohnMcCosh
Contributor II

Hello,

I am starting a new i.MX design with features similar to the Quick Start Board (DDR3, Tough Screen, Ethernet, USB-OTG), but battery powered and charged via the USB-OTG port.  I am considering using either the MC34709 PMIC or the MC13783 PMIC - Audio Device.  Has anyone looked into these compinations?  Thoughts and comments are welcomed.

John

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,700 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,John,

     you have 2 optional PMICs for your design based on i.MX53 :

(1)MC34708

(2)MC34709

     When you desigh your schematic, please pay attention to the following points:

(1)Using DIG_PLL_INT to supply VDDAL

(2)Using a LDO(3V->1.5V) to supply VDDLP on MC34708

This patch can be found in mc34708 errata.

These 2 steps are used to correct the issue of SRTC in i.MX53 (Ensure SRTC can hold correct time after cold reset)

Regards,

Weidong

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,701 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,John,

     you have 2 optional PMICs for your design based on i.MX53 :

(1)MC34708

(2)MC34709

     When you desigh your schematic, please pay attention to the following points:

(1)Using DIG_PLL_INT to supply VDDAL

(2)Using a LDO(3V->1.5V) to supply VDDLP on MC34708

This patch can be found in mc34708 errata.

These 2 steps are used to correct the issue of SRTC in i.MX53 (Ensure SRTC can hold correct time after cold reset)

Regards,

Weidong

0 项奖励
回复