i.MX53 Frame Synchronization Flow debugging

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX53 Frame Synchronization Flow debugging

跳至解决方案
2,134 次查看
torus1000
Contributor V

Hello chip experts,

Now I'm debugging my code for IPU IDMAC ch23.

In spite of following the Frame Synchronization Flow described in p2777 of i.MX53 RM,

IDMAC buffer toggling didn't observed when double buffer page flipping was used.
Please see step 4 on p2777.

Is there any tips or secrets to activate it?

How can I debug it? Which status registers should I check first?

Thanks.

标签 (2)
0 项奖励
回复
1 解答
2,029 次查看
igorpadykov
NXP Employee
NXP Employee

HI torus1000

I am not aware of such tips, probably one can look

at IPU examples in On-Board Diagnostic Suit for the i.MX53 Quick Start Board

or i.MX 6Series Platform SDK

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,030 次查看
igorpadykov
NXP Employee
NXP Employee

HI torus1000

I am not aware of such tips, probably one can look

at IPU examples in On-Board Diagnostic Suit for the i.MX53 Quick Start Board

or i.MX 6Series Platform SDK

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,029 次查看
torus1000
Contributor V

Dear Igor

Thank you for replying.

Finally I found my mistake which lost complete flag by read-modify-write access to the SET/CLEAR registers.

Have a nice day!

0 项奖励
回复