i.MX53 Frame Synchronization Flow debugging

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX53 Frame Synchronization Flow debugging

ソリューションへジャンプ
2,130件の閲覧回数
torus1000
Contributor V

Hello chip experts,

Now I'm debugging my code for IPU IDMAC ch23.

In spite of following the Frame Synchronization Flow described in p2777 of i.MX53 RM,

IDMAC buffer toggling didn't observed when double buffer page flipping was used.
Please see step 4 on p2777.

Is there any tips or secrets to activate it?

How can I debug it? Which status registers should I check first?

Thanks.

ラベル(2)
0 件の賞賛
返信
1 解決策
2,025件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI torus1000

I am not aware of such tips, probably one can look

at IPU examples in On-Board Diagnostic Suit for the i.MX53 Quick Start Board

or i.MX 6Series Platform SDK

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,026件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI torus1000

I am not aware of such tips, probably one can look

at IPU examples in On-Board Diagnostic Suit for the i.MX53 Quick Start Board

or i.MX 6Series Platform SDK

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,025件の閲覧回数
torus1000
Contributor V

Dear Igor

Thank you for replying.

Finally I found my mistake which lost complete flag by read-modify-write access to the SET/CLEAR registers.

Have a nice day!

0 件の賞賛
返信