i.MX53 Frame Synchronization Flow debugging

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53 Frame Synchronization Flow debugging

Jump to solution
2,070 Views
torus1000
Contributor V

Hello chip experts,

Now I'm debugging my code for IPU IDMAC ch23.

In spite of following the Frame Synchronization Flow described in p2777 of i.MX53 RM,

IDMAC buffer toggling didn't observed when double buffer page flipping was used.
Please see step 4 on p2777.

Is there any tips or secrets to activate it?

How can I debug it? Which status registers should I check first?

Thanks.

Labels (2)
0 Kudos
Reply
1 Solution
1,965 Views
igorpadykov
NXP Employee
NXP Employee

HI torus1000

I am not aware of such tips, probably one can look

at IPU examples in On-Board Diagnostic Suit for the i.MX53 Quick Start Board

or i.MX 6Series Platform SDK

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,966 Views
igorpadykov
NXP Employee
NXP Employee

HI torus1000

I am not aware of such tips, probably one can look

at IPU examples in On-Board Diagnostic Suit for the i.MX53 Quick Start Board

or i.MX 6Series Platform SDK

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,965 Views
torus1000
Contributor V

Dear Igor

Thank you for replying.

Finally I found my mistake which lost complete flag by read-modify-write access to the SET/CLEAR registers.

Have a nice day!

0 Kudos
Reply