i.MX51 buzzer driver using IO

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX51 buzzer driver using IO

2,403 次查看
alsaleem
Contributor I

Hi,

Is there a way to output a variable frequency signal (audio range, 200-4K) square wave from i.MX51 to drive an external buzzer?

 

Thanks.

标记 (1)
0 项奖励
回复
3 回复数

2,237 次查看
JerryFan
NXP Employee
NXP Employee
That's right, PWM is designed for brightness tuning, but it can also be used flexibly.  Actually, the PERIOD can be programmed (see Chapter 47.2.2.5, mx51RM for the detail.)  and  the frequency is much accurate that GPIO way. Anyway, if the accuracy  is not important, such as for a buzzer, the GPIO method should be OK.
0 项奖励
回复

2,237 次查看
alsaleem
Contributor I

The driver only allows to set the pulse width not frequency (fixed on initialization) using brightness. How do I change the PWM frequency?

Thanks.

0 项奖励
回复

2,237 次查看
JerryFan
NXP Employee
NXP Employee
PWM was recommended for this case. It is more accurate and need less arm core's involvement.
0 项奖励
回复