i.MX51 VDDGP Absolute Maximum Ratings(max) and Operating Ranges(max)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX51 VDDGP Absolute Maximum Ratings(max) and Operating Ranges(max)

1,249 Views
eishishibusawa
Contributor III

Dear Sir

 

I want to confirm the Absolute Maximum Ratings(max) and Operating Ranges(max) of i.MX51(Consumer Product) VDDGP.

It is described that both are 1.15V.

 

Q1.

Is this correct?

 

Best Regards,

Eishi SHIBUSAWA

Labels (1)
0 Kudos
Reply
1 Reply

1,150 Views
Yuri
NXP Employee
NXP Employee

Hello,

  yes, this is correct - the both voltages are 1.15V

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply