i.MX51 VDDGP Absolute Maximum Ratings(max) and Operating Ranges(max)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX51 VDDGP Absolute Maximum Ratings(max) and Operating Ranges(max)

1,236件の閲覧回数
eishishibusawa
Contributor III

Dear Sir

 

I want to confirm the Absolute Maximum Ratings(max) and Operating Ranges(max) of i.MX51(Consumer Product) VDDGP.

It is described that both are 1.15V.

 

Q1.

Is this correct?

 

Best Regards,

Eishi SHIBUSAWA

ラベル(1)
0 件の賞賛
返信
1 返信

1,137件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  yes, this is correct - the both voltages are 1.15V

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信