i.MX51 Image Rotator performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX51 Image Rotator performance

Jump to solution
2,432 Views
norishinozaki
Contributor V

Hello Champs,

In the i.MX51 RM, there is this description,

imx51_image_rotate.png

I'm using a LCD with 1024x768@60Hz, the pixel clock is 65MHz.

Simply, 1024x768x60 = 47MHz pixels/sec, which is within the spec 50 M pixels/sec.

Isn't there bit per pixel specification?

Can I use Image Rotator for 1024x768@60Hz?


BR,
Nori Shinozaki

Labels (3)
0 Kudos
Reply
1 Solution
2,336 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nori

data is provided for YUV/RGB format, 8 bits/value

as described in sect.42.1.3.3.2 Image Rotator (IRT),

sorry there is no bit per pixel specification.

>Can I use Image Rotator for 1024x768@60Hz?

in theory yes, in practice performance may be affected by available

memory bandwidth (depending on application) as IRT uses

input/output from/to system memory.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,337 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nori

data is provided for YUV/RGB format, 8 bits/value

as described in sect.42.1.3.3.2 Image Rotator (IRT),

sorry there is no bit per pixel specification.

>Can I use Image Rotator for 1024x768@60Hz?

in theory yes, in practice performance may be affected by available

memory bandwidth (depending on application) as IRT uses

input/output from/to system memory.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,336 Views
norishinozaki
Contributor V

Hello Igor,

Thanks!

BR, N.S.

0 Kudos
Reply