i.MX35 Setting SD2 gpio to pull up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX35 Setting SD2 gpio to pull up

ソリューションへジャンプ
4,046件の閲覧回数
frk
Contributor III

Hi all,


I'm trying to activate a new input on my i.MX35 device MX35_PAD_SD2_DATA3__GPIO2_4 and activating the pull up mode to this input.

But I'm a bit confused with the device tree configuration :

gpio_exporter: gpio-exporter {
compatible = "linux,gpio-exporter";
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_gpio_exporter>;

GPIO_IN {
gpios = <&gpio3 13 GPIO_ACTIVE_HIGH>;
};

GPIO_OUT {
gpios = <&gpio3 12 GPIO_ACTIVE_HIGH>;
output;
initial-state = <0>;
};

...

GPIO_NEWINPUT {
gpios = <&gpio2 4 GPIO_ACTIVE_HIGH>;
};
};

pinctrl_gpio_exporter: gpioexportergrp {
fsl,pins = <

MX35_PAD_RTS2__GPIO3_12 0x80000000
MX35_PAD_CTS2__GPIO3_13 0x80000000
...
MX35_PAD_SD2_DATA2__GPIO2_4 0x80000000
>;
};

Others GPIOs use the 0x80000000 value but what is it's meaning?

I have take a look to Table 301: Register: IOMUXC_SW_MUX_CTL_PAD_SD2_DATA2 but this subject is not clear enough for me.

I also have check in my include/dt-bindings/gpio/gpio.h file and no reference to pull up configuration.

0 件の賞賛
返信
1 解決策
4,036件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi frk

 

0x80000000 means that settings are inherited from uboot ( pin does not need config.)

https://source.codeaurora.org/external/imx/linux-imx/tree/Documentation/devicetree/bindings/pinctrl/...

More details can be found in AN5078

Influence of Pin Setting on System Function and Performance

Field "PULL_KEEP_CTL" Register: IOMUXC_SW_PAD_CTL_PAD_SD2_DATA3 configures

pull settings, described on p.2900  i.MX35 (MCIMX35) Multimedia Applications Processor Reference

 

 

 

Best regards
igor

 

元の投稿で解決策を見る

4 返答(返信)
4,014件の閲覧回数
frk
Contributor III

Thanks for your support.

Things are clearer now.

0 件の賞賛
返信
4,037件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi frk

 

0x80000000 means that settings are inherited from uboot ( pin does not need config.)

https://source.codeaurora.org/external/imx/linux-imx/tree/Documentation/devicetree/bindings/pinctrl/...

More details can be found in AN5078

Influence of Pin Setting on System Function and Performance

Field "PULL_KEEP_CTL" Register: IOMUXC_SW_PAD_CTL_PAD_SD2_DATA3 configures

pull settings, described on p.2900  i.MX35 (MCIMX35) Multimedia Applications Processor Reference

 

 

 

Best regards
igor

 

4,032件の閲覧回数
frk
Contributor III

So if 0x80000000 is used and nothing come from the bootloader, state can be considered as unknown/invalid?

 

I'll check the documentation, AN5078 seems pretty usefull.

0 件の賞賛
返信
4,026件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

>So if 0x80000000 is used and nothing come from the bootloader, state can be considered as unknown/invalid?

 

it is set as default state (after reset)

 

~igor