i.MX31 SDHC input setup/hold timing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX31 SDHC input setup/hold timing

1,219 Views
sugiyamatoshihi
Contributor V

Hi,

Does some one know the SDHC spec. of i.MX31?

There are input setup/hold time of SDHC in data sheet. However, it specify max value of setup/hold time like below.

SDHC input setup MAX  18.5nS, SDHC input hold MAX -11.5nS.

Usually, setup/hold time should be minimum  value not MAX.

Could you teach min value of setup/hold time? 

pastedImage_1.png

Best Regards,

Sugiyama

0 Kudos
Reply
3 Replies

1,121 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

   Parameters SD7 and SD8 are defined in the i.MX31 specs with regard to the failing CLK.

SD specs assume rising ones; so min values of  SD7 and SD8 are calculated as

CLK period / 2 - SD7/8.

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos
Reply

1,121 Views
sugiyamatoshihi
Contributor V

Hi, Yuri,

Thank you for quick reply.

If it is CLK period/2 - SD7/8, it depend on frequency, but I think setup/hold timing are fixed value.

Does it aware only 25MHz clock and use that value for other frequency?

I calculated them at 25MHz, 40nS cycle

Does it mean setup is 1.5nS min and hold is 8.5nS min?

Does this use for all frequency?

Best Regards,

Sugiyama

0 Kudos
Reply

1,121 Views
Yuri
NXP Employee
NXP Employee

Generally You are right: setup is 1.5nS min, hold is 8.5nS min for all frequencies.

~Yuri.

0 Kudos
Reply