i.MX287 ddr2-400 phy to ddr2-800 memory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX287 ddr2-400 phy to ddr2-800 memory

716 次查看
manonmanishanmu
Contributor I

Hi, We have i.MX287 (which  is having a DDR2- 400 Phy) connected to the DDR2-800 (PC2-6400)memory and the EVK reference design and power calculations allow 205MHz as EMI frequency but for DDR2-400 the maximum Frequency (for 400 Mbos)data rate the clock should be < 100 MHz please clarify and also I assume even though we configure the clock as 205MHz the Phy will run at 100 MHz only right please clarify

0 项奖励
回复
1 回复

620 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Manonmani

it is necessary to configure i.MX28 as for DDR2- 400 memory, also please

pay attention to drive strength tweaking. Recommended to use ddr test, like below

https://community.freescale.com/message/375692#375692

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复