i.MX28 - running elftosb on target

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX28 - running elftosb on target

跳至解决方案
2,477 次查看
ChristophG_Baum
Contributor III

Hello Forum,

trying to use an encrypted firmware based on Linux, I ran into the problem of executing elftosb natively on the i.MX28.

The reason behind this is that I want to avoid to store the key outside the SoC. So elftosb needs to use the DCP to generate an encrypted image (assuming the unencrypted image was transferred securely onto the system).

Is there a version of elftosb or some other tool which uses the DCP natively?

Regards,

Christoph

标签 (2)
标记 (4)
0 项奖励
回复
1 解答
2,065 次查看
JackLee1z
NXP Employee
NXP Employee

Hi Christoph,

It is understood but the requested tool is not available. If you think this new feature is a must for your project, please go through sales and marketing channel to have an arrangement. Thanks.

BR,

Jack

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,065 次查看
JackLee1z
NXP Employee
NXP Employee

Hi Chris,

There is no such version for elftosb to be run on i.MX28 SoC. You are suggested to use the provided tool in BSP on host environment.

BR,

Jack

0 项奖励
回复
2,065 次查看
ChristophG_Baum
Contributor III

Hello,

the idea behind my question is that when you use the DCP to encrypt the bootstream, the AES key does not need to exist outside the device. It is kept in the OTP and only the DCP can use it.

Regards

Christoph

0 项奖励
回复
2,066 次查看
JackLee1z
NXP Employee
NXP Employee

Hi Christoph,

It is understood but the requested tool is not available. If you think this new feature is a must for your project, please go through sales and marketing channel to have an arrangement. Thanks.

BR,

Jack

0 项奖励
回复