i.MX28 not recognizing bad blocks in DBBT

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX28 not recognizing bad blocks in DBBT

1,571 次查看
SJA
Contributor II

We have found that the i.MX28 boot ROM is ignoring the DBBT tables.

Below is a dump of the NAND where we have one bad block at index 0xD0.

It is marked in the DBBT but the system will not boot the primary image.

We are creating and writing the images to nand using stock freescale kobs-ng.

Also we took a unit with no bad blocks and changed kobs-ng to put some fake bad

blocks just in the DBBT but the system still booted just fine. (If the boot ROM

was reading the DBBT it would have not booted since the bad blocks in the DBBT

did not match what was written to NAND)

Here us a hand annotated hexdump of NAND flash

First FCB:

00000000  00 00 00 00 00 00 00 00  00 00 00 00 7f fc ff ff  |................|

00000010  46 43 42 20 00 00 00 01  50 3c 19 06 00 00 00 00  |FCB ....P<......|

00000020  00 08 00 00 40 08 00 00  40 00 00 00 00 00 00 00  |....@...@.......|

00000030  00 00 00 00 00 00 00 00  04 00 00 00 00 02 00 00  |................|

00000040  00 02 00 00 04 00 00 00  0a 00 00 00 03 00 00 00  |................|

00000050  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

00000060  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

00000070  00 00 00 00 00 02 00 00  00 29 00 00 0e 0d 00 00  |.........)......|

00000080  0e 0d 00 00 00 01 00 00  cf 07 00 00 00 00 00 00  |................|

00000090  00 08 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000000a0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

*

Hamming codes:

00000200  00 00 00 00 00 00 00 00  00 00 00 00 08 0c 06 06  |................|

00000210  10 1f 03 07 00 00 00 1c  0f 17 1f 05 00 00 00 00  |................|

00000220  00 19 00 00 15 19 00 00  15 00 00 00 00 00 00 00  |................|

00000230  00 00 00 00 00 00 00 00  13 00 00 00 00 16 00 00  |................|

00000240  00 16 00 00 13 00 00 00  0f 00 00 00 0a 00 00 00  |................|

00000250  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

00000260  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

00000270  00 00 00 00 00 16 00 00  00 02 00 00 1c 16 00 00  |................|

00000280  1c 16 00 00 00 1c 00 00  1b 19 00 00 00 00 00 00  |................|

00000290  00 19 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000002a0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

*

00000800  ff ff ff ff ff ff ff ff  ff ff ff ff ff ff ff ff  |................|

*

Second FCB:

00021000  00 00 00 00 00 00 00 00  00 00 00 00 7f fc ff ff  |................|

00021010  46 43 42 20 00 00 00 01  50 3c 19 06 00 00 00 00  |FCB ....P<......|

00021020  00 08 00 00 40 08 00 00  40 00 00 00 00 00 00 00  |....@...@.......|

00021030  00 00 00 00 00 00 00 00  04 00 00 00 00 02 00 00  |................|

00021040  00 02 00 00 04 00 00 00  0a 00 00 00 03 00 00 00  |................|

00021050  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

00021060  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

00021070  00 00 00 00 00 02 00 00  00 29 00 00 0e 0d 00 00  |.........)......|

00021080  0e 0d 00 00 00 01 00 00  cf 07 00 00 00 00 00 00  |................|

00021090  00 08 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000210a0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

*

Hamming codes:

00021200  00 00 00 00 00 00 00 00  00 00 00 00 08 0c 06 06  |................|

00021210  10 1f 03 07 00 00 00 1c  0f 17 1f 05 00 00 00 00  |................|

00021220  00 19 00 00 15 19 00 00  15 00 00 00 00 00 00 00  |................|

00021230  00 00 00 00 00 00 00 00  13 00 00 00 00 16 00 00  |................|

00021240  00 16 00 00 13 00 00 00  0f 00 00 00 0a 00 00 00  |................|

00021250  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

00021260  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

00021270  00 00 00 00 00 16 00 00  00 02 00 00 1c 16 00 00  |................|

00021280  1c 16 00 00 00 1c 00 00  1b 19 00 00 00 00 00 00  |................|

00021290  00 19 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000212a0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

*

00021800  ff ff ff ff ff ff ff ff  ff ff ff ff ff ff ff ff  |................|

*

Third FCB:

00042000  00 00 00 00 00 00 00 00  00 00 00 00 7f fc ff ff  |................|

00042010  46 43 42 20 00 00 00 01  50 3c 19 06 00 00 00 00  |FCB ....P<......|

00042020  00 08 00 00 40 08 00 00  40 00 00 00 00 00 00 00  |....@...@.......|

00042030  00 00 00 00 00 00 00 00  04 00 00 00 00 02 00 00  |................|

00042040  00 02 00 00 04 00 00 00  0a 00 00 00 03 00 00 00  |................|

00042050  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

00042060  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

00042070  00 00 00 00 00 02 00 00  00 29 00 00 0e 0d 00 00  |.........)......|

00042080  0e 0d 00 00 00 01 00 00  cf 07 00 00 00 00 00 00  |................|

00042090  00 08 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000420a0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

*

Hamming codes:

00042200  00 00 00 00 00 00 00 00  00 00 00 00 08 0c 06 06  |................|

00042210  10 1f 03 07 00 00 00 1c  0f 17 1f 05 00 00 00 00  |................|

00042220  00 19 00 00 15 19 00 00  15 00 00 00 00 00 00 00  |................|

00042230  00 00 00 00 00 00 00 00  13 00 00 00 00 16 00 00  |................|

00042240  00 16 00 00 13 00 00 00  0f 00 00 00 0a 00 00 00  |................|

00042250  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

00042260  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

00042270  00 00 00 00 00 16 00 00  00 02 00 00 1c 16 00 00  |................|

00042280  1c 16 00 00 00 1c 00 00  1b 19 00 00 00 00 00 00  |................|

00042290  00 19 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000422a0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

*

00042800  ff ff ff ff ff ff ff ff  ff ff ff ff ff ff ff ff  |................|

*

Forth FCB:

00063000  00 00 00 00 00 00 00 00  00 00 00 00 7f fc ff ff  |................|

00063010  46 43 42 20 00 00 00 01  50 3c 19 06 00 00 00 00  |FCB ....P<......|

00063020  00 08 00 00 40 08 00 00  40 00 00 00 00 00 00 00  |....@...@.......|

00063030  00 00 00 00 00 00 00 00  04 00 00 00 00 02 00 00  |................|

00063040  00 02 00 00 04 00 00 00  0a 00 00 00 03 00 00 00  |................|

00063050  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

00063060  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

00063070  00 00 00 00 00 02 00 00  00 29 00 00 0e 0d 00 00  |.........)......|

00063080  0e 0d 00 00 00 01 00 00  cf 07 00 00 00 00 00 00  |................|

00063090  00 08 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000630a0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

*

Hamming codes:

00063200  00 00 00 00 00 00 00 00  00 00 00 00 08 0c 06 06  |................|

00063210  10 1f 03 07 00 00 00 1c  0f 17 1f 05 00 00 00 00  |................|

00063220  00 19 00 00 15 19 00 00  15 00 00 00 00 00 00 00  |................|

00063230  00 00 00 00 00 00 00 00  13 00 00 00 00 16 00 00  |................|

00063240  00 16 00 00 13 00 00 00  0f 00 00 00 0a 00 00 00  |................|

00063250  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

00063260  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

00063270  00 00 00 00 00 16 00 00  00 02 00 00 1c 16 00 00  |................|

00063280  1c 16 00 00 00 1c 00 00  1b 19 00 00 00 00 00 00  |................|

00063290  00 19 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000632a0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

*

00063800  ff ff ff ff ff ff ff ff  ff ff ff ff ff ff ff ff  |................|

*

First DBBT header:

00084000  00 ff ff ff ff ff ff ff  ff ff 00 00 00 00 44 42  |..............DB|

00084010  42 54 00 00 00 01 01 00  00 00 01 00 00 00 00 00  |BT..............|

00084020  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

*

BCH-ECC?:

00084200  00 00 00 00 00 00 00 00  00 00 37 a7 79 1c d7 41  |..........7.y..A|

00084210  c2 b0 99 0b c3 e1 c6 00  00 00 00 00 00 00 00 00  |................|

00084220  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

*

BCH-ECC?:

00084800  ff 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

00084810  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

00084820  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

00084830  00 92 2a bd 77 36 7e e7  bd 28 20 22 28 92 00 00  |..*.w6~..( "(...|

00084840  ff ff ff ff ff ff ff ff  ff ff ff ff ff ff ff ff  |................|

*

First BBTN: note the bad block index, 0xD0, on second line

00086100  00 ff ff ff ff ff ff ff  ff ff 00 00 00 00 01 00  |................|

00086110  00 00 d0 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

00086120  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

*

BCH-ECC?:

00086300  00 00 00 00 00 00 00 00  00 00 3d 5c c3 ed cd f2  |..........=\....|

00086310  e2 a6 67 37 70 8f 06 00  00 00 00 00 00 00 00 00  |..g7p...........|

00086320  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

*

BCH-ECC?:

00086900  ff 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

00086910  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

00086920  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

00086930  00 92 2a bd 77 36 7e e7  bd 28 20 22 28 92 00 00  |..*.w6~..( "(...|

00086940  ff ff ff ff ff ff ff ff  ff ff ff ff ff ff ff ff  |................|

*

Second DBBT header:

000a5000  00 ff ff ff ff ff ff ff  ff ff 00 00 00 00 44 42  |..............DB|

000a5010  42 54 00 00 00 01 01 00  00 00 01 00 00 00 00 00  |BT..............|

000a5020  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

*

BCH-ECC?:

000a5200  00 00 00 00 00 00 00 00  00 00 37 a7 79 1c d7 41  |..........7.y..A|

000a5210  c2 b0 99 0b c3 e1 c6 00  00 00 00 00 00 00 00 00  |................|

000a5220  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

*

BCH-ECC?:

000a5800  ff 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000a5810  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000a5830  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000a5830  00 92 2a bd 77 36 7e e7  bd 28 20 22 28 92 00 00  |..*.w6~..( "(...|

000a5840  ff ff ff ff ff ff ff ff  ff ff ff ff ff ff ff ff  |................|

*

Second BBTN:

000a7100  00 ff ff ff ff ff ff ff  ff ff 00 00 00 00 01 00  |................|

000a7110  00 00 d0 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000a7120  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

*

BCH-ECC?:

000a7300  00 00 00 00 00 00 00 00  00 00 3d 5c c3 ed cd f2  |..........=\....|

000a7310  e2 a6 67 37 70 8f 06 00  00 00 00 00 00 00 00 00  |..g7p...........|

000a7320  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

*

BCH-ECC?:

000a7900  ff 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000a7910  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000a7920  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000a7930  00 92 2a bd 77 36 7e e7  bd 28 20 22 28 92 00 00  |..*.w6~..( "(...|

000a7940  ff ff ff ff ff ff ff ff  ff ff ff ff ff ff ff ff  |................|

*

Third DBBT header:

000c6000  00 ff ff ff ff ff ff ff  ff ff 00 00 00 00 44 42  |..............DB|

000c6010  42 54 00 00 00 01 01 00  00 00 01 00 00 00 00 00  |BT..............|

000c6020  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

*

BCH-ECC?:

000c6200  00 00 00 00 00 00 00 00  00 00 37 a7 79 1c d7 41  |..........7.y..A|

000c6210  c2 b0 99 0b c3 e1 c6 00  00 00 00 00 00 00 00 00  |................|

000c6220  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

*

BCH-ECC?:

000c6800  ff 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000c6810  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000c6820  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000c6830  00 92 2a bd 77 36 7e e7  bd 28 20 22 28 92 00 00  |..*.w6~..( "(...|

000c6840  ff ff ff ff ff ff ff ff  ff ff ff ff ff ff ff ff  |................|

*

Third BBTN:

000c8100  00 ff ff ff ff ff ff ff  ff ff 00 00 00 00 01 00  |................|

000c8110  00 00 d0 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000c8120  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

*

BCH-ECC?:

000c8300  00 00 00 00 00 00 00 00  00 00 3d 5c c3 ed cd f2  |..........=\....|

000c8310  e2 a6 67 37 70 8f 06 00  00 00 00 00 00 00 00 00  |..g7p...........|

000c8320  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

*

BCH-ECC?:

000c8900  ff 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000c8910  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000c8920  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000c8930  00 92 2a bd 77 36 7e e7  bd 28 20 22 28 92 00 00  |..*.w6~..( "(...|

000c8940  ff ff ff ff ff ff ff ff  ff ff ff ff ff ff ff ff  |................|

*

Forth DBBT header:

000e7000  00 ff ff ff ff ff ff ff  ff ff 00 00 00 00 44 42  |..............DB|

000e7010  42 54 00 00 00 01 01 00  00 00 01 00 00 00 00 00  |BT..............|

000e7020  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

*

BCH-ECC?:

000e7200  00 00 00 00 00 00 00 00  00 00 37 a7 79 1c d7 41  |..........7.y..A|

000e7210  c2 b0 99 0b c3 e1 c6 00  00 00 00 00 00 00 00 00  |................|

000e7220  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

*

BCH-ECC?:

000e7800  ff 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000e7810  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000e7820  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000e7830  00 92 2a bd 77 36 7e e7  bd 28 20 22 28 92 00 00  |..*.w6~..( "(...|

000e7840  ff ff ff ff ff ff ff ff  ff ff ff ff ff ff ff ff  |................|

*

Forth BBTN:

000e9100  00 ff ff ff ff ff ff ff  ff ff 00 00 00 00 01 00  |................|

000e9110  00 00 d0 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000e9120  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

*

BCH-ECC?:

000e9300  00 00 00 00 00 00 00 00  00 00 3d 5c c3 ed cd f2  |..........=\....|

000e9310  e2 a6 67 37 70 8f 06 00  00 00 00 00 00 00 00 00  |..g7p...........|

000e9320  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

*

BCH-ECC?:

000e9900  ff 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000e9910  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000e9920  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

000e9930  00 92 2a bd 77 36 7e e7  bd 28 20 22 28 92 00 00  |..*.w6~..( "(...|

000e9940  ff ff ff ff ff ff ff ff  ff ff ff ff ff ff ff ff  |................|

*

00108000

标签 (1)
0 项奖励
回复
3 回复数

1,343 次查看
YixingKong
Senior Contributor IV

Stuart

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 项奖励
回复

1,343 次查看
YixingKong
Senior Contributor IV

Stuart

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 项奖励
回复

1,343 次查看
GraceH
Senior Contributor II

MX28 ROM code checks the bad block table in DBBT. Can you run "kobs-ng init -v $FILE" to dump the FCB structure?

In your DBBT header, DBBT fingerprint starts at byte 14.

First DBBT header:

00084000  00 ff ff ff ff ff ff ff  ff ff 00 00 00 00 44 42  |..............DB|

00084010  42 54 00 00 00 01 01 00  00 00 01 00 00 00 00 00  |BT..............|

00084020  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|

*


But the definition of boot block is 4 bytes checksum followed by 4 bytes fingerprint and 4 bytes version number.


typedef struct _BootBlockStruct_t

{

    uint32_t    m_u32Checksum;         //!< First fingerprint in first byte.

    uint32_t    m_u32FingerPrint;      //!< 2nd fingerprint at byte 4.

    uint32_t    m_u32Version;          //!< 3rd fingerprint at byte 8.

Grace

0 项奖励
回复