i.MX28 latest Linux kernel version

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX28 latest Linux kernel version

2,865 Views
sangilikumar
Contributor I

Hi

      We plan to use i.MX28 processor with Linux. Linux version is 2.6.35 its the final version or it have any latest kernel version ?

      We need higher kernel version above 3.x.x.

Thanks

Sangly

Labels (2)
0 Kudos
Reply
4 Replies

2,419 Views
Yuri
NXP Employee
NXP Employee

1.

L2.6.35_1.1.0 on the Web is the recent officially supported BSP.

2.

Perhaps it makes sense to try i.MX28 mainline kernel.

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_2.6.35_10.12.01


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,419 Views
lategoodbye
Senior Contributor I

Hi Sangly,

i would recommend to use the latest stable Linux version like 3.14.1.

0 Kudos
Reply

2,419 Views
sangilikumar
Contributor I

Hi

       Is't official and its available in Freescale GIT branch ?

0 Kudos
Reply

2,419 Views
lategoodbye
Senior Contributor I

If you think of official, that Freescale supports it: no as far as i know.

0 Kudos
Reply