i.MX28 i2c1 bus issue with last linux kernel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX28 i2c1 bus issue with last linux kernel

跳至解决方案
3,829 次查看
julienmorand
Contributor II

Hi community,

I have made a custom board with an i.MX287 processor. I'm currently using Yocto to compile and use the mainline kernel (3.12) / U-boot 2013.10.

Everything is working great so far (boot from SD card, SPI, USB, ethernet, i2c0) except the i2c1 bus.

I have enabled the i2c device interface to see my i2c busses in /dev.

Using the i2c-tools gives the following output:

i2cdetect -y -r 0

     0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f

00:          -- -- -- -- -- -- -- -- -- -- -- -- --

10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

20: 20 21 22 -- -- -- -- -- -- -- -- -- -- -- -- --

30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

70: -- -- -- -- -- -- -- --

For i2c1 bus I get a "Failed to get PIO reg. write descriptor." error.

Here is my device tree configuration:

  i2c0: i2c@80058000 {

       pinctrl-names = "default";

       pinctrl-0 = <&i2c0_pins_a>;

       status = "okay";

  };

  i2c1: i2c@8005a000 {

       pinctrl-names = "default";

       pinctrl-0 = <&i2c1_pins_a>;

       status = "okay";

  };*/

i2c1_pins_a: i2c1@0 {

     reg = <0>;

     fsl,pinmux-ids = <

     0x30a1 /* MX28_PAD_AUART2_CTS__I2C1_SCL

     0x30b1 /* MX28_PAD_AUART2_RTS__I2C1_SDA

     >;

     fsl,drive-strength = <1>;

     fsl,voltage = <1>;

     fsl,pull-up = <1>;

};

First I've tried these patches:

[PATCH 1/3 V2] i2c: mxs: distinguish i.MX23 and i.MX28 based I2C controller -- Linux I2C

[PATCH 2/3 V4] i2c: mxs: Rework the PIO mode operation -- Linux I2C

[PATCH 3/3 V3] i2c: mxs: Fix PIO mode on i.MX23 -- Linux I2C

But it's even worse...this time neither i2c0 nor i2c1 bus is working. I get a "PIO: Failed to send SELECT command!" error.

Finally, switching bus i2c1 to bit banging allow me to use it but clock frequency is around 35kHz.

i2c1 {

       compatible = "i2c-gpio";

       pinctrl-0 = <&i2c1_pins_gpio>;

       pinctrl-names = "default";

       gpios = <

            &gpio3 11 0 /* sda */

            &gpio3 10 0 /* scl */

       >;

       i2c-gpio,delay-us = <2>;

       #address-cells = <1>;

       #size-cells = <0>;

       status = "okay";

  };

It would be great to find a solution so we can use the i2c1 bus with the i2c-mxs driver.

Does anyone have any suggestions to help me correct this bug ?

Thanks a lot in advance for your time.

标签 (2)
0 项奖励
回复
1 解答
2,074 次查看
julienmorand
Contributor II

Hi community,

Turns out I was facing a GND issue on my custom board...

Here is my final dts file for those who are interested:

i2c0: i2c@80058000 {

          pinctrl-names = "default";

          pinctrl-0 = <&i2c0_pins_a>;

          status = "okay";

};

i2c1: i2c@8005a000 {

          pinctrl-names = "default";

          pinctrl-0 = <&i2c1_pins_a>;

          status = "okay";

};

i2c1_pins_a: i2c1@0 {

          reg = <0>;

          fsl,pinmux-ids = <

          0x30a1 /* MX28_PAD_AUART2_CTS__I2C1_SCL */

          0x30b1 /* MX28_PAD_AUART2_RTS__I2C1_SDA */

          >;

          fsl,drive-strength = <1>;

          fsl,voltage = <1>;

          fsl,pull-up = <1>;

};

Now both i2c0 and i2c1 busses work fine with i2c-mxs driver.

Bye.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,075 次查看
julienmorand
Contributor II

Hi community,

Turns out I was facing a GND issue on my custom board...

Here is my final dts file for those who are interested:

i2c0: i2c@80058000 {

          pinctrl-names = "default";

          pinctrl-0 = <&i2c0_pins_a>;

          status = "okay";

};

i2c1: i2c@8005a000 {

          pinctrl-names = "default";

          pinctrl-0 = <&i2c1_pins_a>;

          status = "okay";

};

i2c1_pins_a: i2c1@0 {

          reg = <0>;

          fsl,pinmux-ids = <

          0x30a1 /* MX28_PAD_AUART2_CTS__I2C1_SCL */

          0x30b1 /* MX28_PAD_AUART2_RTS__I2C1_SDA */

          >;

          fsl,drive-strength = <1>;

          fsl,voltage = <1>;

          fsl,pull-up = <1>;

};

Now both i2c0 and i2c1 busses work fine with i2c-mxs driver.

Bye.

0 项奖励
回复
2,074 次查看
artemkochetkov
Contributor I

Can You show Your kernel .config ?

0 项奖励
回复
2,074 次查看
julienmorand
Contributor II

Hi Artem,

Here's my kernel .config (sorry for the full copy/paste, can't find how to join a .txt file...) :

#

# Automatically generated file; DO NOT EDIT.

# Linux/arm 3.10.17 Kernel Configuration

#

CONFIG_ARM=y

CONFIG_HAVE_PWM=y

CONFIG_SYS_SUPPORTS_APM_EMULATION=y

CONFIG_HAVE_PROC_CPU=y

CONFIG_STACKTRACE_SUPPORT=y

CONFIG_HAVE_LATENCYTOP_SUPPORT=y

CONFIG_LOCKDEP_SUPPORT=y

CONFIG_TRACE_IRQFLAGS_SUPPORT=y

CONFIG_RWSEM_GENERIC_SPINLOCK=y

CONFIG_GENERIC_HWEIGHT=y

CONFIG_GENERIC_CALIBRATE_DELAY=y

CONFIG_NEED_DMA_MAP_STATE=y

CONFIG_VECTORS_BASE=0xffff0000

CONFIG_ARM_PATCH_PHYS_VIRT=y

CONFIG_GENERIC_BUG=y

CONFIG_DEFCONFIG_LIST="/lib/modules/$UNAME_RELEASE/.config"

CONFIG_IRQ_WORK=y

CONFIG_BUILDTIME_EXTABLE_SORT=y

#

# General setup

#

CONFIG_BROKEN_ON_SMP=y

CONFIG_INIT_ENV_ARG_LIMIT=32

CONFIG_CROSS_COMPILE=""

CONFIG_LOCALVERSION="-yocto-standard"

CONFIG_LOCALVERSION_AUTO=y

CONFIG_HAVE_KERNEL_GZIP=y

CONFIG_HAVE_KERNEL_LZMA=y

CONFIG_HAVE_KERNEL_XZ=y

CONFIG_HAVE_KERNEL_LZO=y

CONFIG_KERNEL_GZIP=y

# CONFIG_KERNEL_LZMA is not set

# CONFIG_KERNEL_XZ is not set

# CONFIG_KERNEL_LZO is not set

CONFIG_DEFAULT_HOSTNAME="(None)"

CONFIG_SWAP=y

CONFIG_SYSVIPC=y

CONFIG_SYSVIPC_SYSCTL=y

# CONFIG_POSIX_MQUEUE is not set

# CONFIG_FHANDLE is not set

# CONFIG_AUDIT is not set

CONFIG_HAVE_GENERIC_HARDIRQS=y

#

# IRQ subsystem

#

CONFIG_GENERIC_HARDIRQS=y

CONFIG_GENERIC_IRQ_PROBE=y

CONFIG_GENERIC_IRQ_SHOW=y

CONFIG_HARDIRQS_SW_RESEND=y

CONFIG_GENERIC_IRQ_CHIP=y

CONFIG_IRQ_DOMAIN=y

# CONFIG_IRQ_DOMAIN_DEBUG is not set

CONFIG_SPARSE_IRQ=y

CONFIG_KTIME_SCALAR=y

CONFIG_GENERIC_CLOCKEVENTS=y

CONFIG_GENERIC_CLOCKEVENTS_BUILD=y

#

# Timers subsystem

#

CONFIG_TICK_ONESHOT=y

CONFIG_NO_HZ_COMMON=y

# CONFIG_HZ_PERIODIC is not set

CONFIG_NO_HZ_IDLE=y

CONFIG_NO_HZ=y

CONFIG_HIGH_RES_TIMERS=y

#

# CPU/Task time and stats accounting

#

CONFIG_TICK_CPU_ACCOUNTING=y

# CONFIG_IRQ_TIME_ACCOUNTING is not set

# CONFIG_BSD_PROCESS_ACCT is not set

CONFIG_TASKSTATS=y

CONFIG_TASK_DELAY_ACCT=y

CONFIG_TASK_XACCT=y

CONFIG_TASK_IO_ACCOUNTING=y

#

# RCU Subsystem

#

CONFIG_TINY_RCU=y

# CONFIG_PREEMPT_RCU is not set

# CONFIG_RCU_STALL_COMMON is not set

# CONFIG_TREE_RCU_TRACE is not set

CONFIG_IKCONFIG=y

CONFIG_IKCONFIG_PROC=y

CONFIG_LOG_BUF_SHIFT=17

# CONFIG_CGROUPS is not set

# CONFIG_CHECKPOINT_RESTORE is not set

CONFIG_NAMESPACES=y

# CONFIG_UTS_NS is not set

# CONFIG_IPC_NS is not set

# CONFIG_USER_NS is not set

# CONFIG_PID_NS is not set

# CONFIG_NET_NS is not set

CONFIG_UIDGID_CONVERTED=y

# CONFIG_UIDGID_STRICT_TYPE_CHECKS is not set

# CONFIG_SCHED_AUTOGROUP is not set

# CONFIG_SYSFS_DEPRECATED is not set

CONFIG_RELAY=y

# CONFIG_BLK_DEV_INITRD is not set

# CONFIG_CC_OPTIMIZE_FOR_SIZE is not set

CONFIG_SYSCTL=y

CONFIG_ANON_INODES=y

CONFIG_HAVE_UID16=y

CONFIG_HOTPLUG=y

CONFIG_EXPERT=y

# CONFIG_UPTIME_LIMITED_KERNEL is not set

CONFIG_UID16=y

# CONFIG_SYSCTL_SYSCALL is not set

CONFIG_KALLSYMS=y

CONFIG_KALLSYMS_ALL=y

CONFIG_PRINTK=y

CONFIG_BUG=y

CONFIG_ELF_CORE=y

CONFIG_BASE_FULL=y

CONFIG_FUTEX=y

CONFIG_EPOLL=y

CONFIG_SIGNALFD=y

CONFIG_TIMERFD=y

CONFIG_EVENTFD=y

CONFIG_SHMEM=y

CONFIG_AIO=y

CONFIG_EMBEDDED=y

CONFIG_HAVE_PERF_EVENTS=y

CONFIG_PERF_USE_VMALLOC=y

#

# Kernel Performance Events And Counters

#

CONFIG_PERF_EVENTS=y

# CONFIG_DEBUG_PERF_USE_VMALLOC is not set

CONFIG_VM_EVENT_COUNTERS=y

CONFIG_SLUB_DEBUG=y

# CONFIG_COMPAT_BRK is not set

# CONFIG_SLAB is not set

CONFIG_SLUB=y

# CONFIG_SLOB is not set

# CONFIG_PROFILING is not set

CONFIG_TRACEPOINTS=y

CONFIG_HAVE_OPROFILE=y

# CONFIG_KPROBES is not set

# CONFIG_JUMP_LABEL is not set

# CONFIG_HAVE_64BIT_ALIGNED_ACCESS is not set

CONFIG_HAVE_KPROBES=y

CONFIG_HAVE_KRETPROBES=y

CONFIG_HAVE_ARCH_TRACEHOOK=y

CONFIG_HAVE_DMA_ATTRS=y

CONFIG_HAVE_DMA_CONTIGUOUS=y

CONFIG_GENERIC_SMP_IDLE_THREAD=y

CONFIG_GENERIC_IDLE_POLL_SETUP=y

CONFIG_HAVE_REGS_AND_STACK_ACCESS_API=y

CONFIG_HAVE_CLK=y

CONFIG_HAVE_DMA_API_DEBUG=y

CONFIG_HAVE_ARCH_JUMP_LABEL=y

CONFIG_ARCH_WANT_IPC_PARSE_VERSION=y

CONFIG_HAVE_ARCH_SECCOMP_FILTER=y

CONFIG_HAVE_CONTEXT_TRACKING=y

CONFIG_HAVE_IRQ_TIME_ACCOUNTING=y

CONFIG_HAVE_MOD_ARCH_SPECIFIC=y

CONFIG_MODULES_USE_ELF_REL=y

CONFIG_CLONE_BACKWARDS=y

CONFIG_OLD_SIGSUSPEND3=y

CONFIG_OLD_SIGACTION=y

#

# GCOV-based kernel profiling

#

# CONFIG_GCOV_KERNEL is not set

CONFIG_HAVE_GENERIC_DMA_COHERENT=y

CONFIG_SLABINFO=y

CONFIG_RT_MUTEXES=y

CONFIG_BASE_SMALL=0

CONFIG_MODULES=y

CONFIG_MODULE_FORCE_LOAD=y

CONFIG_MODULE_UNLOAD=y

CONFIG_MODULE_FORCE_UNLOAD=y

CONFIG_MODVERSIONS=y

# CONFIG_MODULE_SRCVERSION_ALL is not set

# CONFIG_MODULE_SIG is not set

CONFIG_BLOCK=y

CONFIG_LBDAF=y

CONFIG_BLK_DEV_BSG=y

# CONFIG_BLK_DEV_BSGLIB is not set

CONFIG_BLK_DEV_INTEGRITY=y

#

# Partition Types

#

# CONFIG_PARTITION_ADVANCED is not set

CONFIG_MSDOS_PARTITION=y

CONFIG_EFI_PARTITION=y

#

# IO Schedulers

#

CONFIG_IOSCHED_NOOP=y

# CONFIG_IOSCHED_DEADLINE is not set

# CONFIG_IOSCHED_CFQ is not set

CONFIG_DEFAULT_NOOP=y

CONFIG_DEFAULT_IOSCHED="noop"

CONFIG_UNINLINE_SPIN_UNLOCK=y

CONFIG_FREEZER=y

#

# System Type

#

CONFIG_MMU=y

CONFIG_ARCH_MULTIPLATFORM=y

# CONFIG_ARCH_INTEGRATOR is not set

# CONFIG_ARCH_REALVIEW is not set

# CONFIG_ARCH_VERSATILE is not set

# CONFIG_ARCH_AT91 is not set

# CONFIG_ARCH_CLPS711X is not set

# CONFIG_ARCH_GEMINI is not set

# CONFIG_ARCH_EBSA110 is not set

# CONFIG_ARCH_EP93XX is not set

# CONFIG_ARCH_FOOTBRIDGE is not set

# CONFIG_ARCH_NETX is not set

# CONFIG_ARCH_IOP13XX is not set

# CONFIG_ARCH_IOP32X is not set

# CONFIG_ARCH_IOP33X is not set

# CONFIG_ARCH_IXP4XX is not set

# CONFIG_ARCH_DOVE is not set

# CONFIG_ARCH_KIRKWOOD is not set

# CONFIG_ARCH_MV78XX0 is not set

# CONFIG_ARCH_ORION5X is not set

# CONFIG_ARCH_MMP is not set

# CONFIG_ARCH_KS8695 is not set

# CONFIG_ARCH_W90X900 is not set

# CONFIG_ARCH_LPC32XX is not set

# CONFIG_ARCH_PXA is not set

# CONFIG_ARCH_MSM is not set

# CONFIG_ARCH_SHMOBILE is not set

# CONFIG_ARCH_RPC is not set

# CONFIG_ARCH_SA1100 is not set

# CONFIG_ARCH_S3C24XX is not set

# CONFIG_ARCH_S3C64XX is not set

# CONFIG_ARCH_S5P64X0 is not set

# CONFIG_ARCH_S5PC100 is not set

# CONFIG_ARCH_S5PV210 is not set

# CONFIG_ARCH_EXYNOS is not set

# CONFIG_ARCH_SHARK is not set

# CONFIG_ARCH_U300 is not set

# CONFIG_ARCH_DAVINCI is not set

# CONFIG_ARCH_OMAP1 is not set

#

# Multiple platform selection

#

#

# CPU Core family selection

#

# CONFIG_ARCH_MULTI_V4 is not set

# CONFIG_ARCH_MULTI_V4T is not set

CONFIG_ARCH_MULTI_V5=y

CONFIG_ARCH_MULTI_V4_V5=y

# CONFIG_ARCH_MULTI_V6 is not set

# CONFIG_ARCH_MULTI_V7 is not set

CONFIG_ARCH_MULTI_CPU_AUTO=y

# CONFIG_GPIO_PCA953X is not set

# CONFIG_ARCH_MXC is not set

CONFIG_SOC_IMX23=y

CONFIG_SOC_IMX28=y

CONFIG_ARCH_MXS=y

# CONFIG_ARCH_NOMADIK is not set

# CONFIG_PLAT_SPEAR is not set

# CONFIG_ARCH_WM8505 is not set

#

# Processor Type

#

CONFIG_CPU_ARM926T=y

CONFIG_CPU_32v5=y

CONFIG_CPU_ABRT_EV5TJ=y

CONFIG_CPU_PABRT_LEGACY=y

CONFIG_CPU_CACHE_VIVT=y

CONFIG_CPU_COPY_V4WB=y

CONFIG_CPU_TLB_V4WBI=y

CONFIG_CPU_CP15=y

CONFIG_CPU_CP15_MMU=y

CONFIG_CPU_USE_DOMAINS=y

#

# Processor Features

#

# CONFIG_ARCH_PHYS_ADDR_T_64BIT is not set

# CONFIG_ARM_THUMB is not set

# CONFIG_CPU_ICACHE_DISABLE is not set

# CONFIG_CPU_DCACHE_DISABLE is not set

# CONFIG_CPU_DCACHE_WRITETHROUGH is not set

# CONFIG_CPU_CACHE_ROUND_ROBIN is not set

CONFIG_NEED_KUSER_HELPERS=y

CONFIG_KUSER_HELPERS=y

# CONFIG_CACHE_L2X0 is not set

CONFIG_ARM_L1_CACHE_SHIFT=5

CONFIG_ARM_NR_BANKS=8

CONFIG_MULTI_IRQ_HANDLER=y

#

# Bus support

#

CONFIG_ARM_AMBA=y

# CONFIG_PCI_SYSCALL is not set

# CONFIG_PCCARD is not set

#

# Kernel Features

#

CONFIG_VMSPLIT_3G=y

# CONFIG_VMSPLIT_2G is not set

# CONFIG_VMSPLIT_1G is not set

CONFIG_PAGE_OFFSET=0xC0000000

CONFIG_ARCH_NR_GPIO=0

# CONFIG_PREEMPT_NONE is not set

CONFIG_PREEMPT_VOLUNTARY=y

# CONFIG_PREEMPT is not set

CONFIG_HZ=100

CONFIG_SCHED_HRTICK=y

CONFIG_AEABI=y

CONFIG_OABI_COMPAT=y

# CONFIG_ARCH_SPARSEMEM_DEFAULT is not set

# CONFIG_ARCH_SELECT_MEMORY_MODEL is not set

CONFIG_HAVE_ARCH_PFN_VALID=y

# CONFIG_HIGHMEM is not set

CONFIG_HW_PERF_EVENTS=y

CONFIG_FLATMEM=y

CONFIG_FLAT_NODE_MEM_MAP=y

CONFIG_HAVE_MEMBLOCK=y

# CONFIG_HAVE_BOOTMEM_INFO_NODE is not set

CONFIG_PAGEFLAGS_EXTENDED=y

CONFIG_SPLIT_PTLOCK_CPUS=999999

CONFIG_COMPACTION=y

CONFIG_MIGRATION=y

# CONFIG_PHYS_ADDR_T_64BIT is not set

CONFIG_ZONE_DMA_FLAG=0

CONFIG_NEED_BOUNCE_POOL=y

# CONFIG_KSM is not set

CONFIG_DEFAULT_MMAP_MIN_ADDR=4096

CONFIG_CROSS_MEMORY_ATTACH=y

CONFIG_NEED_PER_CPU_KM=y

# CONFIG_CLEANCACHE is not set

# CONFIG_FRONTSWAP is not set

CONFIG_FORCE_MAX_ZONEORDER=11

CONFIG_ALIGNMENT_TRAP=y

# CONFIG_UACCESS_WITH_MEMCPY is not set

# CONFIG_SECCOMP is not set

# CONFIG_CC_STACKPROTECTOR is not set

#

# Boot options

#

CONFIG_USE_OF=y

CONFIG_ATAGS=y

# CONFIG_DEPRECATED_PARAM_STRUCT is not set

CONFIG_ZBOOT_ROM_TEXT=0x0

CONFIG_ZBOOT_ROM_BSS=0x0

# CONFIG_ARM_APPENDED_DTB is not set

CONFIG_CMDLINE=""

# CONFIG_KEXEC is not set

# CONFIG_CRASH_DUMP is not set

CONFIG_AUTO_ZRELADDR=y

#

# CPU Power Management

#

# CONFIG_CPU_IDLE is not set

# CONFIG_ARCH_NEEDS_CPU_IDLE_COUPLED is not set

#

# Floating point emulation

#

#

# At least one emulation must be selected

#

CONFIG_FPE_NWFPE=y

# CONFIG_FPE_NWFPE_XP is not set

# CONFIG_FPE_FASTFPE is not set

# CONFIG_VFP is not set

#

# Userspace binary formats

#

CONFIG_BINFMT_ELF=y

CONFIG_ARCH_BINFMT_ELF_RANDOMIZE_PIE=y

CONFIG_CORE_DUMP_DEFAULT_ELF_HEADERS=y

CONFIG_BINFMT_SCRIPT=y

# CONFIG_HAVE_AOUT is not set

# CONFIG_BINFMT_MISC is not set

CONFIG_COREDUMP=y

#

# Power management options

#

CONFIG_SUSPEND=y

CONFIG_SUSPEND_FREEZER=y

CONFIG_PM_SLEEP=y

# CONFIG_PM_AUTOSLEEP is not set

# CONFIG_PM_WAKELOCKS is not set

# CONFIG_PM_RUNTIME is not set

CONFIG_PM=y

# CONFIG_PM_DEBUG is not set

# CONFIG_APM_EMULATION is not set

CONFIG_PM_CLK=y

CONFIG_CPU_PM=y

CONFIG_ARCH_SUSPEND_POSSIBLE=y

CONFIG_ARM_CPU_SUSPEND=y

CONFIG_NET=y

#

# Networking options

#

CONFIG_PACKET=y

# CONFIG_PACKET_DIAG is not set

CONFIG_UNIX=y

# CONFIG_UNIX_DIAG is not set

CONFIG_XFRM=y

# CONFIG_XFRM_USER is not set

# CONFIG_XFRM_SUB_POLICY is not set

# CONFIG_XFRM_MIGRATE is not set

# CONFIG_XFRM_STATISTICS is not set

# CONFIG_NET_KEY is not set

CONFIG_INET=y

# CONFIG_IP_MULTICAST is not set

# CONFIG_IP_ADVANCED_ROUTER is not set

CONFIG_IP_ROUTE_CLASSID=y

CONFIG_IP_PNP=y

CONFIG_IP_PNP_DHCP=y

# CONFIG_IP_PNP_BOOTP is not set

# CONFIG_IP_PNP_RARP is not set

# CONFIG_NET_IPIP is not set

# CONFIG_NET_IPGRE_DEMUX is not set

CONFIG_NET_IP_TUNNEL=y

# CONFIG_ARPD is not set

CONFIG_SYN_COOKIES=y

# CONFIG_INET_AH is not set

# CONFIG_INET_ESP is not set

# CONFIG_INET_IPCOMP is not set

# CONFIG_INET_XFRM_TUNNEL is not set

CONFIG_INET_TUNNEL=y

# CONFIG_INET_XFRM_MODE_TRANSPORT is not set

# CONFIG_INET_XFRM_MODE_TUNNEL is not set

# CONFIG_INET_XFRM_MODE_BEET is not set

CONFIG_INET_LRO=y

# CONFIG_INET_DIAG is not set

# CONFIG_TCP_CONG_ADVANCED is not set

CONFIG_TCP_CONG_CUBIC=y

CONFIG_DEFAULT_TCP_CONG="cubic"

# CONFIG_TCP_MD5SIG is not set

CONFIG_IPV6=y

# CONFIG_IPV6_PRIVACY is not set

# CONFIG_IPV6_ROUTER_PREF is not set

# CONFIG_IPV6_OPTIMISTIC_DAD is not set

# CONFIG_INET6_AH is not set

# CONFIG_INET6_ESP is not set

# CONFIG_INET6_IPCOMP is not set

# CONFIG_IPV6_MIP6 is not set

# CONFIG_INET6_XFRM_TUNNEL is not set

# CONFIG_INET6_TUNNEL is not set

CONFIG_INET6_XFRM_MODE_TRANSPORT=y

CONFIG_INET6_XFRM_MODE_TUNNEL=y

CONFIG_INET6_XFRM_MODE_BEET=y

# CONFIG_INET6_XFRM_MODE_ROUTEOPTIMIZATION is not set

CONFIG_IPV6_SIT=y

# CONFIG_IPV6_SIT_6RD is not set

CONFIG_IPV6_NDISC_NODETYPE=y

# CONFIG_IPV6_TUNNEL is not set

# CONFIG_IPV6_GRE is not set

# CONFIG_IPV6_MULTIPLE_TABLES is not set

# CONFIG_IPV6_MROUTE is not set

# CONFIG_NETWORK_SECMARK is not set

# CONFIG_NETWORK_PHY_TIMESTAMPING is not set

CONFIG_NETFILTER=y

# CONFIG_NETFILTER_DEBUG is not set

CONFIG_NETFILTER_ADVANCED=y

#

# Core Netfilter Configuration

#

CONFIG_NETFILTER_NETLINK=m

CONFIG_NETFILTER_NETLINK_ACCT=m

CONFIG_NETFILTER_NETLINK_QUEUE=m

CONFIG_NETFILTER_NETLINK_LOG=m

CONFIG_NF_CONNTRACK=m

CONFIG_NF_CONNTRACK_MARK=y

CONFIG_NF_CONNTRACK_ZONES=y

CONFIG_NF_CONNTRACK_PROCFS=y

CONFIG_NF_CONNTRACK_EVENTS=y

CONFIG_NF_CONNTRACK_TIMEOUT=y

CONFIG_NF_CONNTRACK_TIMESTAMP=y

CONFIG_NF_CONNTRACK_LABELS=y

CONFIG_NF_CT_PROTO_DCCP=m

CONFIG_NF_CT_PROTO_GRE=m

CONFIG_NF_CT_PROTO_SCTP=m

CONFIG_NF_CT_PROTO_UDPLITE=m

CONFIG_NF_CONNTRACK_AMANDA=m

CONFIG_NF_CONNTRACK_FTP=m

CONFIG_NF_CONNTRACK_H323=m

CONFIG_NF_CONNTRACK_IRC=m

CONFIG_NF_CONNTRACK_BROADCAST=m

CONFIG_NF_CONNTRACK_NETBIOS_NS=m

CONFIG_NF_CONNTRACK_SNMP=m

CONFIG_NF_CONNTRACK_PPTP=m

CONFIG_NF_CONNTRACK_SANE=m

CONFIG_NF_CONNTRACK_SIP=m

CONFIG_NF_CONNTRACK_TFTP=m

CONFIG_NF_CT_NETLINK=m

CONFIG_NF_CT_NETLINK_TIMEOUT=m

# CONFIG_NF_CT_NETLINK_HELPER is not set

CONFIG_NETFILTER_NETLINK_QUEUE_CT=y

CONFIG_NF_NAT=m

CONFIG_NF_NAT_NEEDED=y

CONFIG_NF_NAT_PROTO_DCCP=m

CONFIG_NF_NAT_PROTO_UDPLITE=m

CONFIG_NF_NAT_PROTO_SCTP=m

CONFIG_NF_NAT_AMANDA=m

CONFIG_NF_NAT_FTP=m

CONFIG_NF_NAT_IRC=m

CONFIG_NF_NAT_SIP=m

CONFIG_NF_NAT_TFTP=m

# CONFIG_NETFILTER_TPROXY is not set

CONFIG_NETFILTER_XTABLES=m

#

# Xtables combined modules

#

CONFIG_NETFILTER_XT_MARK=m

CONFIG_NETFILTER_XT_CONNMARK=m

#

# Xtables targets

#

CONFIG_NETFILTER_XT_TARGET_CHECKSUM=m

CONFIG_NETFILTER_XT_TARGET_CLASSIFY=m

CONFIG_NETFILTER_XT_TARGET_CONNMARK=m

CONFIG_NETFILTER_XT_TARGET_CT=m

CONFIG_NETFILTER_XT_TARGET_DSCP=m

CONFIG_NETFILTER_XT_TARGET_HL=m

CONFIG_NETFILTER_XT_TARGET_HMARK=m

CONFIG_NETFILTER_XT_TARGET_IDLETIMER=m

CONFIG_NETFILTER_XT_TARGET_LOG=m

CONFIG_NETFILTER_XT_TARGET_MARK=m

CONFIG_NETFILTER_XT_TARGET_NETMAP=m

CONFIG_NETFILTER_XT_TARGET_NFLOG=m

CONFIG_NETFILTER_XT_TARGET_NFQUEUE=m

CONFIG_NETFILTER_XT_TARGET_NOTRACK=m

CONFIG_NETFILTER_XT_TARGET_RATEEST=m

CONFIG_NETFILTER_XT_TARGET_REDIRECT=m

CONFIG_NETFILTER_XT_TARGET_TEE=m

CONFIG_NETFILTER_XT_TARGET_TRACE=m

CONFIG_NETFILTER_XT_TARGET_TCPMSS=m

CONFIG_NETFILTER_XT_TARGET_TCPOPTSTRIP=m

#

# Xtables matches

#

CONFIG_NETFILTER_XT_MATCH_ADDRTYPE=m

CONFIG_NETFILTER_XT_MATCH_BPF=m

CONFIG_NETFILTER_XT_MATCH_CLUSTER=m

CONFIG_NETFILTER_XT_MATCH_COMMENT=m

CONFIG_NETFILTER_XT_MATCH_CONNBYTES=m

CONFIG_NETFILTER_XT_MATCH_CONNLABEL=m

CONFIG_NETFILTER_XT_MATCH_CONNLIMIT=m

CONFIG_NETFILTER_XT_MATCH_CONNMARK=m

CONFIG_NETFILTER_XT_MATCH_CONNTRACK=m

CONFIG_NETFILTER_XT_MATCH_CPU=m

CONFIG_NETFILTER_XT_MATCH_DCCP=m

CONFIG_NETFILTER_XT_MATCH_DEVGROUP=m

CONFIG_NETFILTER_XT_MATCH_DSCP=m

CONFIG_NETFILTER_XT_MATCH_ECN=m

CONFIG_NETFILTER_XT_MATCH_ESP=m

CONFIG_NETFILTER_XT_MATCH_HASHLIMIT=m

CONFIG_NETFILTER_XT_MATCH_HELPER=m

CONFIG_NETFILTER_XT_MATCH_HL=m

CONFIG_NETFILTER_XT_MATCH_IPRANGE=m

CONFIG_NETFILTER_XT_MATCH_LENGTH=m

CONFIG_NETFILTER_XT_MATCH_LIMIT=m

CONFIG_NETFILTER_XT_MATCH_MAC=m

CONFIG_NETFILTER_XT_MATCH_MARK=m

CONFIG_NETFILTER_XT_MATCH_MULTIPORT=m

CONFIG_NETFILTER_XT_MATCH_NFACCT=m

# CONFIG_NETFILTER_XT_MATCH_OSF is not set

CONFIG_NETFILTER_XT_MATCH_OWNER=m

CONFIG_NETFILTER_XT_MATCH_POLICY=m

CONFIG_NETFILTER_XT_MATCH_PKTTYPE=m

CONFIG_NETFILTER_XT_MATCH_QUOTA=m

CONFIG_NETFILTER_XT_MATCH_RATEEST=m

CONFIG_NETFILTER_XT_MATCH_REALM=m

CONFIG_NETFILTER_XT_MATCH_RECENT=m

CONFIG_NETFILTER_XT_MATCH_SCTP=m

CONFIG_NETFILTER_XT_MATCH_STATE=m

CONFIG_NETFILTER_XT_MATCH_STATISTIC=m

CONFIG_NETFILTER_XT_MATCH_STRING=m

CONFIG_NETFILTER_XT_MATCH_TCPMSS=m

CONFIG_NETFILTER_XT_MATCH_TIME=m

CONFIG_NETFILTER_XT_MATCH_U32=m

# CONFIG_IP_SET is not set

# CONFIG_IP_VS is not set

#

# IP: Netfilter Configuration

#

CONFIG_NF_DEFRAG_IPV4=m

CONFIG_NF_CONNTRACK_IPV4=m

CONFIG_NF_CONNTRACK_PROC_COMPAT=y

CONFIG_IP_NF_IPTABLES=m

CONFIG_IP_NF_MATCH_AH=m

CONFIG_IP_NF_MATCH_ECN=m

CONFIG_IP_NF_MATCH_RPFILTER=m

CONFIG_IP_NF_MATCH_TTL=m

CONFIG_IP_NF_FILTER=m

CONFIG_IP_NF_TARGET_REJECT=m

CONFIG_IP_NF_TARGET_ULOG=m

CONFIG_NF_NAT_IPV4=m

CONFIG_IP_NF_TARGET_MASQUERADE=m

CONFIG_IP_NF_TARGET_NETMAP=m

CONFIG_IP_NF_TARGET_REDIRECT=m

CONFIG_NF_NAT_SNMP_BASIC=m

CONFIG_NF_NAT_PROTO_GRE=m

CONFIG_NF_NAT_PPTP=m

CONFIG_NF_NAT_H323=m

CONFIG_IP_NF_MANGLE=m

CONFIG_IP_NF_TARGET_CLUSTERIP=m

CONFIG_IP_NF_TARGET_ECN=m

CONFIG_IP_NF_TARGET_TTL=m

CONFIG_IP_NF_RAW=m

CONFIG_IP_NF_ARPTABLES=m

CONFIG_IP_NF_ARPFILTER=m

CONFIG_IP_NF_ARP_MANGLE=m

#

# IPv6: Netfilter Configuration

#

CONFIG_NF_DEFRAG_IPV6=m

CONFIG_NF_CONNTRACK_IPV6=m

CONFIG_IP6_NF_IPTABLES=m

CONFIG_IP6_NF_MATCH_AH=m

CONFIG_IP6_NF_MATCH_EUI64=m

CONFIG_IP6_NF_MATCH_FRAG=m

CONFIG_IP6_NF_MATCH_OPTS=m

CONFIG_IP6_NF_MATCH_HL=m

CONFIG_IP6_NF_MATCH_IPV6HEADER=m

CONFIG_IP6_NF_MATCH_MH=m

CONFIG_IP6_NF_MATCH_RPFILTER=m

CONFIG_IP6_NF_MATCH_RT=m

CONFIG_IP6_NF_TARGET_HL=m

CONFIG_IP6_NF_FILTER=m

CONFIG_IP6_NF_TARGET_REJECT=m

CONFIG_IP6_NF_MANGLE=m

CONFIG_IP6_NF_RAW=m

CONFIG_NF_NAT_IPV6=m

CONFIG_IP6_NF_TARGET_MASQUERADE=m

CONFIG_IP6_NF_TARGET_NPT=m

# CONFIG_IP_DCCP is not set

# CONFIG_IP_SCTP is not set

# CONFIG_RDS is not set

# CONFIG_TIPC is not set

# CONFIG_ATM is not set

# CONFIG_L2TP is not set

# CONFIG_BRIDGE is not set

CONFIG_HAVE_NET_DSA=y

# CONFIG_VLAN_8021Q is not set

# CONFIG_DECNET is not set

# CONFIG_LLC2 is not set

# CONFIG_IPX is not set

# CONFIG_ATALK is not set

# CONFIG_X25 is not set

# CONFIG_LAPB is not set

# CONFIG_PHONET is not set

# CONFIG_IEEE802154 is not set

CONFIG_NET_SCHED=y

#

# Queueing/Scheduling

#

# CONFIG_NET_SCH_CBQ is not set

# CONFIG_NET_SCH_HTB is not set

# CONFIG_NET_SCH_HFSC is not set

# CONFIG_NET_SCH_PRIO is not set

# CONFIG_NET_SCH_MULTIQ is not set

# CONFIG_NET_SCH_RED is not set

# CONFIG_NET_SCH_SFB is not set

# CONFIG_NET_SCH_SFQ is not set

# CONFIG_NET_SCH_TEQL is not set

# CONFIG_NET_SCH_TBF is not set

# CONFIG_NET_SCH_GRED is not set

# CONFIG_NET_SCH_DSMARK is not set

# CONFIG_NET_SCH_NETEM is not set

# CONFIG_NET_SCH_DRR is not set

# CONFIG_NET_SCH_MQPRIO is not set

# CONFIG_NET_SCH_CHOKE is not set

# CONFIG_NET_SCH_QFQ is not set

# CONFIG_NET_SCH_CODEL is not set

# CONFIG_NET_SCH_FQ_CODEL is not set

# CONFIG_NET_SCH_PLUG is not set

#

# Classification

#

# CONFIG_NET_CLS_BASIC is not set

# CONFIG_NET_CLS_TCINDEX is not set

# CONFIG_NET_CLS_ROUTE4 is not set

# CONFIG_NET_CLS_FW is not set

# CONFIG_NET_CLS_U32 is not set

# CONFIG_NET_CLS_RSVP is not set

# CONFIG_NET_CLS_RSVP6 is not set

# CONFIG_NET_CLS_FLOW is not set

# CONFIG_NET_EMATCH is not set

# CONFIG_NET_CLS_ACT is not set

CONFIG_NET_SCH_FIFO=y

# CONFIG_DCB is not set

CONFIG_DNS_RESOLVER=y

# CONFIG_BATMAN_ADV is not set

# CONFIG_OPENVSWITCH is not set

# CONFIG_VSOCKETS is not set

# CONFIG_NETLINK_MMAP is not set

# CONFIG_NETLINK_DIAG is not set

CONFIG_BQL=y

# CONFIG_BPF_JIT is not set

#

# Network testing

#

# CONFIG_NET_PKTGEN is not set

# CONFIG_NET_DROP_MONITOR is not set

# CONFIG_HAMRADIO is not set

# CONFIG_CAN is not set

# CONFIG_IRDA is not set

# CONFIG_BT is not set

# CONFIG_AF_RXRPC is not set

# CONFIG_WIRELESS is not set

# CONFIG_WIMAX is not set

# CONFIG_RFKILL is not set

# CONFIG_RFKILL_REGULATOR is not set

# CONFIG_NET_9P is not set

# CONFIG_CAIF is not set

# CONFIG_CEPH_LIB is not set

# CONFIG_NFC is not set

CONFIG_HAVE_BPF_JIT=y

#

# Device Drivers

#

#

# Generic Driver Options

#

CONFIG_UEVENT_HELPER_PATH=""

CONFIG_DEVTMPFS=y

CONFIG_DEVTMPFS_MOUNT=y

CONFIG_STANDALONE=y

CONFIG_PREVENT_FIRMWARE_BUILD=y

CONFIG_FW_LOADER=y

# CONFIG_FIRMWARE_IN_KERNEL is not set

CONFIG_EXTRA_FIRMWARE=""

CONFIG_FW_LOADER_USER_HELPER=y

# CONFIG_DEBUG_DRIVER is not set

# CONFIG_DEBUG_DEVRES is not set

# CONFIG_SYS_HYPERVISOR is not set

# CONFIG_GENERIC_CPU_DEVICES is not set

# CONFIG_DMA_SHARED_BUFFER is not set

# CONFIG_CMA is not set

#

# Bus devices

#

# CONFIG_CONNECTOR is not set

CONFIG_MTD=y

# CONFIG_MTD_TESTS is not set

# CONFIG_MTD_REDBOOT_PARTS is not set

CONFIG_MTD_CMDLINE_PARTS=y

# CONFIG_MTD_AFS_PARTS is not set

CONFIG_MTD_OF_PARTS=y

# CONFIG_MTD_AR7_PARTS is not set

#

# User Modules And Translation Layers

#

CONFIG_MTD_BLKDEVS=y

CONFIG_MTD_BLOCK=y

# CONFIG_FTL is not set

# CONFIG_NFTL is not set

# CONFIG_INFTL is not set

# CONFIG_RFD_FTL is not set

# CONFIG_SSFDC is not set

# CONFIG_SM_FTL is not set

# CONFIG_MTD_OOPS is not set

# CONFIG_MTD_SWAP is not set

#

# RAM/ROM/Flash chip drivers

#

# CONFIG_MTD_CFI is not set

# CONFIG_MTD_JEDECPROBE is not set

CONFIG_MTD_MAP_BANK_WIDTH_1=y

CONFIG_MTD_MAP_BANK_WIDTH_2=y

CONFIG_MTD_MAP_BANK_WIDTH_4=y

# CONFIG_MTD_MAP_BANK_WIDTH_8 is not set

# CONFIG_MTD_MAP_BANK_WIDTH_16 is not set

# CONFIG_MTD_MAP_BANK_WIDTH_32 is not set

CONFIG_MTD_CFI_I1=y

CONFIG_MTD_CFI_I2=y

# CONFIG_MTD_CFI_I4 is not set

# CONFIG_MTD_CFI_I8 is not set

# CONFIG_MTD_RAM is not set

# CONFIG_MTD_ROM is not set

# CONFIG_MTD_ABSENT is not set

#

# Mapping drivers for chip access

#

# CONFIG_MTD_COMPLEX_MAPPINGS is not set

# CONFIG_MTD_PLATRAM is not set

#

# Self-contained MTD device drivers

#

CONFIG_MTD_DATAFLASH=y

# CONFIG_MTD_DATAFLASH_WRITE_VERIFY is not set

# CONFIG_MTD_DATAFLASH_OTP is not set

CONFIG_MTD_M25P80=y

# CONFIG_M25PXX_USE_FAST_READ is not set

CONFIG_MTD_SST25L=y

# CONFIG_MTD_SLRAM is not set

# CONFIG_MTD_PHRAM is not set

# CONFIG_MTD_MTDRAM is not set

# CONFIG_MTD_BLOCK2MTD is not set

#

# Disk-On-Chip Device Drivers

#

# CONFIG_MTD_DOCG3 is not set

CONFIG_MTD_NAND_ECC=y

# CONFIG_MTD_NAND_ECC_SMC is not set

CONFIG_MTD_NAND=y

# CONFIG_MTD_NAND_ECC_BCH is not set

# CONFIG_MTD_SM_COMMON is not set

# CONFIG_MTD_NAND_DENALI is not set

# CONFIG_MTD_NAND_GPIO is not set

CONFIG_MTD_NAND_IDS=y

# CONFIG_MTD_NAND_DISKONCHIP is not set

# CONFIG_MTD_NAND_DOCG4 is not set

# CONFIG_MTD_NAND_NANDSIM is not set

CONFIG_MTD_NAND_GPMI_NAND=y

# CONFIG_MTD_NAND_PLATFORM is not set

# CONFIG_MTD_ALAUDA is not set

# CONFIG_MTD_ONENAND is not set

#

# LPDDR flash memory drivers

#

# CONFIG_MTD_LPDDR is not set

CONFIG_MTD_UBI=y

CONFIG_MTD_UBI_WL_THRESHOLD=4096

CONFIG_MTD_UBI_BEB_LIMIT=20

# CONFIG_MTD_UBI_FASTMAP is not set

# CONFIG_MTD_UBI_GLUEBI is not set

CONFIG_DTC=y

CONFIG_OF=y

#

# Device Tree and Open Firmware support

#

CONFIG_PROC_DEVICETREE=y

# CONFIG_OF_SELFTEST is not set

CONFIG_OF_FLATTREE=y

CONFIG_OF_EARLY_FLATTREE=y

CONFIG_OF_ADDRESS=y

CONFIG_OF_IRQ=y

CONFIG_OF_DEVICE=y

CONFIG_OF_I2C=y

CONFIG_OF_NET=y

CONFIG_OF_MDIO=y

CONFIG_OF_MTD=y

# CONFIG_PARPORT is not set

# CONFIG_BLK_DEV is not set

#

# Misc devices

#

# CONFIG_SENSORS_LIS3LV02D is not set

# CONFIG_AD525X_DPOT is not set

# CONFIG_ATMEL_PWM is not set

# CONFIG_DUMMY_IRQ is not set

# CONFIG_ICS932S401 is not set

# CONFIG_ATMEL_SSC is not set

# CONFIG_ENCLOSURE_SERVICES is not set

# CONFIG_APDS9802ALS is not set

# CONFIG_ISL29003 is not set

# CONFIG_ISL29020 is not set

# CONFIG_SENSORS_TSL2550 is not set

# CONFIG_SENSORS_BH1780 is not set

# CONFIG_SENSORS_BH1770 is not set

# CONFIG_SENSORS_APDS990X is not set

# CONFIG_HMC6352 is not set

# CONFIG_YOCTO_TESTMOD is not set

# CONFIG_DS1682 is not set

# CONFIG_TI_DAC7512 is not set

# CONFIG_BMP085_I2C is not set

# CONFIG_BMP085_SPI is not set

# CONFIG_USB_SWITCH_FSA9480 is not set

# CONFIG_LATTICE_ECP3_CONFIG is not set

# CONFIG_SRAM is not set

# CONFIG_C2PORT is not set

#

# EEPROM support

#

CONFIG_EEPROM_AT24=y

# CONFIG_EEPROM_AT25 is not set

# CONFIG_EEPROM_LEGACY is not set

# CONFIG_EEPROM_MAX6875 is not set

# CONFIG_EEPROM_93CX6 is not set

# CONFIG_EEPROM_93XX46 is not set

#

# Texas Instruments shared transport line discipline

#

# CONFIG_TI_ST is not set

# CONFIG_SENSORS_LIS3_SPI is not set

# CONFIG_SENSORS_LIS3_I2C is not set

#

# Altera FPGA firmware download module

#

# CONFIG_ALTERA_STAPL is not set

#

# SCSI device support

#

CONFIG_SCSI_MOD=y

# CONFIG_RAID_ATTRS is not set

CONFIG_SCSI=y

CONFIG_SCSI_DMA=y

# CONFIG_SCSI_TGT is not set

# CONFIG_SCSI_NETLINK is not set

CONFIG_SCSI_PROC_FS=y

#

# SCSI support type (disk, tape, CD-ROM)

#

CONFIG_BLK_DEV_SD=y

# CONFIG_CHR_DEV_ST is not set

# CONFIG_CHR_DEV_OSST is not set

# CONFIG_BLK_DEV_SR is not set

# CONFIG_CHR_DEV_SG is not set

# CONFIG_CHR_DEV_SCH is not set

# CONFIG_SCSI_MULTI_LUN is not set

# CONFIG_SCSI_CONSTANTS is not set

# CONFIG_SCSI_LOGGING is not set

# CONFIG_SCSI_SCAN_ASYNC is not set

#

# SCSI Transports

#

# CONFIG_SCSI_SPI_ATTRS is not set

# CONFIG_SCSI_FC_ATTRS is not set

# CONFIG_SCSI_ISCSI_ATTRS is not set

# CONFIG_SCSI_SAS_ATTRS is not set

# CONFIG_SCSI_SAS_LIBSAS is not set

# CONFIG_SCSI_SRP_ATTRS is not set

CONFIG_SCSI_LOWLEVEL=y

# CONFIG_ISCSI_TCP is not set

# CONFIG_ISCSI_BOOT_SYSFS is not set

# CONFIG_SCSI_UFSHCD is not set

# CONFIG_LIBFC is not set

# CONFIG_LIBFCOE is not set

# CONFIG_SCSI_DEBUG is not set

# CONFIG_SCSI_DH is not set

# CONFIG_SCSI_OSD_INITIATOR is not set

# CONFIG_ATA is not set

# CONFIG_MD is not set

# CONFIG_TARGET_CORE is not set

CONFIG_NETDEVICES=y

CONFIG_NET_CORE=y

# CONFIG_BONDING is not set

# CONFIG_DUMMY is not set

# CONFIG_EQUALIZER is not set

CONFIG_MII=y

# CONFIG_NET_TEAM is not set

# CONFIG_MACVLAN is not set

# CONFIG_VXLAN is not set

# CONFIG_NETCONSOLE is not set

# CONFIG_NETPOLL is not set

# CONFIG_NET_POLL_CONTROLLER is not set

# CONFIG_TUN is not set

# CONFIG_VETH is not set

#

# CAIF transport drivers

#

#

# Distributed Switch Architecture drivers

#

# CONFIG_NET_DSA_MV88E6XXX is not set

# CONFIG_NET_DSA_MV88E6060 is not set

# CONFIG_NET_DSA_MV88E6XXX_NEED_PPU is not set

# CONFIG_NET_DSA_MV88E6131 is not set

# CONFIG_NET_DSA_MV88E6123_61_65 is not set

CONFIG_ETHERNET=y

CONFIG_NET_CADENCE=y

# CONFIG_ARM_AT91_ETHER is not set

# CONFIG_MACB is not set

CONFIG_NET_VENDOR_BROADCOM=y

# CONFIG_B44 is not set

# CONFIG_NET_CALXEDA_XGMAC is not set

CONFIG_NET_VENDOR_CIRRUS=y

# CONFIG_CS89x0 is not set

# CONFIG_DM9000 is not set

# CONFIG_DNET is not set

CONFIG_NET_VENDOR_FARADAY=y

# CONFIG_FTMAC100 is not set

# CONFIG_FTGMAC100 is not set

CONFIG_NET_VENDOR_FREESCALE=y

CONFIG_FEC=y

CONFIG_NET_VENDOR_INTEL=y

CONFIG_NET_VENDOR_I825XX=y

CONFIG_NET_VENDOR_MARVELL=y

# CONFIG_MVMDIO is not set

CONFIG_NET_VENDOR_MICREL=y

# CONFIG_KS8842 is not set

# CONFIG_KS8851 is not set

# CONFIG_KS8851_MLL is not set

CONFIG_NET_VENDOR_MICROCHIP=y

CONFIG_ENC28J60=y

# CONFIG_ENC28J60_WRITEVERIFY is not set

CONFIG_NET_VENDOR_NATSEMI=y

CONFIG_NET_VENDOR_8390=y

# CONFIG_AX88796 is not set

# CONFIG_ETHOC is not set

CONFIG_NET_VENDOR_SEEQ=y

CONFIG_NET_VENDOR_SMSC=y

# CONFIG_SMC91X is not set

# CONFIG_SMC911X is not set

# CONFIG_SMSC911X is not set

CONFIG_NET_VENDOR_STMICRO=y

# CONFIG_STMMAC_ETH is not set

CONFIG_NET_VENDOR_WIZNET=y

# CONFIG_WIZNET_W5100 is not set

# CONFIG_WIZNET_W5300 is not set

CONFIG_PHYLIB=y

#

# MII PHY device drivers

#

# CONFIG_AT803X_PHY is not set

# CONFIG_AMD_PHY is not set

# CONFIG_MARVELL_PHY is not set

# CONFIG_DAVICOM_PHY is not set

# CONFIG_QSEMI_PHY is not set

# CONFIG_LXT_PHY is not set

# CONFIG_CICADA_PHY is not set

# CONFIG_VITESSE_PHY is not set

CONFIG_SMSC_PHY=y

# CONFIG_BROADCOM_PHY is not set

# CONFIG_BCM87XX_PHY is not set

CONFIG_ICPLUS_PHY=y

CONFIG_REALTEK_PHY=y

# CONFIG_NATIONAL_PHY is not set

# CONFIG_STE10XP is not set

# CONFIG_LSI_ET1011C_PHY is not set

CONFIG_MICREL_PHY=y

# CONFIG_FIXED_PHY is not set

# CONFIG_MDIO_BITBANG is not set

# CONFIG_MDIO_BUS_MUX_GPIO is not set

# CONFIG_MDIO_BUS_MUX_MMIOREG is not set

# CONFIG_MICREL_KS8995MA is not set

# CONFIG_PPP is not set

# CONFIG_SLIP is not set

#

# USB Network Adapters

#

# CONFIG_USB_CATC is not set

# CONFIG_USB_KAWETH is not set

# CONFIG_USB_PEGASUS is not set

# CONFIG_USB_RTL8150 is not set

# CONFIG_USB_RTL8152 is not set

CONFIG_USB_USBNET=y

CONFIG_USB_NET_AX8817X=y

CONFIG_USB_NET_AX88179_178A=y

CONFIG_USB_NET_CDCETHER=y

# CONFIG_USB_NET_CDC_EEM is not set

CONFIG_USB_NET_CDC_NCM=y

# CONFIG_USB_NET_CDC_MBIM is not set

# CONFIG_USB_NET_DM9601 is not set

# CONFIG_USB_NET_SMSC75XX is not set

CONFIG_USB_NET_SMSC95XX=y

# CONFIG_USB_NET_GL620A is not set

CONFIG_USB_NET_NET1080=y

# CONFIG_USB_NET_PLUSB is not set

# CONFIG_USB_NET_MCS7830 is not set

# CONFIG_USB_NET_RNDIS_HOST is not set

CONFIG_USB_NET_CDC_SUBSET=y

# CONFIG_USB_ALI_M5632 is not set

# CONFIG_USB_AN2720 is not set

CONFIG_USB_BELKIN=y

CONFIG_USB_ARMLINUX=y

# CONFIG_USB_EPSON2888 is not set

# CONFIG_USB_KC2190 is not set

CONFIG_USB_NET_ZAURUS=y

# CONFIG_USB_NET_CX82310_ETH is not set

# CONFIG_USB_NET_KALMIA is not set

# CONFIG_USB_NET_QMI_WWAN is not set

# CONFIG_USB_NET_INT51X1 is not set

# CONFIG_USB_IPHETH is not set

# CONFIG_USB_SIERRA_NET is not set

# CONFIG_USB_VL600 is not set

# CONFIG_WLAN is not set

#

# Enable WiMAX (Networking options) to see the WiMAX drivers

#

# CONFIG_WAN is not set

# CONFIG_ISDN is not set

#

# Input device support

#

CONFIG_INPUT=y

# CONFIG_INPUT_FF_MEMLESS is not set

# CONFIG_INPUT_POLLDEV is not set

# CONFIG_INPUT_SPARSEKMAP is not set

# CONFIG_INPUT_MATRIXKMAP is not set

#

# Userland interfaces

#

CONFIG_INPUT_MOUSEDEV=y

# CONFIG_INPUT_MOUSEDEV_PSAUX is not set

CONFIG_INPUT_MOUSEDEV_SCREEN_X=1024

CONFIG_INPUT_MOUSEDEV_SCREEN_Y=768

# CONFIG_INPUT_JOYDEV is not set

CONFIG_INPUT_EVDEV=y

# CONFIG_INPUT_EVBUG is not set

#

# Input Device Drivers

#

# CONFIG_INPUT_KEYBOARD is not set

# CONFIG_INPUT_MOUSE is not set

# CONFIG_INPUT_JOYSTICK is not set

# CONFIG_INPUT_TABLET is not set

# CONFIG_INPUT_TOUCHSCREEN is not set

# CONFIG_INPUT_MISC is not set

#

# Hardware I/O ports

#

# CONFIG_SERIO is not set

# CONFIG_GAMEPORT is not set

#

# Character devices

#

CONFIG_TTY=y

CONFIG_VT=y

CONFIG_CONSOLE_TRANSLATIONS=y

CONFIG_VT_CONSOLE=y

CONFIG_VT_CONSOLE_SLEEP=y

CONFIG_HW_CONSOLE=y

CONFIG_VT_HW_CONSOLE_BINDING=y

CONFIG_UNIX98_PTYS=y

CONFIG_DEVPTS_MULTIPLE_INSTANCES=y

CONFIG_LEGACY_PTYS=y

CONFIG_LEGACY_PTY_COUNT=256

# CONFIG_SERIAL_NONSTANDARD is not set

# CONFIG_N_GSM is not set

# CONFIG_TRACE_SINK is not set

# CONFIG_DEVKMEM is not set

#

# Serial drivers

#

# CONFIG_SERIAL_8250 is not set

#

# Non-8250 serial port support

#

# CONFIG_SERIAL_AMBA_PL010 is not set

CONFIG_SERIAL_AMBA_PL011=y

CONFIG_SERIAL_AMBA_PL011_CONSOLE=y

# CONFIG_SERIAL_MAX3100 is not set

# CONFIG_SERIAL_MAX310X is not set

CONFIG_SERIAL_CORE=y

CONFIG_SERIAL_CORE_CONSOLE=y

# CONFIG_SERIAL_SCCNXP is not set

# CONFIG_SERIAL_TIMBERDALE is not set

# CONFIG_SERIAL_ALTERA_JTAGUART is not set

# CONFIG_SERIAL_ALTERA_UART is not set

# CONFIG_SERIAL_IFX6X60 is not set

CONFIG_SERIAL_MXS_AUART=y

# CONFIG_SERIAL_MXS_AUART_CONSOLE is not set

# CONFIG_SERIAL_XILINX_PS_UART is not set

# CONFIG_SERIAL_ARC is not set

# CONFIG_TTY_PRINTK is not set

# CONFIG_HVC_DCC is not set

# CONFIG_IPMI_HANDLER is not set

# CONFIG_HW_RANDOM is not set

# CONFIG_R3964 is not set

# CONFIG_RAW_DRIVER is not set

# CONFIG_TCG_TPM is not set

CONFIG_I2C=y

CONFIG_I2C_BOARDINFO=y

# CONFIG_I2C_COMPAT is not set

CONFIG_I2C_CHARDEV=y

# CONFIG_I2C_MUX is not set

CONFIG_I2C_HELPER_AUTO=y

CONFIG_I2C_ALGOBIT=y

#

# I2C Hardware Bus support

#

#

# I2C system bus drivers (mostly embedded / system-on-chip)

#

# CONFIG_I2C_CBUS_GPIO is not set

# CONFIG_I2C_DESIGNWARE_PLATFORM is not set

CONFIG_I2C_GPIO=y

CONFIG_I2C_MXS=y

# CONFIG_I2C_NOMADIK is not set

# CONFIG_I2C_OCORES is not set

# CONFIG_I2C_PCA_PLATFORM is not set

# CONFIG_I2C_PXA_PCI is not set

# CONFIG_I2C_SIMTEC is not set

# CONFIG_I2C_XILINX is not set

#

# External I2C/SMBus adapter drivers

#

# CONFIG_I2C_DIOLAN_U2C is not set

# CONFIG_I2C_PARPORT_LIGHT is not set

# CONFIG_I2C_TAOS_EVM is not set

# CONFIG_I2C_TINY_USB is not set

#

# Other I2C/SMBus bus drivers

#

# CONFIG_I2C_STUB is not set

# CONFIG_I2C_DEBUG_CORE is not set

# CONFIG_I2C_DEBUG_ALGO is not set

# CONFIG_I2C_DEBUG_BUS is not set

CONFIG_SPI=y

# CONFIG_SPI_DEBUG is not set

CONFIG_SPI_MASTER=y

#

# SPI Master Controller Drivers

#

# CONFIG_SPI_ALTERA is not set

# CONFIG_SPI_BITBANG is not set

# CONFIG_SPI_GPIO is not set

# CONFIG_SPI_FSL_SPI is not set

# CONFIG_SPI_OC_TINY is not set

# CONFIG_SPI_PL022 is not set

# CONFIG_SPI_PXA2XX_PCI is not set

# CONFIG_SPI_SC18IS602 is not set

CONFIG_SPI_MXS=y

# CONFIG_SPI_XCOMM is not set

# CONFIG_SPI_XILINX is not set

# CONFIG_SPI_DESIGNWARE is not set

#

# SPI Protocol Masters

#

CONFIG_SPI_SPIDEV=y

# CONFIG_SPI_TLE62X0 is not set

#

# Qualcomm MSM SSBI bus support

#

# CONFIG_SSBI is not set

# CONFIG_HSI is not set

#

# PPS support

#

CONFIG_PPS=y

# CONFIG_PPS_DEBUG is not set

#

# PPS clients support

#

# CONFIG_PPS_CLIENT_KTIMER is not set

# CONFIG_PPS_CLIENT_LDISC is not set

# CONFIG_PPS_CLIENT_GPIO is not set

#

# PPS generators support

#

#

# PTP clock support

#

CONFIG_PTP_1588_CLOCK=y

#

# Enable PHYLIB and NETWORK_PHY_TIMESTAMPING to see the additional clocks.

#

# CONFIG_PTP_1588_CLOCK_PCH is not set

CONFIG_PINCTRL=y

#

# Pin controllers

#

CONFIG_PINMUX=y

CONFIG_PINCONF=y

# CONFIG_DEBUG_PINCTRL is not set

CONFIG_PINCTRL_MXS=y

CONFIG_PINCTRL_IMX23=y

CONFIG_PINCTRL_IMX28=y

# CONFIG_PINCTRL_SINGLE is not set

# CONFIG_PINCTRL_EXYNOS is not set

# CONFIG_PINCTRL_EXYNOS5440 is not set

CONFIG_ARCH_HAVE_CUSTOM_GPIO_H=y

CONFIG_ARCH_REQUIRE_GPIOLIB=y

CONFIG_GPIO_DEVRES=y

CONFIG_GPIOLIB=y

CONFIG_OF_GPIO=y

CONFIG_DEBUG_GPIO=y

CONFIG_GPIO_SYSFS=y

CONFIG_GPIO_GENERIC=y

#

# Memory mapped GPIO drivers:

#

# CONFIG_GPIO_GENERIC_PLATFORM is not set

# CONFIG_GPIO_EM is not set

CONFIG_GPIO_MXS=y

# CONFIG_GPIO_PL061 is not set

# CONFIG_GPIO_RCAR is not set

# CONFIG_GPIO_TS5500 is not set

# CONFIG_GPIO_GRGPIO is not set

#

# I2C GPIO expanders:

#

# CONFIG_GPIO_MAX7300 is not set

# CONFIG_GPIO_MAX732X is not set

# CONFIG_GPIO_PCF857X is not set

# CONFIG_GPIO_SX150X is not set

# CONFIG_GPIO_ADP5588 is not set

# CONFIG_GPIO_ADNP is not set

#

# PCI GPIO expanders:

#

#

# SPI GPIO expanders:

#

# CONFIG_GPIO_MAX7301 is not set

# CONFIG_GPIO_MCP23S08 is not set

# CONFIG_GPIO_MC33880 is not set

# CONFIG_GPIO_74X164 is not set

#

# AC97 GPIO expanders:

#

#

# MODULbus GPIO expanders:

#

#

# USB GPIO expanders:

#

# CONFIG_W1 is not set

# CONFIG_POWER_SUPPLY is not set

# CONFIG_POWER_AVS is not set

# CONFIG_HWMON is not set

# CONFIG_THERMAL is not set

CONFIG_WATCHDOG=y

CONFIG_WATCHDOG_CORE=y

CONFIG_WATCHDOG_NOWAYOUT=y

#

# Watchdog Device Drivers

#

# CONFIG_SOFT_WATCHDOG is not set

# CONFIG_ARM_SP805_WATCHDOG is not set

# CONFIG_DW_WATCHDOG is not set

CONFIG_STMP3XXX_RTC_WATCHDOG=y

# CONFIG_MAX63XX_WATCHDOG is not set

#

# USB-based Watchdog Cards

#

# CONFIG_USBPCWATCHDOG is not set

CONFIG_SSB_POSSIBLE=y

#

# Sonics Silicon Backplane

#

# CONFIG_SSB is not set

CONFIG_BCMA_POSSIBLE=y

#

# Broadcom specific AMBA

#

# CONFIG_BCMA is not set

#

# Multifunction device drivers

#

# CONFIG_MFD_CORE is not set

# CONFIG_MFD_AS3711 is not set

# CONFIG_PMIC_ADP5520 is not set

# CONFIG_MFD_AAT2870_CORE is not set

# CONFIG_MFD_CROS_EC is not set

# CONFIG_MFD_ASIC3 is not set

# CONFIG_PMIC_DA903X is not set

# CONFIG_MFD_DA9052_SPI is not set

# CONFIG_MFD_DA9052_I2C is not set

# CONFIG_MFD_DA9055 is not set

# CONFIG_MFD_MC13XXX_SPI is not set

# CONFIG_MFD_MC13XXX_I2C is not set

# CONFIG_HTC_EGPIO is not set

# CONFIG_HTC_PASIC3 is not set

# CONFIG_HTC_I2CPLD is not set

# CONFIG_MFD_88PM800 is not set

# CONFIG_MFD_88PM805 is not set

# CONFIG_MFD_88PM860X is not set

# CONFIG_MFD_MAX77686 is not set

# CONFIG_MFD_MAX77693 is not set

# CONFIG_MFD_MAX8907 is not set

# CONFIG_MFD_MAX8925 is not set

# CONFIG_MFD_MAX8997 is not set

# CONFIG_MFD_MAX8998 is not set

# CONFIG_EZX_PCAP is not set

# CONFIG_MFD_VIPERBOARD is not set

# CONFIG_MFD_RETU is not set

# CONFIG_MFD_PCF50633 is not set

# CONFIG_MFD_RC5T583 is not set

# CONFIG_MFD_SEC_CORE is not set

# CONFIG_MFD_SI476X_CORE is not set

# CONFIG_MFD_SM501 is not set

# CONFIG_MFD_SMSC is not set

# CONFIG_ABX500_CORE is not set

# CONFIG_MFD_STMPE is not set

# CONFIG_MFD_SYSCON is not set

# CONFIG_MFD_TI_AM335X_TSCADC is not set

# CONFIG_MFD_LP8788 is not set

# CONFIG_MFD_PALMAS is not set

# CONFIG_TPS6105X is not set

# CONFIG_TPS65010 is not set

# CONFIG_TPS6507X is not set

# CONFIG_MFD_TPS65090 is not set

# CONFIG_MFD_TPS65217 is not set

# CONFIG_MFD_TPS6586X is not set

# CONFIG_MFD_TPS65910 is not set

# CONFIG_MFD_TPS65912 is not set

# CONFIG_MFD_TPS65912_I2C is not set

# CONFIG_MFD_TPS65912_SPI is not set

# CONFIG_MFD_TPS80031 is not set

# CONFIG_TWL4030_CORE is not set

# CONFIG_TWL6040_CORE is not set

# CONFIG_MFD_WL1273_CORE is not set

# CONFIG_MFD_LM3533 is not set

# CONFIG_MFD_TC3589X is not set

# CONFIG_MFD_TMIO is not set

# CONFIG_MFD_T7L66XB is not set

# CONFIG_MFD_TC6387XB is not set

# CONFIG_MFD_TC6393XB is not set

# CONFIG_MFD_ARIZONA_I2C is not set

# CONFIG_MFD_ARIZONA_SPI is not set

# CONFIG_MFD_WM8400 is not set

# CONFIG_MFD_WM831X_I2C is not set

# CONFIG_MFD_WM831X_SPI is not set

# CONFIG_MFD_WM8350_I2C is not set

# CONFIG_MFD_WM8994 is not set

CONFIG_REGULATOR=y

# CONFIG_REGULATOR_DEBUG is not set

# CONFIG_REGULATOR_DUMMY is not set

CONFIG_REGULATOR_FIXED_VOLTAGE=y

# CONFIG_REGULATOR_VIRTUAL_CONSUMER is not set

# CONFIG_REGULATOR_USERSPACE_CONSUMER is not set

# CONFIG_REGULATOR_GPIO is not set

# CONFIG_REGULATOR_AD5398 is not set

# CONFIG_REGULATOR_FAN53555 is not set

# CONFIG_REGULATOR_ISL6271A is not set

# CONFIG_REGULATOR_MAX1586 is not set

# CONFIG_REGULATOR_MAX8649 is not set

# CONFIG_REGULATOR_MAX8660 is not set

# CONFIG_REGULATOR_MAX8952 is not set

# CONFIG_REGULATOR_MAX8973 is not set

# CONFIG_REGULATOR_LP3971 is not set

# CONFIG_REGULATOR_LP3972 is not set

# CONFIG_REGULATOR_LP872X is not set

# CONFIG_REGULATOR_LP8755 is not set

# CONFIG_REGULATOR_TPS51632 is not set

# CONFIG_REGULATOR_TPS62360 is not set

# CONFIG_REGULATOR_TPS65023 is not set

# CONFIG_REGULATOR_TPS6507X is not set

# CONFIG_REGULATOR_TPS6524X is not set

# CONFIG_MEDIA_SUPPORT is not set

#

# Graphics support

#

# CONFIG_DRM is not set

# CONFIG_TEGRA_HOST1X is not set

# CONFIG_VGASTATE is not set

# CONFIG_VIDEO_OUTPUT_CONTROL is not set

# CONFIG_FB is not set

# CONFIG_EXYNOS_VIDEO is not set

# CONFIG_BACKLIGHT_LCD_SUPPORT is not set

#

# Console display driver support

#

CONFIG_DUMMY_CONSOLE=y

# CONFIG_SOUND is not set

#

# HID support

#

CONFIG_HID=y

# CONFIG_HIDRAW is not set

# CONFIG_UHID is not set

CONFIG_HID_GENERIC=y

#

# Special HID drivers

#

# CONFIG_HID_A4TECH is not set

# CONFIG_HID_ACRUX is not set

# CONFIG_HID_APPLE is not set

# CONFIG_HID_APPLEIR is not set

# CONFIG_HID_AUREAL is not set

# CONFIG_HID_BELKIN is not set

# CONFIG_HID_CHERRY is not set

# CONFIG_HID_CHICONY is not set

# CONFIG_HID_CYPRESS is not set

# CONFIG_HID_DRAGONRISE is not set

# CONFIG_HID_EMS_FF is not set

# CONFIG_HID_ELECOM is not set

# CONFIG_HID_EZKEY is not set

# CONFIG_HID_HOLTEK is not set

# CONFIG_HID_KEYTOUCH is not set

# CONFIG_HID_KYE is not set

# CONFIG_HID_UCLOGIC is not set

# CONFIG_HID_WALTOP is not set

# CONFIG_HID_GYRATION is not set

# CONFIG_HID_ICADE is not set

# CONFIG_HID_TWINHAN is not set

# CONFIG_HID_KENSINGTON is not set

# CONFIG_HID_LCPOWER is not set

# CONFIG_HID_LENOVO_TPKBD is not set

# CONFIG_HID_LOGITECH is not set

# CONFIG_HID_MAGICMOUSE is not set

# CONFIG_HID_MICROSOFT is not set

# CONFIG_HID_MONTEREY is not set

# CONFIG_HID_MULTITOUCH is not set

# CONFIG_HID_NTRIG is not set

# CONFIG_HID_ORTEK is not set

# CONFIG_HID_PANTHERLORD is not set

# CONFIG_HID_PETALYNX is not set

# CONFIG_HID_PICOLCD is not set

# CONFIG_HID_PRIMAX is not set

# CONFIG_HID_PS3REMOTE is not set

# CONFIG_HID_ROCCAT is not set

# CONFIG_HID_SAITEK is not set

# CONFIG_HID_SAMSUNG is not set

# CONFIG_HID_SONY is not set

# CONFIG_HID_SPEEDLINK is not set

# CONFIG_HID_STEELSERIES is not set

# CONFIG_HID_SUNPLUS is not set

# CONFIG_HID_GREENASIA is not set

# CONFIG_HID_SMARTJOYPLUS is not set

# CONFIG_HID_TIVO is not set

# CONFIG_HID_TOPSEED is not set

# CONFIG_HID_THRUSTMASTER is not set

# CONFIG_HID_ZEROPLUS is not set

# CONFIG_HID_ZYDACRON is not set

# CONFIG_HID_SENSOR_HUB is not set

#

# USB HID support

#

CONFIG_USB_HID=y

# CONFIG_HID_PID is not set

# CONFIG_USB_HIDDEV is not set

#

# I2C HID support

#

# CONFIG_I2C_HID is not set

# CONFIG_USB_ARCH_HAS_OHCI is not set

CONFIG_USB_ARCH_HAS_EHCI=y

# CONFIG_USB_ARCH_HAS_XHCI is not set

CONFIG_USB_SUPPORT=y

CONFIG_USB_COMMON=y

CONFIG_USB_ARCH_HAS_HCD=y

CONFIG_USB=y

# CONFIG_USB_DEBUG is not set

# CONFIG_USB_ANNOUNCE_NEW_DEVICES is not set

#

# Miscellaneous USB options

#

CONFIG_USB_DEFAULT_PERSIST=y

# CONFIG_USB_DYNAMIC_MINORS is not set

# CONFIG_USB_OTG_WHITELIST is not set

# CONFIG_USB_OTG_BLACKLIST_HUB is not set

# CONFIG_USB_MON is not set

# CONFIG_USB_WUSB_CBAF is not set

#

# USB Host Controller Drivers

#

# CONFIG_USB_C67X00_HCD is not set

CONFIG_USB_EHCI_HCD=y

CONFIG_USB_EHCI_ROOT_HUB_TT=y

CONFIG_USB_EHCI_TT_NEWSCHED=y

# CONFIG_USB_EHCI_HCD_PLATFORM is not set

# CONFIG_USB_OXU210HP_HCD is not set

# CONFIG_USB_ISP116X_HCD is not set

# CONFIG_USB_ISP1760_HCD is not set

# CONFIG_USB_ISP1362_HCD is not set

# CONFIG_USB_SL811_HCD is not set

# CONFIG_USB_R8A66597_HCD is not set

#

# USB Device Class drivers

#

# CONFIG_USB_ACM is not set

# CONFIG_USB_PRINTER is not set

# CONFIG_USB_WDM is not set

# CONFIG_USB_TMC is not set

#

# NOTE: USB_STORAGE depends on SCSI but BLK_DEV_SD may

#

#

# also be needed; see USB_STORAGE Help for more info

#

CONFIG_USB_STORAGE=y

# CONFIG_USB_STORAGE_DEBUG is not set

# CONFIG_USB_STORAGE_REALTEK is not set

# CONFIG_USB_STORAGE_DATAFAB is not set

# CONFIG_USB_STORAGE_FREECOM is not set

# CONFIG_USB_STORAGE_ISD200 is not set

# CONFIG_USB_STORAGE_USBAT is not set

# CONFIG_USB_STORAGE_SDDR09 is not set

# CONFIG_USB_STORAGE_SDDR55 is not set

# CONFIG_USB_STORAGE_JUMPSHOT is not set

# CONFIG_USB_STORAGE_ALAUDA is not set

# CONFIG_USB_STORAGE_ONETOUCH is not set

# CONFIG_USB_STORAGE_KARMA is not set

# CONFIG_USB_STORAGE_CYPRESS_ATACB is not set

# CONFIG_USB_STORAGE_ENE_UB6250 is not set

#

# USB Imaging devices

#

# CONFIG_USB_MDC800 is not set

# CONFIG_USB_MICROTEK is not set

# CONFIG_USB_DWC3 is not set

CONFIG_USB_CHIPIDEA=y

CONFIG_USB_CHIPIDEA_HOST=y

# CONFIG_USB_CHIPIDEA_DEBUG is not set

#

# USB port drivers

#

# CONFIG_USB_SERIAL is not set

#

# USB Miscellaneous drivers

#

# CONFIG_USB_EMI62 is not set

# CONFIG_USB_EMI26 is not set

# CONFIG_USB_ADUTUX is not set

# CONFIG_USB_SEVSEG is not set

# CONFIG_USB_RIO500 is not set

# CONFIG_USB_LEGOTOWER is not set

# CONFIG_USB_LCD is not set

# CONFIG_USB_LED is not set

# CONFIG_USB_CYPRESS_CY7C63 is not set

# CONFIG_USB_CYTHERM is not set

# CONFIG_USB_IDMOUSE is not set

# CONFIG_USB_FTDI_ELAN is not set

# CONFIG_USB_APPLEDISPLAY is not set

# CONFIG_USB_SISUSBVGA is not set

# CONFIG_USB_LD is not set

# CONFIG_USB_TRANCEVIBRATOR is not set

# CONFIG_USB_IOWARRIOR is not set

# CONFIG_USB_TEST is not set

# CONFIG_USB_ISIGHTFW is not set

# CONFIG_USB_YUREX is not set

# CONFIG_USB_EZUSB_FX2 is not set

# CONFIG_USB_HSIC_USB3503 is not set

CONFIG_USB_PHY=y

# CONFIG_NOP_USB_XCEIV is not set

# CONFIG_OMAP_CONTROL_USB is not set

# CONFIG_OMAP_USB3 is not set

# CONFIG_SAMSUNG_USBPHY is not set

# CONFIG_SAMSUNG_USB2PHY is not set

# CONFIG_SAMSUNG_USB3PHY is not set

# CONFIG_USB_GPIO_VBUS is not set

# CONFIG_USB_ISP1301 is not set

CONFIG_USB_MXS_PHY=y

# CONFIG_USB_RCAR_PHY is not set

# CONFIG_USB_ULPI is not set

# CONFIG_USB_GADGET is not set

CONFIG_MMC=y

# CONFIG_MMC_DEBUG is not set

CONFIG_MMC_UNSAFE_RESUME=y

# CONFIG_MMC_CLKGATE is not set

#

# MMC/SD/SDIO Card Drivers

#

CONFIG_MMC_BLOCK=y

CONFIG_MMC_BLOCK_MINORS=8

CONFIG_MMC_BLOCK_BOUNCE=y

# CONFIG_SDIO_UART is not set

# CONFIG_MMC_TEST is not set

#

# MMC/SD/SDIO Host Controller Drivers

#

# CONFIG_MMC_ARMMMCI is not set

# CONFIG_MMC_SDHCI is not set

# CONFIG_MMC_SDHCI_PXAV3 is not set

# CONFIG_MMC_SDHCI_PXAV2 is not set

CONFIG_MMC_MXS=y

# CONFIG_MMC_SPI is not set

# CONFIG_MMC_DW is not set

# CONFIG_MMC_VUB300 is not set

# CONFIG_MMC_USHC is not set

# CONFIG_MEMSTICK is not set

# CONFIG_NEW_LEDS is not set

# CONFIG_ACCESSIBILITY is not set

# CONFIG_EDAC is not set

CONFIG_RTC_LIB=y

CONFIG_RTC_CLASS=y

CONFIG_RTC_HCTOSYS=y

CONFIG_RTC_SYSTOHC=y

CONFIG_RTC_HCTOSYS_DEVICE="rtc0"

# CONFIG_RTC_DEBUG is not set

#

# RTC interfaces

#

CONFIG_RTC_INTF_SYSFS=y

CONFIG_RTC_INTF_PROC=y

CONFIG_RTC_INTF_DEV=y

# CONFIG_RTC_INTF_DEV_UIE_EMUL is not set

# CONFIG_RTC_DRV_TEST is not set

#

# I2C RTC drivers

#

CONFIG_RTC_DRV_DS1307=m

# CONFIG_RTC_DRV_DS1374 is not set

# CONFIG_RTC_DRV_DS1672 is not set

# CONFIG_RTC_DRV_DS3232 is not set

# CONFIG_RTC_DRV_MAX6900 is not set

# CONFIG_RTC_DRV_RS5C372 is not set

# CONFIG_RTC_DRV_ISL1208 is not set

# CONFIG_RTC_DRV_ISL12022 is not set

# CONFIG_RTC_DRV_X1205 is not set

# CONFIG_RTC_DRV_PCF8523 is not set

# CONFIG_RTC_DRV_PCF8563 is not set

# CONFIG_RTC_DRV_PCF8583 is not set

# CONFIG_RTC_DRV_M41T80 is not set

# CONFIG_RTC_DRV_BQ32K is not set

# CONFIG_RTC_DRV_S35390A is not set

# CONFIG_RTC_DRV_FM3130 is not set

# CONFIG_RTC_DRV_RX8581 is not set

# CONFIG_RTC_DRV_RX8025 is not set

# CONFIG_RTC_DRV_EM3027 is not set

# CONFIG_RTC_DRV_RV3029C2 is not set

#

# SPI RTC drivers

#

# CONFIG_RTC_DRV_M41T93 is not set

# CONFIG_RTC_DRV_M41T94 is not set

# CONFIG_RTC_DRV_DS1305 is not set

# CONFIG_RTC_DRV_DS1390 is not set

# CONFIG_RTC_DRV_MAX6902 is not set

# CONFIG_RTC_DRV_R9701 is not set

# CONFIG_RTC_DRV_RS5C348 is not set

# CONFIG_RTC_DRV_DS3234 is not set

# CONFIG_RTC_DRV_PCF2123 is not set

# CONFIG_RTC_DRV_RX4581 is not set

#

# Platform RTC drivers

#

# CONFIG_RTC_DRV_CMOS is not set

# CONFIG_RTC_DRV_DS1286 is not set

# CONFIG_RTC_DRV_DS1511 is not set

# CONFIG_RTC_DRV_DS1553 is not set

# CONFIG_RTC_DRV_DS1742 is not set

# CONFIG_RTC_DRV_STK17TA8 is not set

# CONFIG_RTC_DRV_M48T86 is not set

# CONFIG_RTC_DRV_M48T35 is not set

# CONFIG_RTC_DRV_M48T59 is not set

# CONFIG_RTC_DRV_MSM6242 is not set

# CONFIG_RTC_DRV_BQ4802 is not set

# CONFIG_RTC_DRV_RP5C01 is not set

# CONFIG_RTC_DRV_V3020 is not set

# CONFIG_RTC_DRV_DS2404 is not set

#

# on-CPU RTC drivers

#

# CONFIG_RTC_DRV_PL030 is not set

# CONFIG_RTC_DRV_PL031 is not set

CONFIG_RTC_DRV_STMP=y

# CONFIG_RTC_DRV_SNVS is not set

#

# HID Sensor RTC drivers

#

# CONFIG_RTC_DRV_HID_SENSOR_TIME is not set

CONFIG_DMADEVICES=y

# CONFIG_DMADEVICES_DEBUG is not set

#

# DMA Devices

#

# CONFIG_AMBA_PL08X is not set

# CONFIG_DW_DMAC is not set

# CONFIG_TIMB_DMA is not set

# CONFIG_PL330_DMA is not set

CONFIG_MXS_DMA=y

CONFIG_DMA_ENGINE=y

CONFIG_DMA_OF=y

#

# DMA Clients

#

# CONFIG_NET_DMA is not set

# CONFIG_ASYNC_TX_DMA is not set

# CONFIG_DMATEST is not set

# CONFIG_AUXDISPLAY is not set

# CONFIG_UIO is not set

# CONFIG_VIRT_DRIVERS is not set

#

# Virtio drivers

#

# CONFIG_VIRTIO_MMIO is not set

#

# Microsoft Hyper-V guest support

#

CONFIG_STAGING=y

# CONFIG_USBIP_CORE is not set

# CONFIG_ECHO is not set

# CONFIG_COMEDI is not set

# CONFIG_ASUS_OLED is not set

# CONFIG_RTS5139 is not set

# CONFIG_TRANZPORT is not set

#

# IIO staging drivers

#

#

# Accelerometers

#

# CONFIG_ADIS16201 is not set

# CONFIG_ADIS16203 is not set

# CONFIG_ADIS16204 is not set

# CONFIG_ADIS16209 is not set

# CONFIG_ADIS16220 is not set

# CONFIG_ADIS16240 is not set

# CONFIG_LIS3L02DQ is not set

# CONFIG_SCA3000 is not set

#

# Analog to digital converters

#

# CONFIG_AD7291 is not set

# CONFIG_AD7606 is not set

# CONFIG_AD799X is not set

# CONFIG_AD7780 is not set

# CONFIG_AD7816 is not set

# CONFIG_AD7192 is not set

# CONFIG_AD7280 is not set

CONFIG_MXS_LRADC=y

#

# Analog digital bi-direction converters

#

# CONFIG_ADT7316 is not set

#

# Capacitance to digital converters

#

# CONFIG_AD7150 is not set

# CONFIG_AD7152 is not set

# CONFIG_AD7746 is not set

#

# Direct Digital Synthesis

#

# CONFIG_AD5930 is not set

# CONFIG_AD9832 is not set

# CONFIG_AD9834 is not set

# CONFIG_AD9850 is not set

# CONFIG_AD9852 is not set

# CONFIG_AD9910 is not set

# CONFIG_AD9951 is not set

#

# Digital gyroscope sensors

#

# CONFIG_ADIS16060 is not set

# CONFIG_ADIS16130 is not set

# CONFIG_ADIS16260 is not set

#

# Network Analyzer, Impedance Converters

#

# CONFIG_AD5933 is not set

#

# Light sensors

#

# CONFIG_SENSORS_ISL29018 is not set

# CONFIG_SENSORS_ISL29028 is not set

# CONFIG_TSL2583 is not set

# CONFIG_TSL2x7x is not set

#

# Magnetometer sensors

#

# CONFIG_SENSORS_HMC5843 is not set

#

# Active energy metering IC

#

# CONFIG_ADE7753 is not set

# CONFIG_ADE7754 is not set

# CONFIG_ADE7758 is not set

# CONFIG_ADE7759 is not set

# CONFIG_ADE7854 is not set

#

# Resolver to digital converters

#

# CONFIG_AD2S90 is not set

# CONFIG_AD2S1200 is not set

# CONFIG_AD2S1210 is not set

#

# Triggers - standalone

#

# CONFIG_IIO_PERIODIC_RTC_TRIGGER is not set

# CONFIG_IIO_GPIO_TRIGGER is not set

CONFIG_IIO_SYSFS_TRIGGER=y

# CONFIG_IIO_SIMPLE_DUMMY is not set

# CONFIG_ZSMALLOC is not set

# CONFIG_USB_ENESTORAGE is not set

# CONFIG_BCM_WIMAX is not set

# CONFIG_FT1000 is not set

#

# Speakup console speech

#

# CONFIG_SPEAKUP is not set

# CONFIG_TOUCHSCREEN_CLEARPAD_TM1217 is not set

# CONFIG_TOUCHSCREEN_SYNAPTICS_I2C_RMI4 is not set

# CONFIG_STAGING_MEDIA is not set

#

# Android

#

# CONFIG_ANDROID is not set

# CONFIG_USB_WPAN_HCD is not set

# CONFIG_WIMAX_GDM72XX is not set

# CONFIG_CED1401 is not set

# CONFIG_DGRP is not set

CONFIG_CLKDEV_LOOKUP=y

CONFIG_HAVE_CLK_PREPARE=y

CONFIG_COMMON_CLK=y

#

# Common Clock Framework

#

CONFIG_COMMON_CLK_DEBUG=y

# CONFIG_COMMON_CLK_SI5351 is not set

#

# Hardware Spinlock drivers

#

CONFIG_CLKSRC_OF=y

CONFIG_CLKSRC_MMIO=y

# CONFIG_MAILBOX is not set

CONFIG_IOMMU_SUPPORT=y

CONFIG_OF_IOMMU=y

#

# Remoteproc drivers

#

# CONFIG_STE_MODEM_RPROC is not set

#

# Rpmsg drivers

#

# CONFIG_PM_DEVFREQ is not set

# CONFIG_EXTCON is not set

# CONFIG_MEMORY is not set

CONFIG_IIO=y

CONFIG_IIO_BUFFER=y

# CONFIG_IIO_BUFFER_CB is not set

CONFIG_IIO_KFIFO_BUF=y

CONFIG_IIO_TRIGGERED_BUFFER=y

CONFIG_IIO_TRIGGER=y

CONFIG_IIO_CONSUMERS_PER_TRIGGER=2

#

# Accelerometers

#

# CONFIG_KXSD9 is not set

# CONFIG_IIO_ST_ACCEL_3AXIS is not set

#

# Analog to digital converters

#

# CONFIG_AD7266 is not set

# CONFIG_AD7298 is not set

# CONFIG_AD7923 is not set

# CONFIG_AD7791 is not set

# CONFIG_AD7793 is not set

# CONFIG_AD7476 is not set

# CONFIG_AD7887 is not set

# CONFIG_EXYNOS_ADC is not set

# CONFIG_MAX1363 is not set

# CONFIG_TI_ADC081C is not set

#

# Amplifiers

#

# CONFIG_AD8366 is not set

#

# Hid Sensor IIO Common

#

#

# Digital to analog converters

#

# CONFIG_AD5064 is not set

# CONFIG_AD5360 is not set

# CONFIG_AD5380 is not set

# CONFIG_AD5421 is not set

# CONFIG_AD5624R_SPI is not set

# CONFIG_AD5446 is not set

# CONFIG_AD5449 is not set

# CONFIG_AD5504 is not set

# CONFIG_AD5755 is not set

# CONFIG_AD5764 is not set

# CONFIG_AD5791 is not set

# CONFIG_AD5686 is not set

# CONFIG_MAX517 is not set

# CONFIG_MCP4725 is not set

#

# Frequency Synthesizers DDS/PLL

#

#

# Clock Generator/Distribution

#

# CONFIG_AD9523 is not set

#

# Phase-Locked Loop (PLL) frequency synthesizers

#

# CONFIG_ADF4350 is not set

#

# Digital gyroscope sensors

#

# CONFIG_ADIS16080 is not set

# CONFIG_ADIS16136 is not set

# CONFIG_ADXRS450 is not set

# CONFIG_IIO_ST_GYRO_3AXIS is not set

# CONFIG_ITG3200 is not set

#

# Inertial measurement units

#

# CONFIG_ADIS16400 is not set

# CONFIG_ADIS16480 is not set

# CONFIG_INV_MPU6050_IIO is not set

#

# Light sensors

#

# CONFIG_ADJD_S311 is not set

# CONFIG_SENSORS_TSL2563 is not set

# CONFIG_VCNL4000 is not set

#

# Magnetometer sensors

#

# CONFIG_AK8975 is not set

# CONFIG_IIO_ST_MAGN_3AXIS is not set

# CONFIG_PWM is not set

CONFIG_IRQCHIP=y

# CONFIG_IPACK_BUS is not set

# CONFIG_RESET_CONTROLLER is not set

#

# File systems

#

CONFIG_EXT2_FS=y

CONFIG_EXT2_FS_XATTR=y

# CONFIG_EXT2_FS_POSIX_ACL is not set

# CONFIG_EXT2_FS_SECURITY is not set

# CONFIG_EXT2_FS_XIP is not set

CONFIG_EXT3_FS=y

CONFIG_EXT3_DEFAULTS_TO_ORDERED=y

CONFIG_EXT3_FS_XATTR=y

# CONFIG_EXT3_FS_POSIX_ACL is not set

# CONFIG_EXT3_FS_SECURITY is not set

CONFIG_EXT4_FS=y

# CONFIG_EXT4_FS_POSIX_ACL is not set

# CONFIG_EXT4_FS_SECURITY is not set

# CONFIG_EXT4_DEBUG is not set

CONFIG_JBD=y

# CONFIG_JBD_DEBUG is not set

CONFIG_JBD2=y

# CONFIG_JBD2_DEBUG is not set

CONFIG_FS_MBCACHE=y

# CONFIG_REISERFS_FS is not set

# CONFIG_JFS_FS is not set

# CONFIG_XFS_FS is not set

# CONFIG_GFS2_FS is not set

# CONFIG_BTRFS_FS is not set

# CONFIG_NILFS2_FS is not set

CONFIG_FS_POSIX_ACL=y

CONFIG_FILE_LOCKING=y

CONFIG_FSNOTIFY=y

# CONFIG_DNOTIFY is not set

CONFIG_INOTIFY_USER=y

# CONFIG_FANOTIFY is not set

# CONFIG_QUOTA is not set

# CONFIG_QUOTACTL is not set

# CONFIG_AUTOFS4_FS is not set

# CONFIG_FUSE_FS is not set

CONFIG_GENERIC_ACL=y

#

# Caches

#

CONFIG_FSCACHE=m

CONFIG_FSCACHE_STATS=y

# CONFIG_FSCACHE_HISTOGRAM is not set

# CONFIG_FSCACHE_DEBUG is not set

# CONFIG_FSCACHE_OBJECT_LIST is not set

CONFIG_CACHEFILES=m

# CONFIG_CACHEFILES_DEBUG is not set

# CONFIG_CACHEFILES_HISTOGRAM is not set

#

# CD-ROM/DVD Filesystems

#

# CONFIG_ISO9660_FS is not set

# CONFIG_UDF_FS is not set

#

# DOS/FAT/NT Filesystems

#

# CONFIG_MSDOS_FS is not set

# CONFIG_VFAT_FS is not set

# CONFIG_NTFS_FS is not set

#

# Pseudo filesystems

#

CONFIG_PROC_FS=y

CONFIG_PROC_SYSCTL=y

CONFIG_PROC_PAGE_MONITOR=y

CONFIG_SYSFS=y

CONFIG_TMPFS=y

CONFIG_TMPFS_POSIX_ACL=y

CONFIG_TMPFS_XATTR=y

# CONFIG_HUGETLB_PAGE is not set

# CONFIG_CONFIGFS_FS is not set

CONFIG_MISC_FILESYSTEMS=y

# CONFIG_ADFS_FS is not set

# CONFIG_AFFS_FS is not set

# CONFIG_ECRYPT_FS is not set

# CONFIG_HFS_FS is not set

# CONFIG_HFSPLUS_FS is not set

# CONFIG_BEFS_FS is not set

# CONFIG_BFS_FS is not set

# CONFIG_EFS_FS is not set

# CONFIG_YAFFS_FS is not set

CONFIG_JFFS2_FS=y

CONFIG_JFFS2_FS_DEBUG=0

CONFIG_JFFS2_FS_WRITEBUFFER=y

# CONFIG_JFFS2_FS_WBUF_VERIFY is not set

# CONFIG_JFFS2_SUMMARY is not set

# CONFIG_JFFS2_FS_XATTR is not set

CONFIG_JFFS2_COMPRESSION_OPTIONS=y

CONFIG_JFFS2_ZLIB=y

CONFIG_JFFS2_LZO=y

CONFIG_JFFS2_RTIME=y

CONFIG_JFFS2_RUBIN=y

# CONFIG_JFFS2_CMODE_NONE is not set

CONFIG_JFFS2_CMODE_PRIORITY=y

# CONFIG_JFFS2_CMODE_SIZE is not set

# CONFIG_JFFS2_CMODE_FAVOURLZO is not set

CONFIG_UBIFS_FS=y

CONFIG_UBIFS_FS_ADVANCED_COMPR=y

CONFIG_UBIFS_FS_LZO=y

CONFIG_UBIFS_FS_ZLIB=y

# CONFIG_LOGFS is not set

# CONFIG_CRAMFS is not set

# CONFIG_SQUASHFS is not set

# CONFIG_VXFS_FS is not set

# CONFIG_MINIX_FS is not set

# CONFIG_OMFS_FS is not set

# CONFIG_HPFS_FS is not set

# CONFIG_QNX4FS_FS is not set

# CONFIG_QNX6FS_FS is not set

# CONFIG_ROMFS_FS is not set

# CONFIG_PSTORE is not set

# CONFIG_SYSV_FS is not set

# CONFIG_UFS_FS is not set

# CONFIG_F2FS_FS is not set

# CONFIG_AUFS_FS is not set

CONFIG_NETWORK_FILESYSTEMS=y

CONFIG_NFS_FS=y

CONFIG_NFS_V2=y

CONFIG_NFS_DEF_FILE_IO_SIZE=4096

CONFIG_NFS_V3=y

CONFIG_NFS_V3_ACL=y

CONFIG_NFS_V4=y

# CONFIG_NFS_SWAP is not set

# CONFIG_NFS_V4_1 is not set

CONFIG_ROOT_NFS=y

# CONFIG_NFS_USE_LEGACY_DNS is not set

CONFIG_NFS_USE_KERNEL_DNS=y

# CONFIG_NFSD is not set

CONFIG_LOCKD=y

CONFIG_LOCKD_V4=y

CONFIG_NFS_ACL_SUPPORT=y

CONFIG_NFS_COMMON=y

CONFIG_SUNRPC=y

CONFIG_SUNRPC_GSS=y

# CONFIG_SUNRPC_DEBUG is not set

# CONFIG_CEPH_FS is not set

# CONFIG_CIFS is not set

# CONFIG_NCP_FS is not set

# CONFIG_CODA_FS is not set

# CONFIG_AFS_FS is not set

CONFIG_NLS=y

CONFIG_NLS_DEFAULT="iso8859-1"

CONFIG_NLS_CODEPAGE_437=y

# CONFIG_NLS_CODEPAGE_737 is not set

# CONFIG_NLS_CODEPAGE_775 is not set

CONFIG_NLS_CODEPAGE_850=y

# CONFIG_NLS_CODEPAGE_852 is not set

# CONFIG_NLS_CODEPAGE_855 is not set

# CONFIG_NLS_CODEPAGE_857 is not set

# CONFIG_NLS_CODEPAGE_860 is not set

# CONFIG_NLS_CODEPAGE_861 is not set

# CONFIG_NLS_CODEPAGE_862 is not set

# CONFIG_NLS_CODEPAGE_863 is not set

# CONFIG_NLS_CODEPAGE_864 is not set

# CONFIG_NLS_CODEPAGE_865 is not set

# CONFIG_NLS_CODEPAGE_866 is not set

# CONFIG_NLS_CODEPAGE_869 is not set

# CONFIG_NLS_CODEPAGE_936 is not set

# CONFIG_NLS_CODEPAGE_950 is not set

# CONFIG_NLS_CODEPAGE_932 is not set

# CONFIG_NLS_CODEPAGE_949 is not set

# CONFIG_NLS_CODEPAGE_874 is not set

# CONFIG_NLS_ISO8859_8 is not set

# CONFIG_NLS_CODEPAGE_1250 is not set

# CONFIG_NLS_CODEPAGE_1251 is not set

# CONFIG_NLS_ASCII is not set

CONFIG_NLS_ISO8859_1=y

# CONFIG_NLS_ISO8859_2 is not set

# CONFIG_NLS_ISO8859_3 is not set

# CONFIG_NLS_ISO8859_4 is not set

# CONFIG_NLS_ISO8859_5 is not set

# CONFIG_NLS_ISO8859_6 is not set

# CONFIG_NLS_ISO8859_7 is not set

# CONFIG_NLS_ISO8859_9 is not set

# CONFIG_NLS_ISO8859_13 is not set

# CONFIG_NLS_ISO8859_14 is not set

CONFIG_NLS_ISO8859_15=y

# CONFIG_NLS_KOI8_R is not set

# CONFIG_NLS_KOI8_U is not set

# CONFIG_NLS_MAC_ROMAN is not set

# CONFIG_NLS_MAC_CELTIC is not set

# CONFIG_NLS_MAC_CENTEURO is not set

# CONFIG_NLS_MAC_CROATIAN is not set

# CONFIG_NLS_MAC_CYRILLIC is not set

# CONFIG_NLS_MAC_GAELIC is not set

# CONFIG_NLS_MAC_GREEK is not set

# CONFIG_NLS_MAC_ICELAND is not set

# CONFIG_NLS_MAC_INUIT is not set

# CONFIG_NLS_MAC_ROMANIAN is not set

# CONFIG_NLS_MAC_TURKISH is not set

# CONFIG_NLS_UTF8 is not set

#

# Kernel hacking

#

CONFIG_PRINTK_TIME=y

CONFIG_DEFAULT_MESSAGE_LOGLEVEL=4

CONFIG_ENABLE_WARN_DEPRECATED=y

CONFIG_ENABLE_MUST_CHECK=y

CONFIG_FRAME_WARN=2048

CONFIG_MAGIC_SYSRQ=y

# CONFIG_STRIP_ASM_SYMS is not set

# CONFIG_READABLE_ASM is not set

CONFIG_UNUSED_SYMBOLS=y

CONFIG_DEBUG_FS=y

# CONFIG_HEADERS_CHECK is not set

# CONFIG_DEBUG_SECTION_MISMATCH is not set

CONFIG_DEBUG_KERNEL=y

# CONFIG_DEBUG_SHIRQ is not set

CONFIG_LOCKUP_DETECTOR=y

# CONFIG_BOOTPARAM_SOFTLOCKUP_PANIC is not set

CONFIG_BOOTPARAM_SOFTLOCKUP_PANIC_VALUE=0

# CONFIG_PANIC_ON_OOPS is not set

CONFIG_PANIC_ON_OOPS_VALUE=0

CONFIG_DETECT_HUNG_TASK=y

CONFIG_DEFAULT_HUNG_TASK_TIMEOUT=120

# CONFIG_BOOTPARAM_HUNG_TASK_PANIC is not set

CONFIG_BOOTPARAM_HUNG_TASK_PANIC_VALUE=0

CONFIG_SCHED_DEBUG=y

# CONFIG_SCHEDSTATS is not set

CONFIG_TIMER_STATS=y

# CONFIG_DEBUG_OBJECTS is not set

# CONFIG_SLUB_DEBUG_ON is not set

# CONFIG_SLUB_STATS is not set

CONFIG_HAVE_DEBUG_KMEMLEAK=y

# CONFIG_DEBUG_KMEMLEAK is not set

# CONFIG_DEBUG_RT_MUTEXES is not set

# CONFIG_RT_MUTEX_TESTER is not set

CONFIG_DEBUG_SPINLOCK=y

CONFIG_DEBUG_MUTEXES=y

CONFIG_DEBUG_LOCK_ALLOC=y

CONFIG_PROVE_LOCKING=y

CONFIG_LOCKDEP=y

# CONFIG_LOCK_STAT is not set

# CONFIG_DEBUG_LOCKDEP is not set

CONFIG_TRACE_IRQFLAGS=y

# CONFIG_DEBUG_ATOMIC_SLEEP is not set

# CONFIG_DEBUG_LOCKING_API_SELFTESTS is not set

CONFIG_STACKTRACE=y

# CONFIG_DEBUG_STACK_USAGE is not set

# CONFIG_DEBUG_KOBJECT is not set

CONFIG_DEBUG_BUGVERBOSE=y

CONFIG_DEBUG_INFO=y

# CONFIG_DEBUG_INFO_REDUCED is not set

# CONFIG_DEBUG_VM is not set

# CONFIG_DEBUG_WRITECOUNT is not set

# CONFIG_DEBUG_MEMORY_INIT is not set

# CONFIG_DEBUG_LIST is not set

# CONFIG_TEST_LIST_SORT is not set

# CONFIG_DEBUG_SG is not set

# CONFIG_DEBUG_NOTIFIERS is not set

# CONFIG_DEBUG_CREDENTIALS is not set

# CONFIG_BOOT_PRINTK_DELAY is not set

#

# RCU Debugging

#

# CONFIG_PROVE_RCU is not set

# CONFIG_SPARSE_RCU_POINTER is not set

# CONFIG_RCU_TORTURE_TEST is not set

# CONFIG_RCU_TRACE is not set

# CONFIG_BACKTRACE_SELF_TEST is not set

# CONFIG_DEBUG_BLOCK_EXT_DEVT is not set

# CONFIG_DEBUG_FORCE_WEAK_PER_CPU is not set

# CONFIG_LKDTM is not set

# CONFIG_NOTIFIER_ERROR_INJECTION is not set

# CONFIG_FAULT_INJECTION is not set

# CONFIG_LATENCYTOP is not set

# CONFIG_DEBUG_PAGEALLOC is not set

CONFIG_NOP_TRACER=y

CONFIG_HAVE_FUNCTION_TRACER=y

CONFIG_HAVE_FUNCTION_GRAPH_TRACER=y

CONFIG_HAVE_DYNAMIC_FTRACE=y

CONFIG_HAVE_FTRACE_MCOUNT_RECORD=y

CONFIG_HAVE_SYSCALL_TRACEPOINTS=y

CONFIG_HAVE_C_RECORDMCOUNT=y

CONFIG_TRACE_CLOCK=y

CONFIG_RING_BUFFER=y

CONFIG_EVENT_TRACING=y

CONFIG_CONTEXT_SWITCH_TRACER=y

CONFIG_TRACING=y

CONFIG_GENERIC_TRACER=y

CONFIG_TRACING_SUPPORT=y

CONFIG_FTRACE=y

# CONFIG_FUNCTION_TRACER is not set

# CONFIG_IRQSOFF_TRACER is not set

# CONFIG_SCHED_TRACER is not set

# CONFIG_FTRACE_SYSCALLS is not set

# CONFIG_TRACER_SNAPSHOT is not set

CONFIG_BRANCH_PROFILE_NONE=y

# CONFIG_PROFILE_ANNOTATED_BRANCHES is not set

# CONFIG_PROFILE_ALL_BRANCHES is not set

# CONFIG_STACK_TRACER is not set

CONFIG_BLK_DEV_IO_TRACE=y

# CONFIG_PROBE_EVENTS is not set

# CONFIG_FTRACE_STARTUP_TEST is not set

# CONFIG_RING_BUFFER_BENCHMARK is not set

# CONFIG_RING_BUFFER_STARTUP_TEST is not set

# CONFIG_RBTREE_TEST is not set

# CONFIG_INTERVAL_TREE_TEST is not set

# CONFIG_DYNAMIC_DEBUG is not set

# CONFIG_DMA_API_DEBUG is not set

# CONFIG_ATOMIC64_SELFTEST is not set

# CONFIG_SAMPLES is not set

CONFIG_HAVE_ARCH_KGDB=y

# CONFIG_KGDB is not set

# CONFIG_TEST_STRING_HELPERS is not set

# CONFIG_TEST_KSTRTOX is not set

CONFIG_STRICT_DEVMEM=y

CONFIG_ARM_UNWIND=y

CONFIG_DEBUG_USER=y

# CONFIG_DEBUG_LL is not set

CONFIG_DEBUG_LL_INCLUDE="mach/debug-macro.S"

CONFIG_UNCOMPRESS_INCLUDE="debug/uncompress.h"

# CONFIG_OC_ETM is not set

#

# Security options

#

CONFIG_KEYS=y

# CONFIG_ENCRYPTED_KEYS is not set

# CONFIG_KEYS_DEBUG_PROC_KEYS is not set

# CONFIG_SECURITY_DMESG_RESTRICT is not set

# CONFIG_SECURITY is not set

# CONFIG_SECURITYFS is not set

CONFIG_DEFAULT_SECURITY_DAC=y

CONFIG_DEFAULT_SECURITY=""

CONFIG_CRYPTO=y

#

# Crypto core or helper

#

# CONFIG_CRYPTODEV is not set

CONFIG_CRYPTO_ALGAPI=y

CONFIG_CRYPTO_ALGAPI2=y

CONFIG_CRYPTO_HASH=y

CONFIG_CRYPTO_HASH2=y

# CONFIG_CRYPTO_MANAGER is not set

# CONFIG_CRYPTO_MANAGER2 is not set

# CONFIG_CRYPTO_USER is not set

# CONFIG_CRYPTO_GF128MUL is not set

# CONFIG_CRYPTO_NULL is not set

# CONFIG_CRYPTO_CRYPTD is not set

# CONFIG_CRYPTO_AUTHENC is not set

# CONFIG_CRYPTO_TEST is not set

#

# Authenticated Encryption with Associated Data

#

# CONFIG_CRYPTO_CCM is not set

# CONFIG_CRYPTO_GCM is not set

# CONFIG_CRYPTO_SEQIV is not set

#

# Block modes

#

# CONFIG_CRYPTO_CBC is not set

# CONFIG_CRYPTO_CTR is not set

# CONFIG_CRYPTO_CTS is not set

# CONFIG_CRYPTO_ECB is not set

# CONFIG_CRYPTO_LRW is not set

# CONFIG_CRYPTO_PCBC is not set

# CONFIG_CRYPTO_XTS is not set

#

# Hash modes

#

# CONFIG_CRYPTO_CMAC is not set

# CONFIG_CRYPTO_HMAC is not set

# CONFIG_CRYPTO_XCBC is not set

# CONFIG_CRYPTO_VMAC is not set

#

# Digest

#

CONFIG_CRYPTO_CRC32C=y

# CONFIG_CRYPTO_CRC32 is not set

# CONFIG_CRYPTO_GHASH is not set

# CONFIG_CRYPTO_MD4 is not set

CONFIG_CRYPTO_MD5=y

# CONFIG_CRYPTO_MICHAEL_MIC is not set

# CONFIG_CRYPTO_RMD128 is not set

# CONFIG_CRYPTO_RMD160 is not set

# CONFIG_CRYPTO_RMD256 is not set

# CONFIG_CRYPTO_RMD320 is not set

# CONFIG_CRYPTO_SHA1 is not set

# CONFIG_CRYPTO_SHA1_ARM is not set

# CONFIG_CRYPTO_SHA256 is not set

# CONFIG_CRYPTO_SHA512 is not set

# CONFIG_CRYPTO_TGR192 is not set

# CONFIG_CRYPTO_WP512 is not set

#

# Ciphers

#

CONFIG_CRYPTO_AES=y

# CONFIG_CRYPTO_AES_ARM is not set

# CONFIG_CRYPTO_ANUBIS is not set

# CONFIG_CRYPTO_ARC4 is not set

# CONFIG_CRYPTO_BLOWFISH is not set

# CONFIG_CRYPTO_CAMELLIA is not set

# CONFIG_CRYPTO_CAST5 is not set

# CONFIG_CRYPTO_CAST6 is not set

# CONFIG_CRYPTO_DES is not set

# CONFIG_CRYPTO_FCRYPT is not set

# CONFIG_CRYPTO_KHAZAD is not set

# CONFIG_CRYPTO_SALSA20 is not set

# CONFIG_CRYPTO_SEED is not set

# CONFIG_CRYPTO_SERPENT is not set

# CONFIG_CRYPTO_TEA is not set

# CONFIG_CRYPTO_TWOFISH is not set

#

# Compression

#

CONFIG_CRYPTO_DEFLATE=y

# CONFIG_CRYPTO_ZLIB is not set

CONFIG_CRYPTO_LZO=y

#

# Random Number Generation

#

# CONFIG_CRYPTO_ANSI_CPRNG is not set

# CONFIG_CRYPTO_USER_API_HASH is not set

# CONFIG_CRYPTO_USER_API_SKCIPHER is not set

# CONFIG_CRYPTO_HW is not set

# CONFIG_ASYMMETRIC_KEY_TYPE is not set

CONFIG_BINARY_PRINTF=y

#

# Library routines

#

CONFIG_BITREVERSE=y

CONFIG_GENERIC_STRNCPY_FROM_USER=y

CONFIG_GENERIC_STRNLEN_USER=y

CONFIG_GENERIC_PCI_IOMAP=y

CONFIG_GENERIC_IO=y

CONFIG_STMP_DEVICE=y

# CONFIG_CRC_CCITT is not set

CONFIG_CRC16=y

CONFIG_CRC_T10DIF=y

CONFIG_CRC_ITU_T=m

CONFIG_CRC32=y

# CONFIG_CRC32_SELFTEST is not set

CONFIG_CRC32_SLICEBY8=y

# CONFIG_CRC32_SLICEBY4 is not set

# CONFIG_CRC32_SARWATE is not set

# CONFIG_CRC32_BIT is not set

CONFIG_CRC7=m

CONFIG_LIBCRC32C=m

# CONFIG_CRC8 is not set

CONFIG_ZLIB_INFLATE=y

CONFIG_ZLIB_DEFLATE=y

CONFIG_LZO_COMPRESS=y

CONFIG_LZO_DECOMPRESS=y

# CONFIG_XZ_DEC is not set

# CONFIG_XZ_DEC_BCJ is not set

CONFIG_TEXTSEARCH=y

CONFIG_TEXTSEARCH_KMP=m

CONFIG_TEXTSEARCH_BM=m

CONFIG_TEXTSEARCH_FSM=m

CONFIG_HAS_IOMEM=y

CONFIG_HAS_IOPORT=y

CONFIG_HAS_DMA=y

CONFIG_DQL=y

CONFIG_NLATTR=y

CONFIG_GENERIC_ATOMIC64=y

CONFIG_ARCH_HAS_ATOMIC64_DEC_IF_POSITIVE=y

# CONFIG_AVERAGE is not set

# CONFIG_CORDIC is not set

# CONFIG_DDR is not set

CONFIG_OID_REGISTRY=y

# CONFIG_VIRTUALIZATION is not set

0 项奖励
回复