i.MX28 WDT reset rarely failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX28 WDT reset rarely failed

1,094 Views
torus1000
Contributor V

Hi,
I tested i.MX28 WDT reset then I found boot failure around once per 500~1000 times.

Observed conditions were as following:
     * Kept on supply 5V to VDD5V
     * Internal LDO outputs droped 1.5 to 1.1@VDDD, 1.5 to1.1V@VDDA and 3.3 to 3.1V@VDDIO.
     * No charactor or no error message sent to the console.
     * GPIO kept initial state

Can anyone explain what happend?  

I couldn't find such errata. It looks stack at on the way to boot up.
In fact some articles in community reported WDT issue via Power down such as
http://lists.infradead.org/pipermail/barebox/2013-February/012839.html

Will anyone please let me know how to avoid this?

Thanks.

Labels (1)
Tags (4)
4 Replies

883 Views
YixingKong
Senior Contributor IV

Torus

Had your issues resolved? If yes, please close this DI, otherwse please reply here with your unresolved issues.

Thanks,

Yixing

0 Kudos
Reply

883 Views
lategoodbye
Senior Contributor I

Hi Torus,

could you please explain which Kernel version and bootloader you are using?

BR Stefan

0 Kudos
Reply

883 Views
torus1000
Contributor V

Dear Stefan,

Thank you for your quick reply.

I'm using u-boot-2009.08 and L2.6.35.

Have you ever heard such rare issue?

BR Torus

0 Kudos
Reply

883 Views
lategoodbye
Senior Contributor I

Hi Torus,

it's hard to distinguish between software or hardware problem.

Is it possible for you to test it with current Mainline Kernel and current U-Boot?