iMX280 : EMI Input voltage low (VLI) value

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX280 : EMI Input voltage low (VLI) value

ソリューションへジャンプ
1,471件の閲覧回数
koichisakagami
Contributor II

Dear community,

I am checking the i.MX28 Data Sheet (IMX28CEC Rev3 07/2012) .
Please see Table 22 EMI Digital Pin DC Characteristics.
It says that the VIL value is 0.3V .

I think that the VIL value is -0.3V.

Which is correct ?

Best Regards,
Koichi Sakagami

ラベル(1)
0 件の賞賛
返信
1 解決策
1,382件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi koichi

sorry, I misunderstood original question,

yes you are right in original post that correct reading

would be:

VIL value is -0.3V (Min.)

Best regards

igor

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,382件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi koichi

correct is VIL value is 0.3V (Min.)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,382件の閲覧回数
koichisakagami
Contributor II

Dear igor san,

Thank you for your reply.

As the VIL value is 0.3V ( Min),

it is not recognized that the Zero Voltage input is the Logical Low.

Is my understanding correct ?

Best Regards,

Koichi Sakagami

0 件の賞賛
返信
1,383件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi koichi

sorry, I misunderstood original question,

yes you are right in original post that correct reading

would be:

VIL value is -0.3V (Min.)

Best regards

igor

0 件の賞賛
返信