i.MX28 EVK JTAG Debugging

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX28 EVK JTAG Debugging

1,802件の閲覧回数
bipulpandey
Contributor III

I want to debug the software through JTAG on i.MX28 Evk Board (https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/i-mx28-evaluati...

I am using J-link segger plus for the same. my hardware connection is correct but not able to download the image on the target. I am using eclipse as IDE.

Please provide any reference configuration file or help document.

Is J-link Segger plus support on i.MX28 ?

ラベル(1)
0 件の賞賛
返信
1 返信

1,786件の閲覧回数
Yuri
NXP Employee
NXP Employee

@bipulpandey 
Hello,

  the following may be helpful:

https://community.nxp.com/t5/i-MX-Processors/Whic-JTAG-tool-for-IMX28/m-p/311381

  To debug, using JTAG, we must enter special boot mode (Wait JTAG connection).
To debug the i.MX28/23, you must boot it in boot mode 6. In this mode, the boot ROM will enable
the JTAG pins and go into a two- instruction infinite loop, waiting for the debugger to release it.

Regards,
Yuri.

0 件の賞賛
返信