i.MX28 DDR2 SDRAM address space mapping (esp. chip select mapping)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX28 DDR2 SDRAM address space mapping (esp. chip select mapping)

Jump to solution
2,480 Views
dimitarboevski
Contributor II

Hello engineers :-)

I have a strange issue.

I have one DDR2 memory chip with 13 address pins, 10 column pins, 8 banks and 16-bit width.

As far as I understand the manual my register configuration should be:

HW_DRAM_CTL29:

CS_MAP=0x0

COLUMN_SIZE=0x2  // 12 - 2 = 10

ADDR_PINS=0x2  // 15 - 2 =13

HW_DRAM_CTL31:

EIGHT_BANK_MODE=0x1

and of course lots of other registers, but the above are the ones i'm currently interested in.  I have disabled the EMI_CE1N pin and disabled the last two address pins. The above configuration doesn't work but as soon as i change CS_MAP to 0xf it works! How come? I have one chip only. My EMI_CE0N pin is connected to the memory chip select, the EMI_CE1N pin is not connected at all. How come mapping over nonexistent chip selects works while the correct configuration doesn't, what am I missing?

Besides, i don't get it how CS_MAP allows for a value of 0xf for enabling the mapping of 4 chip selects when the i.MX28 has only two chip selects on the EMI interface?! Where are the other two chip selects?

Labels (2)
0 Kudos
Reply
1 Solution
1,998 Views
Yuri
NXP Employee
NXP Employee

> Which means the valid values should be 0, 2, 4 and 8.

Really : 1,2,4,8  :-)

View solution in original post

0 Kudos
Reply
4 Replies
1,998 Views
Yuri
NXP Employee
NXP Employee

CS_MAP should not be zero :

1 for Chip Select 0

2 for Chip Select 1

3 for both Chip Selects 11

Please use DDR Excel table  :Board bring-up and DDR initialization tools

0 Kudos
Reply
1,998 Views
dimitarboevski
Contributor II

I did try setting it to 1 and to other values as well but works only when set to 0xf. By the way the reference manual says the number of selected chip selects should be a power of 2. Which makes sense since to map the chips selects as an extra address bit they should be indeed a power of two. Which means the valid values should be 0, 2, 4 and 8. I've read the programming aid you are referring to and it just adds more to the confusion how the CS_MAP value is used.

0 Kudos
Reply
1,999 Views
Yuri
NXP Employee
NXP Employee

> Which means the valid values should be 0, 2, 4 and 8.

Really : 1,2,4,8  :-)

0 Kudos
Reply
1,998 Views
Yuri
NXP Employee
NXP Employee

I just tried to init i.MX28 EVK with CS_MAP=0x1  - memory works !