i.MX257PDK with Capacitive touch Screen

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX257PDK with Capacitive touch Screen

1,331 Views
akshayynarayana
Contributor I

Does i.MX257PDK support 5.7' TFT LCD with Capacitive touch Screen or is any specific BSP to be installed for it?

Labels (2)
0 Kudos
Reply
1 Reply

1,209 Views
igorpadykov
NXP Employee
NXP Employee

Hi Akshayy

Freescale BSP L2.6.31_09.12.00_SDK_SOURCE

supports only resistive touch panel with CPT VGA panel supplied with PDK,

touch driver is described in Chapter 15 Touch Screen and ADC Drivers

Linux Manual included in IMX25_0912_SDK_LINUXDOCS_BUNDLE

Other touch panels also may be supported, provided that its driver will be addded to BSP.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply