i.MX257PDK with Capacitive touch Screen

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX257PDK with Capacitive touch Screen

1,357件の閲覧回数
akshayynarayana
Contributor I

Does i.MX257PDK support 5.7' TFT LCD with Capacitive touch Screen or is any specific BSP to be installed for it?

ラベル(2)
0 件の賞賛
返信
1 返信

1,235件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Akshayy

Freescale BSP L2.6.31_09.12.00_SDK_SOURCE

supports only resistive touch panel with CPT VGA panel supplied with PDK,

touch driver is described in Chapter 15 Touch Screen and ADC Drivers

Linux Manual included in IMX25_0912_SDK_LINUXDOCS_BUNDLE

Other touch panels also may be supported, provided that its driver will be addded to BSP.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信