i.MX25 Serial Boot Configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX25 Serial Boot Configuration

2,039 Views
LI_Dave
Contributor III

I'm trying to boot a blank i.MX25 using the UART boot mode and have a question about what external boot pins really matter in this case. 

I of course have BOOT_MODE_0 and BOOT_MODE_1 pulled high to select UART/USB Boot.  I've also got the three BT_UART_SRC lines pulled LOW to select UART1.  It would appear that nearly all the other boot config pin states are irrelevant to UART boot, but I'm not so sure about the BT_LPB_FREQ pins which configure the Low Power Boot mode.  Do they need to be set correctly (111)  to ensure successful UART boot?   Is there anything else that needs to be tied to force a UART 1 Boot?

Thanks,

Dave

Labels (1)
0 Kudos
Reply
2 Replies

1,872 Views
Yuri
NXP Employee
NXP Employee

General approach is as following - It is recommended to provide (proper / reasonable) configuration for all boot pins,

do not leave some of them free. 

1,872 Views
LI_Dave
Contributor III

Yuri, thanks for the reply I understand that is what is recommended.  Given the choice I would follow the PDK schematic.   I have a board though that is NOT as recommended (not my design) and I'm trying to understand if it will properly serial boot or not. 

0 Kudos
Reply