i.MX25 - SDIO WIFI not detected

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX25 - SDIO WIFI not detected

3,718 次查看
re_chinelatto
Contributor I

Hi,

I have a custom board with Linux v2.6 running perfectly. I am updating Linux (Yocto-thud) and I will configure another SDIO wifi module. I tried communication with the 2 SDIO WIFI modules, but it´s not detected.

I changed the dts:

&esdhc2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_esdhc2>;
#address-cells = <0x1>;
#size-cells = <0x0>;
status = "okay";

esdhc@1 {
compatible = "silabs,wfx-sdio,fsl,imx25-esdhc";
reg = <1>;
pinctrl-names = "default";
};
};
...

pinctrl_esdhc2: esdhc2grp {
fsl,pins = <
MX25_PAD_CSI_D6__SDHC2_CMD 0x80000000
MX25_PAD_CSI_D7__ESDHC2_CLK 0x80000000
MX25_PAD_CSI_MCLK__SDHC2_DAT0 0x80000000
MX25_PAD_CSI_VSYNC__ESDHC2_DAT1 0x80000000
MX25_PAD_CSI_HSYNC__SDHC2_DAT2 0x80000000
MX25_PAD_CSI_PIXCLK__SDHC2_DAT3 0x80000000
>;
};

At startup is displayed:

...
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
sdhci-esdhc-imx 53fb4000.esdhc: Got CD GPIO
sdhci-esdhc-imx 53fb4000.esdhc: Got WP GPIO
mmc0 bounce up to 128 segments into one, max segment size 65536 bytes
mmc0: SDHCI controller on 53fb4000.esdhc [53fb4000.esdhc] using DMA
mmc1 bounce up to 128 segments into one, max segment size 65536 bytes
mmc1: SDHCI controller on 53fb8000.esdhc [53fb8000.esdhc] using DMA
mmc0: new high speed SDHC card at address aaaa
mmcblk0: mmc0:aaaa SS08G 7.40 GiB
mmcblk0: p1
...

The message "mmc1: new high speed SDIO card at address ..." is not displayed

I checked the communication with mmc:

echo 1 > /sys/kernel/debug/tracing/events/mmc/mmc_request_done/enable
echo 'cmd_opcode != 53' > /sys/kernel/debug/tracing/events/mmc/mmc_request_done/filter
cat /sys/kernel/debug/tracing/trace_pipe | grep mmc1 > log.txt &
echo 53fb8000.esdhc > /sys/bus/platform/drivers/sdhci-esdhc-imx/unbind
sleep 2
echo 53fb8000.esdhc > /sys/bus/platform/drivers/sdhci-esdhc-imx/bind

All commands (except 0x00) return cmd_err = -110. Checking in a logic analyzer, I see the commands sent in the 400's, 300's, 200's and 100's KHz. I tried several changes to the dts, but no sucess.

Any idea how to debug or resolve this problem?

标签 (3)
标记 (3)
0 项奖励
回复
3 回复数

3,364 次查看
re_chinelatto
Contributor I

After a long time, I returned to this project.

I fixed a power problem and the Linux detects SDIO:

mmc1: new high speed SDIO card at address fffd

But there is no communication;

            wfx: loading out-of-tree module taints kernel.

wfx: Silicon Labs WFX_2.2.1

wfx-sdio mmc1:0001:1: bad hardware revision number: 4

I tried a redpine´s module and it didn´t work either:

rsi_91x: rsi_probe: ***** 9116 Module *****
rsi_91x: rsi_hal_device_init: oper_mode = 1, coex_mode = 1
rsi_91x: rsi_load_firmware: REGOUT read timedout
rsi_91x: rsi_load_firmware: Soft boot loader not present
rsi_91x: rsi_hal_device_init: Failed to load TA instructions
rsi_91x: rsi_probe: Failed in device init
rsi_91x: set_clr_tx_intention,356: Wait event failed
rsi_91x: rsi_tx_scheduler_thread,560: Failed to get tx_access
rsi_91x: rsi_probe: Failed in probe...Exiting
RSI-SDIO WLAN: probe of mmc1:fffd:1 failed with error 1

All drivers were compiled into the 4.20 kernel.

I lowered the clock speed to 12, 8 and 4 Mhz and didn´t work.

If I connected a SDIO Card it worked perfectly. I can write/read files with no problems.

I tried connect this 2 modules on another custom board (with i.MX6) and it worked.

How Can I solve this? 

0 项奖励
回复

3,364 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Renato

nxp does not support i.mx25 in latest linux bsps, in general one can try to debug it

using description of emmc/sd drivers in Linux Documentation
https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6ser...

Other reason may be that for used wifi module there is no driver for that linux version

(one can ask it from module vendor).

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

3,364 次查看
re_chinelatto
Contributor I

Hi, Igor,

Thanks for answering. I´ll try to debug it.

About the driver, I installed it. Acording to vendor, I need to see the message "mmc1: new high speed SDIO card at address ..." in dmesg.

0 项奖励
回复