i.MX25 LCD output disable

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX25 LCD output disable

跳至解决方案
1,119 次查看
torus1000
Contributor V

Hi,

I want to disable LCD output then I luckily found a LCDC_EN bit.
However this bit seems one of the clock gates.

Is it safe to stop this clock after LCDC initialization done?

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,033 次查看
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

yes safe. Also clock is enabled after all LCDC initialization is done,

as one can see in i.MX25 PDK splashscreen example lcd_ctrl_init()

uboot-imx.git - Freescale i.MX u-boot Tree

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,034 次查看
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

yes safe. Also clock is enabled after all LCDC initialization is done,

as one can see in i.MX25 PDK splashscreen example lcd_ctrl_init()

uboot-imx.git - Freescale i.MX u-boot Tree

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复