Hello All,
Recently, I got one 2GB SD card from market which always causes kernel oops when it is inserted to i.MX233 and i.MX28 EVK board. The error log from the i.MX28 is like this:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
mmc1: new high speed SD card at address b368
mmcblk1: mmc1:b368 SMI 1.87 GiB
mmcblk1:
kernel BUG at drivers/mmc/host/mxs-mmc.c:465!
Unable to handle kernel NULL pointer dereference at virtual address 00000000
pgd = c0004000
[00000000] *pgd=00000000
Internal error: Oops: 817 [#1] PREEMPT
last sysfs file: /sys/kernel/uevent_seqnum
Modules linked in:
CPU: 0 Not tainted (2.6.35.3-571-gcca29a0-g4792be1-dirty #321)
PC is at __bug+0x20/0x2c
LR is at release_console_sem+0x1b4/0x230
pc : [<c0031138>] lr : [<c004a07c>] psr: 60000013
sp : c75f7da8 ip : c75f7cd0 fp : c75f7db4
r10: 00000000 r9 : 01230000 r8 : 00000000
r7 : 00000001 r6 : 00001000 r5 : c75f7e84 r4 : c756d600
r3 : 00000000 r2 : 00000000 r1 : c0469b48 r0 : 00000034
Flags: nZCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel
Control: 0005317f Table: 47d28000 DAC: 00000017
Process mmcqd (pid: 2169, stack limit = 0xc75f6270)
Stack: (0xc75f7da8 to 0xc75f8000)
7da0: c75f7e04 c75f7db8 c0281ba0 c0031128 00000000 00000000
7dc0: 00000000 00000000 00000000 00000000 00000000 00000001 00000000 c756d600
7de0: c75f7e70 c756d400 00000001 c752e3c4 00000000 c75f7e70 c75f7e24 c75f7e08
7e00: c0282380 c0281974 c75f7e70 c756d400 c75f7e30 00000001 c75f7e54 c75f7e28
7e20: c0278fd8 c0282350 c75f7e54 00000000 c75f7e30 c75f7e30 c74a6340 c74a6340
7e40: c7cd6600 c75f6000 c75f7f8c c75f7e58 c028051c c0278ed0 00000000 00000000
7e60: 00000000 c75f7e84 00000000 00000000 c75f7e84 c75f7edc c75f7eb0 c75f7e2c
7e80: c027906c 00000012 00000000 00000000 00000000 00000000 00000000 000000b5
7ea0: 00000000 00000000 c75f7edc c75f7e70 0000000c 00000000 00000000 00000000
7ec0: 00000000 00000000 0000049d 00000000 00000000 00000000 c75f7e70 00000000
7ee0: 00000000 00000200 00000008 00000000 00000200 00000000 c75f7eb0 c75f7e70
7f00: 00000001 c7d20800 c01c9a18 c01c8d4c c75f7f3c c7797458 00000000 c7797498
7f20: c7c25cc0 c75f6000 c7564030 00000000 c75f6000 c7564030 c74a6340 c7564030
7f40: c75f7f74 c75f7f50 c74a6340 c752e3c4 c75f7f74 c75f7f60 c01ba694 c01c0160
7f60: c74a6340 c75f6000 c752e3c4 c752e3cc c7564030 00000001 00000000 c75641a0
7f80: c75f7fc4 c75f7f90 c02810bc c0280330 00000013 00000000 c75f7fc4 c7ca9d80
7fa0: c75f7fcc c0280f88 c752e3c4 00000000 00000000 00000000 c75f7ff4 c75f7fc8
7fc0: c0061688 c0280f98 00000000 00000000 c75f7fd0 c75f7fd0 c7ca9d80 c0061604
7fe0: c004d134 00000013 00000000 c75f7ff8 c004d134 c0061614 00000000 00000000
Backtrace:
[<c0031118>] (__bug+0x0/0x2c) from [<c0281ba0>] (mxs_mmc_start_cmd+0x23c/0x9dc)
[<c0281964>] (mxs_mmc_start_cmd+0x0/0x9dc) from [<c0282380>] (mxs_mmc_request+0x40/0x80)
[<c0282340>] (mxs_mmc_request+0x0/0x80) from [<c0278fd8>] (mmc_wait_for_req+0x118/0x130)
r7:00000001 r6:c75f7e30 r5:c756d400 r4:c75f7e70
[<c0278ec0>] (mmc_wait_for_req+0x0/0x130) from [<c028051c>] (mmc_blk_issue_rq+0x1fc/0x60c)
r6:c75f6000 r5:c7cd6600 r4:c74a6340
[<c0280320>] (mmc_blk_issue_rq+0x0/0x60c) from [<c02810bc>] (mmc_queue_thread+0x134/0x138)
[<c0280f88>] (mmc_queue_thread+0x0/0x138) from [<c0061688>] (kthread+0x84/0x8c)
[<c0061604>] (kthread+0x0/0x8c) from [<c004d134>] (do_exit+0x0/0x6dc)
r7:00000013 r6:c004d134 r5:c0061604 r4:c7ca9d80
Code: e1a01000 e59f000c eb0c803e e3a03000 (e5833000)
---[ end trace e8886db44828e727 ]---
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
The error is due to an invalid field in CSD register of this 2GB SD card. The CSD version of this card is 1.0 but the TAAC field is an invalid value 0. Since the kernel is making use of this TAAC field to calculate the SD card timeout, an invalid value 0 can lead to a oops error at mxs_ns_to_ssp_ticks().
This error is only found on this <=2GB SD card. >2GB SDHC cards will not see this error because these cards are CSD version 2.0. For these cards, kernel always use a fix timeout and calculation that causes the oops error is skipped. Of course, <=2GB SD card that fully complying to SD card physical layer specification will not see this error neither.
To solve this issue, please assign the TAAC field to its maximum value likes this attachment whenever the TAAC field is invalid.
Regards,
Peter
Original Attachment has been moved to: SD_card_invalid_TAAC.patch.zip