i.MX233 as USB device - HighSpeed Handshake Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX233 as USB device - HighSpeed Handshake Problem

Jump to solution
2,679 Views
mbergmann
Contributor II

Hi,


I'm trying to connect our own i.MX233 board as a USB Mass Storage device.

The software is all done ourselfe. No BSP.

Currently I‘m struggling with the HighSpeed Handshake:

The Handshake is looking like this:

   4   ,0:00.000.000,             ,<Host connected>,

FS,5   ,0:04.443.538,             ,<Full-speed>,

FS,6   ,0:04.623.206, 1.504.166 ms,<Reset> / <Chirp J> / <Tiny J>,

FS,7   ,0:04.624.710, 2.000.400 ms,<Chirp K>,

FS,8   ,0:04.626.711,    53.816 us,<Reset> / <Chirp J> / <Tiny J>,

FS,9   ,0:04.626.765,62.309.516 ms,[680 Chirp K-J pairs] [1 Chirp K],

FS,1372,0:04.689.074,   214.083 us,<Reset> / <Chirp J> / <Tiny J>,

HS,1373,0:04.689.288,             ,<High-speed> (Unexpected)

HS,1374,0:04.689.288,   744.733 us,CORRUPTED packet,01 D8 C6 FA DA

FS,1375,0:04.690.033,             ,<Full-speed>,

The USB is allways switching back to Full-speed.

If I start the board in recovery mode I got a propper handshake and a working HID device (and loading software with sb_loader  works fine), so I assume its my software and not the hardware.

Anybody seen this before? Is there a example how to set up the USB as device?

Thanks

Mike

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,209 Views
MarekVasut
Senior Contributor I

The USB IP block is really ChipIdea CI13xxx, you might want to poke around that.

View solution in original post

0 Kudos
Reply
2 Replies
2,210 Views
MarekVasut
Senior Contributor I

The USB IP block is really ChipIdea CI13xxx, you might want to poke around that.

0 Kudos
Reply
2,209 Views
mbergmann
Contributor II

Thanks, that helped. Had problems initializing the cell. Now the handshake is correct.

0 Kudos
Reply