i.MX dual/quad Applications Processor Boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX dual/quad Applications Processor Boot

2,863 Views
nvs
Contributor I

Is it possible to load and boot images from different devices(NAND and NOR)

for different cores.Say i want to load and boot image for Cortex-M4 from NOR

and Cortex-A35 from NAND?

Labels (2)
0 Kudos
Reply
3 Replies

2,243 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nishanth

please look on

Boot The i.mx6 dual With Linux+uC/OS-II AMP 

i.MX6DQ/SDL boot always from primary core.

For i.MX7 image for Cortex-M4 should be loaded by Cortex-A7,

NXP BSPs on link below support FreeRTOS running on M4 core:

https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6ser...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,243 Views
nvs
Contributor I

Thanks Igor.

Iam working on the IMX8 DQ and the datasheet mentions it can supports Multi-image boot (System Controller firmware, Cortex-M4 image, and Cortex-A35 image).My understanding was these cores can boot parallel.

Sorry for not being specific.

0 Kudos
Reply

2,243 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nishanth

I am not aware of "IMX8 DQ" parts. Currently publicly released and supported only i.MX8M family:
i.MX 8M Applications Processor | Arm Cortex-A53, Cortex-M4|NXP 
Other i.MX8 families are not officially released yet and not supported, sorry.

Best regards
igor

0 Kudos
Reply