i.MX RT1170 external input clock requirements

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX RT1170 external input clock requirements

跳至解决方案
1,221 次查看
Eugene3
Contributor II

I'm designing RT1170 application and planning to use an external oscillator for 24MHz on XTALI instead of a crystal.

Would  you tell me the requirements of external oscillator? Frequency stability (ppm), output load, jitter and etc.

0 项奖励
回复
1 解答
1,204 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Eugene3,

As long as the external 24MHz oscillator complies with the description seen in "Table 4. Clocks configurations" of the Hardware Development Guide for the MIMXRT1160/1170 Processor, you will be OK. As you can see, the restrictions mostly depend on whether or not you are using USB and/or Ethernet.

Let me know if this helps.

BR,
Edwin.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,205 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Eugene3,

As long as the external 24MHz oscillator complies with the description seen in "Table 4. Clocks configurations" of the Hardware Development Guide for the MIMXRT1160/1170 Processor, you will be OK. As you can see, the restrictions mostly depend on whether or not you are using USB and/or Ethernet.

Let me know if this helps.

BR,
Edwin.

0 项奖励
回复
1,193 次查看
Eugene3
Contributor II

Hi @EdwinHz 

Thank you, I got it.

0 项奖励
回复