i.MX RT1170 external input clock requirements

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX RT1170 external input clock requirements

ソリューションへジャンプ
1,251件の閲覧回数
Eugene3
Contributor II

I'm designing RT1170 application and planning to use an external oscillator for 24MHz on XTALI instead of a crystal.

Would  you tell me the requirements of external oscillator? Frequency stability (ppm), output load, jitter and etc.

0 件の賞賛
返信
1 解決策
1,234件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Eugene3,

As long as the external 24MHz oscillator complies with the description seen in "Table 4. Clocks configurations" of the Hardware Development Guide for the MIMXRT1160/1170 Processor, you will be OK. As you can see, the restrictions mostly depend on whether or not you are using USB and/or Ethernet.

Let me know if this helps.

BR,
Edwin.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,235件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Eugene3,

As long as the external 24MHz oscillator complies with the description seen in "Table 4. Clocks configurations" of the Hardware Development Guide for the MIMXRT1160/1170 Processor, you will be OK. As you can see, the restrictions mostly depend on whether or not you are using USB and/or Ethernet.

Let me know if this helps.

BR,
Edwin.

0 件の賞賛
返信
1,223件の閲覧回数
Eugene3
Contributor II

Hi @EdwinHz 

Thank you, I got it.

0 件の賞賛
返信