i.MX RT1170 external input clock requirements

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT1170 external input clock requirements

Jump to solution
1,213 Views
Eugene3
Contributor II

I'm designing RT1170 application and planning to use an external oscillator for 24MHz on XTALI instead of a crystal.

Would  you tell me the requirements of external oscillator? Frequency stability (ppm), output load, jitter and etc.

0 Kudos
Reply
1 Solution
1,196 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Eugene3,

As long as the external 24MHz oscillator complies with the description seen in "Table 4. Clocks configurations" of the Hardware Development Guide for the MIMXRT1160/1170 Processor, you will be OK. As you can see, the restrictions mostly depend on whether or not you are using USB and/or Ethernet.

Let me know if this helps.

BR,
Edwin.

View solution in original post

0 Kudos
Reply
2 Replies
1,197 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Eugene3,

As long as the external 24MHz oscillator complies with the description seen in "Table 4. Clocks configurations" of the Hardware Development Guide for the MIMXRT1160/1170 Processor, you will be OK. As you can see, the restrictions mostly depend on whether or not you are using USB and/or Ethernet.

Let me know if this helps.

BR,
Edwin.

0 Kudos
Reply
1,185 Views
Eugene3
Contributor II

Hi @EdwinHz 

Thank you, I got it.

0 Kudos
Reply