i.MX RT1170 Custom Bootloader

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX RT1170 Custom Bootloader

1,954 次查看
joséviníciusmel
Contributor II

Hi guys,

I will develop a custom bootloader in my custom i.MX RT1170 board. In my case, a flash driver will be read through the USB to update the primary application.

I am studying the "evkmimxrt1170_mcuboot_opensource" and the "ota" examples and I have some doubts and I would appreciate some help.

1) Application jump: I tried to study the "evkmimxrt1170_mcuboot_opensource" example but I don't have the i.MX RT1170 evaluation board to debug. I think that the steps to jump are the following:

// Cleanup:

SCB_DisableICache();
SCB_DisableDCache();
ARM_MPU_Disable();

// Peripherals disable (example, USB):

// ...

// Jump:

__set_CONTROL(0);
__set_MSP(vt->msp);
__ISB();
((void (*)(void))vt->reset)();

Is there more steps to pay attention before the jump?

2) Related with the primary application, in my previous bootloaders I had to set the interrupt vector table again after the jump. How is this done on i.MX RT processors?

Thanks.

0 项奖励
回复
4 回复数

1,914 次查看
joséviníciusmel
Contributor II

Hi,

First, thanks for your reply. 

Where is this done in the ota examples (like, evkmimxrt1170_lwip_httpssrv_ota_wifi)?

I tried to find the IOMUXC_LPSR_GPR_GPR26_CM7_INIT_VTOR, but I couldn't see this macro being called.

And related with the jump process, do you think that these commands are ok?

Thanks.

Regards,

Vinícius.

0 项奖励
回复

1,909 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @joséviníciusmel ,

If vector table is changed, VTOR must be reconfigured, either in bootloader or in application. 

You jump process is fine.

 

Regards,

Jing

0 项奖励
回复

1,891 次查看
joséviníciusmel
Contributor II

Hi Jing,

Thanks!

0 项奖励
回复

1,925 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @joséviníciusmel ,

Yes, if your application doesn't change vector table address, you must add it here. It's the IOMUXC_GPR26 register.

 

Regards,

Jing

0 项奖励
回复