i.MX MSD Device storage APIs to access file stored on the SDCard.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX MSD Device storage APIs to access file stored on the SDCard.

1,178 次查看
threeboystech
Contributor II

I am using an IMXRT1020-EVK board running SDK example code: evkmimxrt1020_dev_msc_disk_freertos

I have a 32GB SDCard plugged into my EVK board.

I can start the example application and my Windows11 computer detects the FLASH drive being present as expected.  I can then perform normal file transfer to/from the new drive and the files moved are stored on my SDCard as expected.

The provided readme.txt file provided in the SDK example code indicate the following document:

<MCUXpresso_SDK_Install>/boards/<board>/usb_examples/usb_device_msc_sdcard_lite/<rtos>/readme.pdf.

but this document is not present.  Nor is any other document in the indicated path.

Can someone point me to a link that describe the needed APIs that my f/w application can use to access these files that are on the SDCard?

 

Thanks

Terry

标签 (1)
0 项奖励
回复
2 回复数

1,135 次查看
threeboystech
Contributor II

Thanks. I was able to find this file now.  It's too bad that it's not providing the details of the files added to the flash drive.

After I'm able to copy/write/edit files on the "new flash drive" on computer, I would like to be able to access these files via my RT1021 f/w.  How do I gain the needed details of the files that have been added to the "flash drive".

Thanks.

0 项奖励
回复

1,145 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @threeboystech,

I believe the path described on readme.txt might be outdated. Here is the path where I found the readme.pdf file you look for:

C:\Users\<user>\mcuxpresso\02\SDKPackages\SDK_2_12_0_EVK-MIMXRT1020.zip\boards\evkmimxrt1020\usb_examples\usb_device_msc_disk\freertos\readme.pdf

This of course is based on the default installation location for the SDK. In reality, you can access the path from wherever the SDK archive is located, you just require to open the zip file:

SDK_2_12_0_EVK-MIMXRT1020.zip\boards\evkmimxrt1020\usb_examples\usb_device_msc_disk\freertos\readme.pdf

BR,
Edwin

0 项奖励
回复