i.MX Linux compilation problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX Linux compilation problem

跳至解决方案
3,569 次查看
pengjing918
Contributor II

1. Does the NXP i.MX series SOC only use yocto to compile and package the kernel, uboot, root file system?

2. Is there a separate BSP patch for Linux, and then add the BSP patch for i.MX to the Linux source code, and then compile it?

1.请问NXP i.MX系列SOC, 都只能使用yocto编译打包内核, uboot, 根文件系统吗? 

2.有没有单独提供Linux 的BSP补丁, 然后对Linux源码加上i.MX 的BSP补丁, 再编译的呢?

标记 (2)
1 解答
3,364 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

1\Yes, the linux BSP use the Yocto.

2\Sorry, no this kind of patch.

I have searched one thread also use Yocto, but Standalone, hope it can do some for you.

Detailed Operations For Standalone On Linux BSP of I.MX Processors 

Have a nice day

Rita

在原帖中查看解决方案

3 回复数
3,365 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

1\Yes, the linux BSP use the Yocto.

2\Sorry, no this kind of patch.

I have searched one thread also use Yocto, but Standalone, hope it can do some for you.

Detailed Operations For Standalone On Linux BSP of I.MX Processors 

Have a nice day

Rita

3,364 次查看
pengjing918
Contributor II

Thank you very much for your answer.
Are you an employee of nxp?

0 项奖励
回复
3,364 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

You are welcome. Yes, many engineers in this community, you can create thread if you have questions.

0 项奖励
回复