i.MX Framebuffer queries

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Framebuffer queries

2,322件の閲覧回数
positron
Contributor I

I'm using a mx53 QSB along with a TFT touch panel.

When going thro the imxfb.h under arch/arm/plat-mxc/include/mach/imxfb.h

I notice this structure.

struct imx_fb_videomode {
    struct fb_videomode mode;
    u32 pcr;
    unsigned char    bpp;
};

What does this pcr and bpp symbolize? I'm totally new to framebuffers and any pointers on this would be appreciated.

Thanks

タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,133件の閲覧回数
KursadOney
NXP Employee
NXP Employee

I think those values depend on your display. The user's manual for your display might have them listed. I'd start with some basic harmless values and modify if things look distorted or out of place. The link I put in my original reply goes over those a little bit too. Look for Panel Configuration Register. Older i.mx manual (maybe mx21?) might have more info.

0 件の賞賛
返信

2,133件の閲覧回数
positron
Contributor I

Thanks Kursad. I'll have a look at the attachment. Also I wanted to know on what pcr takes. I see some cryptic hex values all around. There is no where, it is explained why. Any ideas to find out the one for my display?

(One can see the pcr values in latest kernel sources)

0 件の賞賛
返信

2,133件の閲覧回数
KursadOney
NXP Employee
NXP Employee

bpp is bits per pixel.

It looks like pcr comes from here: http://cache.freescale.com/files/32bit/doc/app_note/AN2868.pdf and is for "panel configuration register". This name does not appear in the mx53 manual though so it's either renamed or not exactly used for mx53. I'm not sure.

0 件の賞賛
返信