i.MX 93 Using External Clock for Fractional PLL 'VIDEO_PLL'

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX 93 Using External Clock for Fractional PLL 'VIDEO_PLL'

2,025 次查看
dunk
Contributor III

Hi Community,

According to section 70.5 'PLL' in document 'IMX93RM.pdf', fractional PLL, including SYSTEM_PLL1, DRAM PLL, AUDIO_PLL and VIDEO_PLL.
I would like to feed my own clock (via CLKIN1 or CLKIN2) to VIDEO_PLL which will be used as clock root 'enet_timer2_clk_root'.

How do I do for this usage? Couple setting from RM as below:

- Register 'CLOCK_ROOT88_CONTROL': set to 11: VIDEO_PLL_CLK
- What's the register to select 'CLKIN1' or 'CLKIN2' for VIDEO_PLL_CLK? Register 'GPR20' seems to be relevant, but not precisely stated.

GPR20 (SRC General Purpose Register 20):
anamix_atx_sense_bus_enable_lv = gpr_src_general_reg_gpr20_gpr[0] default 0
anamix_pll_clk_mux = gpr_src_general_reg_gpr20_gpr[4:1] default 0
anamix_clkin_mux = gpr_src_general_reg_gpr20_gpr[6:5] default 0
anamix_clkin_mux2 = gpr_src_general_reg_gpr20_gpr[8:7] default 0
anamix_clkin1_ipp_ibe = gpr_src_general_reg_gpr20_gpr[9] default 1
anamix_clkin2_ipp_ibe = gpr_src_general_reg_gpr20_gpr[10] default 1

0 项奖励
回复
4 回复数

2,003 次查看
joanxie
NXP TechSupport
NXP TechSupport

what peripheral do you need to use  CLKIN1 or CLKIN2? do you use any OS?pls share more detailed information with me

0 项奖励
回复

1,992 次查看
dunk
Contributor III
Hi Joan,
The idea is to use external clock for driving the 1588 of ENET1 without sharing the same clock of rest of system.
With eternel clock, we can use additional DPLL for beter timing control.
0 项奖励
回复

1,982 次查看
joanxie
NXP TechSupport
NXP TechSupport

CLKIN1/CLKIN2 is for test purpose, if you need set the frequency for enet_timer2_clk_root, you just need to choose the source from ROOT88 you already know it, then set the corresponding pll frequency, you can refer to the dts file

linux-imx/arch/arm64/boot/dts/freescale/imx93.dtsi at lf-6.6.y · nxp-imx/linux-imx

clocks = <&clk IMX93_CLK_ENET1_GATE>,
<&clk IMX93_CLK_ENET1_GATE>,
<&clk IMX93_CLK_ENET_TIMER1>,
<&clk IMX93_CLK_ENET_REF>,
<&clk IMX93_CLK_ENET_REF_PHY>;
clock-names = "ipg", "ahb", "ptp",
"enet_clk_ref", "enet_out";
assigned-clocks = <&clk IMX93_CLK_ENET_TIMER1>,
<&clk IMX93_CLK_ENET_REF>,
<&clk IMX93_CLK_ENET_REF_PHY>;
assigned-clock-parents = <&clk IMX93_CLK_SYS_PLL_PFD1_DIV2>,
<&clk IMX93_CLK_SYS_PLL_PFD0_DIV2>,
<&clk IMX93_CLK_SYS_PLL_PFD1_DIV2>;
assigned-clock-rates = <100000000>, <250000000>, <50000000>;

0 项奖励
回复

1,980 次查看
dunk
Contributor III
Thanks for this details and dts example. I'll try this.
0 项奖励
回复