i.MX 8XLite Evaluation Kit boot error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX 8XLite Evaluation Kit boot error

ソリューションへジャンプ
5,685件の閲覧回数
jackchen1
Contributor I

Hello everyone,

    I have a i.MX 8XLite Evaluation Kit(MCIMX8DXL-WEVK, SCH-54318 REV A3). Now, there is

 some questions:  1、if boot from SD card,it will  power down and up cyclical about 300 milliseconds. 

2、serial download mode,when insert USB typ C(J15),PC show "LIBUSB_ERROR_IO" by uuu download.

 

0 件の賞賛
返信
1 解決策
5,503件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @jackchen1,

 

I hope you are doing well
 

 

Both BSP versions will function well, however using the most recent BSP version is usually advised as it comes with the latest drivers and firmware for more flexibility.

 

 
Thanks & Regards,
Sanket Parekh

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
5,386件の閲覧回数
claudio_b
Contributor II

I have the same problem.

I downloaded LF_v6.1.36-2.1.0_images_IMX8DXLEVK.zip and I mounted on SD card "imx-image-full-imx8dxlevk.wic" (7GB size)

.When I plug the SD card and I switch on the board, led D3 start blinking (I suppose it is resetting continously).

Dip switches of SW1 are set to 1101.

i don't see any data on the serial port. I only see COM port 12-13-14-15 even if the board is powered off.

0 件の賞賛
返信
5,629件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @jackchen1,

 
I hope you are doing well
 
Kindly confirm that you are booting the EVK with the correct image.
Please try to boot the board with the Demo images provided by NXP from the below link.
 
Thanks & Regards,
Sanket Parekh
0 件の賞賛
返信
5,619件の閲覧回数
jackchen1
Contributor I
Hi Sanket Parekh,
Thanks for your response, We have tried a few image including Linux 6.1.1_1.0.0 and Linux 6.1.22_2.0.0 (latest version). We couldn't be sure which version is OK. thanks!
0 件の賞賛
返信
5,504件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @jackchen1,

 

I hope you are doing well
 

 

Both BSP versions will function well, however using the most recent BSP version is usually advised as it comes with the latest drivers and firmware for more flexibility.

 

 
Thanks & Regards,
Sanket Parekh

0 件の賞賛
返信